Public Attributes#

uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint16_t

Public Attribute Documentation#

sof#

uint8_t tx_beam_stop_frame_t::sof

Definition at line 106 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

type#

uint8_t tx_beam_stop_frame_t::type

Definition at line 107 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

timestamp1#

uint8_t tx_beam_stop_frame_t::timestamp1

Definition at line 108 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

timestamp2#

uint8_t tx_beam_stop_frame_t::timestamp2

Definition at line 109 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

rssi#

uint8_t tx_beam_stop_frame_t::rssi

Definition at line 110 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

counter#

uint16_t tx_beam_stop_frame_t::counter

Definition at line 111 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h