Managing GPIOs and Peripherals
- GPIO Commands and Variables
- GPIO Functions and Pins
- Viewing GPIO Usage
- Deregistering a GPIO
- Setting GPIO Function
- Setting and Getting GPIO Values
- LEDs
- Communicating Peripheral Information Over the Network
- Peripheral GPIO Mapping by Function
Peripheral commands and variables enable access to general purpose input/outputs (GPIOs).
GPIO Commands and Variables
Typically, particular GPIOs are hard-wired to components such as LEDs, buttons and sensors. Other GPIOs are configurable for input and output.
GPIOs can be used for special system functions, including (but not limited to):
- assigning a LED as wlan status indicator
- selecting between serial bus modes: COMMAND or STREAM
- general standard IO function
- out-of-band interrupts
GPIO commands and variables allow control of the function and direction of the GPIOs.
GPIO Commands
GPIO Variables
- broadcast.data
- bus.stream.cmd_gpio
- gpio.init
- gpio.usage
- ioconn.control_gpio
- ioconn.status_gpio
- setup.gpio.control_gpio
- system.indicator.gpio
- system.indicator.state
- tcp.server.connected_gpio
- tcp.server.data_gpio
- udp.server.data_gpio
GPIO Functions and Pins
GPIO functions and pins differ for different devices.
Viewing GPIO Usage
To see the current GPIO usage, read the gpio.usage variable:
get gp u
The
gpio_usage
command does not list GPIOs set to
none
: these GPIOs have no function configured.
Deregistering a GPIO
GPIOs that are already assigned to a function need to be deregistered before reassignment. To determine if the GPIO is assigned, read the gpio.usage variable.
Deregistering a Standard I/O GPIO
If a GPIO is assigned to a Standard I/O function, use the
gpio_dir
command with an argument of
none
or
-1
.
For example, to deregister user LED1 on the Moray board (GPIO13):
gdi 13 none
For the change to persist after reboot, you need to set the gpio.init variable and save. For example:
set gpio.init 13 none
save
Deregistering Alternative Function GPIOs
Variables that allow functions to be assigned to a GPIO are as follows:
- bus.stream.cmd_gpio
- ioconn.control_gpio
- ioconn.status_gpio
- setup.gpio.control_gpio
- system.indicator.gpio
- tcp.server.connected_gpio
- udp.server.data_gpio
To de-register a GPIO assigned to a function, set the function variable to
-1
. For example, if the GPIO is assigned to
setup.gpio.control_gpio
:
set setup.gpio.control_gpio -1
You can also deregister a GPIO by assigning its function to a different GPIO. For example, if setup.gpio.control_gpio is assigned to GPIO 6, you can deregister GPIO 6 by assigning the function to GPIO 7:
set setup.gpio.control_gpio 7
If the GPIO is assigned to a system.indicator.gpio function, you need to specify the function argument as well as the GPIO number argument. See System Indicator Functions .
Setting GPIO Function
GPIO function can be set by commands or variables.
To use a GPIO as Standard I/O, deregister the GPIO if it is already assigned, then use the gpio_dir command to set its direction.
For example, to set user LED1 on the Moray to an output:
gdi 13 out
For the change to persist after reboot, you need to set the gpio.init variable and save. For example:
set gpio.init 13 out
save
You can also use a GPIO for a number of special functions, such as indicators, or inputs to control special features.
System Indicator Functions
Use the system.indicator.gpio and system.indicator.state to configure a GPIO for a system indicator function. Deregister the GPIO if necessary before setting its function.
Save the variables and reboot to complete the configuration change, since these functions are managed by services configured during bootup.
Note
: This GPIO function change cannot be implemented by Gecko OS command if a
gpio_config_init.csv
file sets the GPIO function.
On the Mackerel and Moray evaluation boards, the red, yellow and green LEDs are configured by default as system indicators, showing soft AP, network and wlan status.
Each system indicator function can be associated with only one GPIO. Setting the indicator to a GPIO automatically sets to
none
( any GPIO previously assigned to that system indicator.
Bus Stream Command GPIO
Set the bus.stream.cmd_gpio to configure a GPIO to force Gecko OS from stream mode to command mode. See Serial Interface for a discussion of stream mode and command mode.
This feature is intended for automated use with a host MCU. In the following demonstration of this feature on the Mackerel evaluation board, we use Button 2 (GPIO 11).
| Gecko OS commands | Comments |
|---|---|
|
|
Because the device is in stream mode, characters typed into the serial terminal are not echoed. Press Button 2, and Gecko OS displays:
Command Mode Start
While holding down Button 2, Gecko OS commands may be typed into the terminal, and characters are echoed. For example, you can set bus mode to command and save, to restore command mode after a reboot. Release Button 2 and the device returns to stream mode.
GPIO Controlled Network Connection
Gecko OS allows you to configure full details of a connection to a host, then connect and disconnect under the control of a single GPIO. The connection can be via:
- TCP
- TCP with TLS
- UDP
Set ioconn.control_gpio to assign a GPIO to the control function that makes and breaks the connection.
Set ioconn.status_gpio to assign a GPIO to indicate the status of the connection.
See the ioconn.* variables for details.
The GPIO-Controlled Network Connection application note provides further examples.
TCP Server Status GPIOs
The tcp.server.connected_gpio variable provides a GPIO to indicate whether a client is connected to the TCP server.
The tcp.server.data_gpio variable provides a GPIO to indicate whether a connected client has data available to read.
See the TCP Server + softAP application note for further information.
UDP Server Data GPIO
The udp.server.data_gpio variable allows assignment of a GPIO to indicate whether a connected UDP client has data available to read.
Setting and Getting GPIO Values
If a GPIO is set to the Standard I/O function, and the GPIO direction is set as an output with the
gdi
(
gpio_dir
) command, the GPIO value may be configured with the
gse
(
gpio_set
) and
gge
(
gpio_get
) commands. For example:
> gdi 12 out
Set OK
> gge 12
0
> gse 12 1
Set OK
> gge 12
1
If a Standard I/O GPIO is configured for input, you can read the GPIO value but you cannot set it:
> gdi 12 in
Set OK
> gge 12
0
> gse 12 1
GPIO not configured for output
Command failed
LEDs
The level of a LED can be controlled via a GPIO with the Standard I/O output.
GPIO Standard I/O Control
A LED can be turned on or off by configuring as a Standard I/O output, then setting the GPIO level.
For example, to turn on Mackerel user LED1, use the gpio_dir command and the gpio_set command:
| Gecko OS commands | Comments |
|---|---|
|
|
Communicating Peripheral Information Over the Network
The Gecko OS TCP and UDP client and server features provide frameworks for building a customised application for transmitting and receiving monitor and control data from your Gecko OS device. For examples of these applications, see:
Gecko OS also provides general systems for handling information transfer.
A Gecko OS device can be configured to broadcast GPIO and other data at regular intervals, via the broadcast group of variables.
The broadcast.data variable lets you specify what data is broadcast. GPIOs are specified by GPIO number. See the Broadcast UDP Packet for a demonstration of this feature.
Peripheral GPIO Mapping by Function
See your Silabs datasheet. .