Troubleshooting Guide
If you clicked through to here, then we expect you are having some trouble with Gecko OS. Please accept our apologies; perhaps our documentation is not clear enough or you have found an operational corner case.
The notes in the following sections should get you up and running again quickly. If you are still having trouble after reading through these notes, please log a support ticket .
Basics
- Check the power LED is on
- When you type into the terminal application (see Getting Started ), the UART LED(s) on the evaluation board should blink.
My device fails to associate to the network
Please check each of the following points carefully to help resolve this issue.
- Double-triple check the spelling of the network name assigned to wlan.ssid . It is VERY easy to incorrectly enter the name of a network, and especially so if the network name is long and unwieldy.
- Check the network password or security key assigned to wlan.passkey . If your network uses WEP (and we sincerely hope it does not since WEP is NOT secure), follow the setup procedure for WEP keys documented in the wlan variable documentation .
My device has missing commands or variables. What do I do?
If you enter a valid command or variable and see an
Unknown command
or
Unknown variable or option
error, your device may be in
Safe Mode
. Alternatively an
OTA update
may have been interrupted before completion.
Recovery from Safe Mode
In safe mode,
system.safemode.status
is set to
1
, and there is a reduced set of commands and variables (see
help all
).
To recover from Safe Mode, follow the instructions in Update and Recovery, Safe Mode . The essential recovery commands are summarised below.
| Gecko OS Commands | Description |
|---|---|
|
|
Once the device has successfully returned to normal operation, it is advisable to ensure you have the latest Gecko OS firmware version. Upgrading to the latest firmware provides your device with the latest fixes to problems, one of which may have caused the device to enter safemode. To update, simply enter the ota command.
Recovery from Interrupted OTA Update
If an OTA update is interrupted, you can resume it and complete the update. You may have to set the wlan.ssid and wlan.passkey variables to rejoin your WLAN. Then run the ota command. When the OTA update completes, your device returns to normal operation.
TLS Errors
If when attempting a TLS connection, you receive an error message such as
TLS malloc failed
, then Gecko OS may be low on memory. See
Networking and Security, Increasing Available Memory for TLS
.