Gecko OS Commands
This page lists the Gecko OS Command API with a full description of how to use each command.
There are several interfaces for issuing commands. See Serial Interface, Issuing Commands and Streaming Data. For command format, see Serial Interface, Command Protocol.
Gecko OS Variables, which are used to configure Gecko OS, are accessed using the get and set commands.
Nav Tips for Humans
The Gecko OS Command API is friendly for humans too. Use the following tips and you'll be an expert Gecko OS terminal jockey in no time flat!
Tip | Description |
---|---|
Tab complete | Type part of a command or variable name then hit the tab key. The command completes or partially completes, just like a terminal in the linux or DOS world. |
History | Up to 5 commands of history are available. Press the up-arrow key to access recently entered commands. |
Edit | The left-arrow, home, end and backspace keys may be used to edit or navigate commands already present on the command line. |
Shortcuts
A shortcut is assigned to each command. Common sense dictates the rules for shortcuts. Commands that are already short do not need a shortcut other than their name, shortcuts for longer commands sometimes take the first three letters of the command name, and other times take the first letter of the name plus several other letters contained in the name. Shortcuts are no longer than six characters and are easy to guess, the ultimate reference however is command help and the documentation on this page.
Documentation Format
Many of the Gecko OS responses shown in the examples on this page were captured with system.print_level = all, and system.cmd.header_enabled = true. These settings are provided to make it easy for a host microcontroller to parse responses by examining response headers. Information about machine parsing is available in Serial Interface, MCU Config.
Documentation for each command is provided in the format shown below.
command
Abbreviation
cmd
Description
A description of how to use the command with, together with notes about available options and arguments.
Syntax
Formal command syntax with a listing of all available options and arguments.
Example
One or more examples demonstrating how the command is used.
Commands by Group
- File System and Flash
- Faults and SafeMode
- Network Management
- GPIOs and Peripherals
- Variable and Configuration Management
- DMS and OTA
- DFU
- Serial Bus Mode
- Streams
- HTTP Methods
- HTTP Files
- Ping
- Setup
- TCP
- UART
- UDP
- Device System and Power Management
- Host Boot
Description of Commands
dfu_query
Abbreviation
dfuq
Description
Query the Device Management Server (DMS), and return either Up-to-date
or bundle version string if newer release available. If a newer release is available, use dfu_update to update your device.
Result codes and messages are:
204, Up-to-date
200, <DMS generated bundle string version>
e.g.
Note: Querying the DMS requires a memory-intensive TLS connection, and may fail if memory is low. See Networking and Security, Increasing Available Memory for TLS.
Note: If the dfu_query
command fails with the message:
{"result":"fail","message":"device not claimed"}
then you need to claim the device before running the df_query
command. See Update and Recovery, the DMS Server.
Note: The dfu_update
and dfu_query
commands replace the ota
command for versions previous to v2.2. The ota
command is deprecated and will be removed in the next major version.
Syntax
> dfu_query
Example
dfu_query
dfu_update
Abbreviation
dfuu
Description
Initiate a secure update. The secure OTA protocol uses industry standard TLS/HTTPS security with both client-side and server-side certificate verification.
For details of this process and associated requirements, see Update and Recovery, Secure OTA Update. This process requires you to claim the device using the dms_claim command.
As an additional measure of security, the server authenticates each device using the universally unique system.uuid embedded inside the hardware of each device.
Downloaded bundle files overwrite local files only if the bundle file has a later version. To ensure that bundle files overwrite local files regardless of version, force an update with the -f
option.
Download a specific firmware bundle version with the -b
option. Specifying a bundle forces an update. Bundle files overwrite local files regardless of version. See the note for the -b
option in Syntax below.
To maintain a saved configuration through an OTA update, save the configuration as default_config.csv
.
Note: OTA requires a memory-intensive TLS connection, and may fail if memory is low. See Networking and Security, Increasing Available Memory for TLS.
Note: If the ota
command fails with the message:
{"result":"fail","message":"device not claimed"}
then you need to claim the device before running the ota
command. See Update and Recovery, the DMS Server.
Note: The dfu_update
and dfu_query
commands replace the ota
command for versions previous to v2.2. The ota
command is deprecated and will be removed in the next major version.
Syntax
> dfu_update [-f] [-b <full version>]
-f
: force update. Bundle files overwrite local files, regardless of version.-b
: download a specified bundle, for example a previous version. For a Gecko OS bundle, specify only the full version number, e.g.dfu_update -b 2.0.4
. For full versions of Gecko OS by platform, see DMS Products. For full versions of custom product bundles, refer to the DMS Products list for that product.- Note: the
-b
option is available only when you are updating a development product. From the moment you load a production product on your device, the device canota
only to the most recent release of the product, corresponding to the device's product release type (alpha, beta or release).
- Note: the
Platforms
- AMW007
Example
> dfu_update
Connecting to network
Request POST /ota/05b300df003134534e394b8330393232323a3533/0
Connecting (HTTP): ota.zentri.com:443
Starting TLS
HTTP response: 200
Downloading new firmware...
Bundle version: Gecko OS-1.0.0.1, Built:2015-11-11 02:23:15 for AMW004.3
Downloading: command_help.csv-1.0.0.1 (25822, 0xFB, 0x1)
Downloading: default_setup.script-1.0.0.1 (189, 0xFD, 0x9)
Downloading: /setup/index.html-1.0.0.1 (9266, 0xFE, 0x1)
Downloading: /setup/images.png-1.0.0.1 (18067, 0xFE, 0x1)
Downloading: /sys/kernel.bin-1.0.0.1 (352804, 0x0, 0x801F)
Downloading: wifi_fw.bin-1.0.0.1 (191677, 0x1, 0x8009)
Downloading: /sys/services.bin-1.0.0.1 (83848, 0x80, 0x801F)
Downloading: geotrust_ca.pem-1.0.0.1 (1162, 0x3, 0x9)
Downloading: /favicon.ico.gz-1.0.0.1 (1853, 0xFE, 0x1)
Downloading: /setup/index.css.gz-1.0.0.1 (10539, 0xFE, 0x1)
Downloading: /setup/index.js.gz-1.0.0.1 (38771, 0xFE, 0x1)
Updating kernel to version: 1.0.0.1
Updating firmware files...
Updating file: wifi_fw.bin to version: 1.0.0.1
Updating file: /sys/services.bin to version: 1.0.0.1
Found new bootable app: /sys/services.bin (47), booting to it now!
OTA completed successfully
[Ready]
dms_activate
Abbreviation
dmsa
Description
Activates the current device to the specified product.
This command requires the device to have access to the Internet, so network credentials wlan.ssid and wlan.passkey must be set. See Getting Started.
Platforms
- AMW007
Syntax
dms_activate <product_code>
Example
> dms_activate MY_PRODUCTCODE
Success
dms_claim
Abbreviation
dmsc
Description
Claims the current device, associating it with your DMS account.
This command requires the device to have access to the Internet, so network credentials wlan.ssid and wlan.passkey must be set. See Getting Started.
The device can be claimed with a token.
To obtain a DMS token:
- If you don't already have a Zentri DMS account, use your Silicon Labs login to create a free account at https://dms.zentri.com/signup
- Log in to https://dms.zentri.com with your Silicon Labs login
- Click the
Profile
link to go to profile - Choose the
API tokens
tab. This takes you to https://dms.zentri.com/account/tokens - Click
Issue API Token
- Copy the token to use as the argument to the
dms_claim
command
Example
Syntax
Claim with username and password
dms_claim <dms_username> <dms_password>
Example
> dms_claim my_dms_username my_dms_pw
Success
Claim with dummy username and token
This option is provided for backward compatibility with the two argument requirement in previous versions.
dms_claim <dummy_username> <token>
Note that the <dummy_username>
argument is a placeholder and does not need to be a valid username.
Example
> dms_claim dummy_username Q3txWTdHYktvRVV5ekhwQkJHeXJGOFdW
Success
Claim with token only
dms_claim <token>
> dms_claim Q3txWTdHYktvRVV5ekhwQkJHeXJGOFdW
Success
exit
Abbreviation
exit
Description
Exits command mode immediately and returns to stream mode. Only valid when stream mode is operational.
Syntax
> exit
Platforms
- AMW007
Example
> exit
Command Mode Stop
factory_reset
Abbreviation
fac
Description
Reset the application configuration to factory default values. The WLAN MAC address wlan.mac
must be provided as an argument to avoid accidental factory reset.
Note: The application may also be factory reset by asserting GPIO0 for 10 seconds through a module reset as described in Update and Recovery, Factory Reset.
Syntax
> factory_reset <MAC address>
Properties
- available in Safe Mode
Platforms
- AMW007
Example
> get wl m
R000019
4C:55:CC:10:03:44
> fac 4C:55:CC:10:03:44
Success
faults_print
Abbreviation
faup
Description
List system faults. After 8 faults, the system enters Safe Mode. See Update and Recovery, Safe Mode.
Syntax
> faults_print
Properties
- available in Safe Mode
Platforms
- AMW007
Example
> faup
Success
faults_reset
Abbreviation
faur
Description
Reset system fault counter. See Update and Recovery, Safe Mode.
Syntax
> faults_reset
Properties
- available in Safe Mode
Platforms
- AMW007
Example
> faur
Success
file_copy
Abbreviation
fcp
Description
Copy a file.
The new file name must be different to the old file name, and there must be enough space for the new file to be created.
Syntax
> file_copy <old_filename> <new_filename>
where
<old_filename>
is the name of the existing file<new_filename>
is the name of the new file
Platforms
- AMW007
Example
> file_copy myfile.txt mynewfile.txt
R000009
Success
file_create
Abbreviation
fcr
Description
Create a new file <size>
bytes in length. After the command is issued, the ensuing <size>
number of bytes is written to the file system.
Files can be written in chunks smaller than the specified length, using the -o
option.
Additional options include a version, file type and CRC, or checksum.
See File System, Writing Files.
Syntax
> file_create [-o] <filename> <size> [<version> [<type> [<crc>]]]
Option | Description |
---|---|
-o | Optional. Leave file open for writing. Default: Off If the -o option is not specified, then all the file data must come immediately after the command.If the -o option is specified, the file can be written in chunks. A stream handle is returned after the command. The write command is used to write data to the file. The stream closes automatically after the specified <size> bytes of data is written. The file is not considered 'valid' until it automatically closes.If the module is rebooted or the close command is issued before all data is written, the file data is lost. It is not possible to restart writing the file after the stream is manually closed. See Networking and Security, Network Connections and Streams. |
filename | Name of file to be written. |
size | Length of file in bytes. After the command is issued, write the file content to the serial interface. |
version | Specify version number. Default 1.0.0 |
type | The file type, in hex format1. See File System, File Types Default: FE (MISC_FIX_LEN ) |
crc | optional, CRC16-CCITT checksum of the file data, in hex format1. See File System, Checksum |
1: hex format: upper or lower case, with or without leading 0x
, e.g. 0xFE
, fe
, 0xe1c8
Platforms
- AMW007
Examples
Create a file with no special options
In the example below, the file content , Hello World!
is 12 bytes in length and is entered or sent by the user.
> fcr myfile.txt 12
Hello World!
File created
Check result:
> ls -l
! # Type Flags Hnd Size Version Filename
...
# 6 e-FE 0021 104 12 1.0.0.0 myfile.txt
The associated file handle (Hnd) may vary.
Flags 0021
: Valid User
Create an essential
file that is not deleted during an OTA update
> fcr -e myfile.txt 12
Hello World!
File created
Check result:
> ls -l
! # Type Flags Hnd Size Version Filename
...
# 6 e-FE 0061 104 12 1.0.0.0 myfile.txt
Flags 0061
: Valid User Essential
Create a file with specified version and user type
(See File System, File Types)
> fcr myfile.txt 12 1.1.0.1 AB
Hello World!
File created
Check result:
> ls -l
! # Type Flags Hnd Size Version Filename
...
# 6 e-AB 0021 104 12 1.1.0.1 myfile.txt
Create file for writing in chunks
> file_create -o my_file.txt 100
3
> write 3 50
... <50 bytes of data> ...
> write 3 50
... <50 bytes of data> ...
File created
Check result:
! # Type Flags Hnd Size Version Filename
...
# 6 e-FE 0021 107 100 1.0.0.0 my_file.txt
file_delete
Abbreviation
fde
Description
Delete a file from the file system.
Note: Deleting a file automatically closes the associated file stream.
Syntax
> file_delete <filename> | <memory>-<handle>
where
<filename>
is the name of the file<memory>-<handle>
can be used to distinguish between files with the same name:<memory>
is the memory type, which may be one of the following:i
- internal memorye
- extended memoryb
- bulk memory
<handle>
is the file handle on the memory. This appears under theHnd
column of the file listing
Note: <memory>-<handle>
overrides <filename>
- for example, if there exist both a file in extended flash with file handle 234
, and a file named e-234
, then the command file_delete e-234
deletes the file with memory-handle e-234
, rather than the file named e-234
.
Properties
- available in Safe Mode
Platforms
- AMW007
Example
> fde myfile.txt
L000014
File deleted
R000009
Success
Example
To delete the file with handle 234
on e
xtended flash:
> file_delete e-234
L000014
File deleted
R000009
Success
file_open
Abbreviation
fop
Description
Open a file and return a file stream handle if successful. Once open, the file contents may be read with the stream_read command.
See Networking and Security, Network Connections and Streams.
Syntax
where:
<filename>
is the name of the file<memory>-<handle>
can be used to distinguish between files with the same name:<memory>
is the memory type, which may be one of the following:i
- internal memorye
- extended memoryb
- bulk memory
<handle>
is the file handle on the memory. This appears under theHnd
column of the file listing
Note: <memory>-<handle>
overrides <filename>
- for example, if there exist both a file in extended flash with file handle 234
, and a file named e-234
, then the command file_open e-234
opens the file with memory-handle e-234
, rather than the file named e-234
.
Platforms
- AMW007
Example
> fop myfile.txt
R000003
0
Example
To open the file with handle 234
on e
xtended flash:
> file_open e-234
R000003
0
file_stat
Abbreviation
fst
Description
Display file statistics for the specified file.
Statistics are displayed in a comma separated list, in the order:
size,CRC,long version,storage type,file type,flags,handle
# | Stat | Comment | Reference |
---|---|---|---|
1 | size | file size, displayed in decimal format | |
2 | CRC | CRC is calculated from the unencrypted file data. Displayed in hex format, with no 0x prefix. | File System, File Checksum |
3 | long version | File System, File Version | |
4 | storage type |
| File System, Flash Storage |
5 | file type | File System, File Types | |
6 | flags | File System, File Flags | |
7 | handle | Listed in the 'Hnd' column in ls -l output | A unique ID assigned to each file |
The ls -v (verbose file listing) command displays all of these properties except the CRC.
Syntax
> file_stat <filename>/<memory type>-<handle>
where:
<memory type>
is the letter at the start of theType
column in the ls -l listing of a file:e
:extendedi
:internalb
:bulk.
See File System, File Types.
<handle>
is the file ID number listed in theHnd
column in the ls -l listing of a file.
The handle must be prefixed by the memory type followed by a dash, e.ge-
for extended flash.
Platforms
- AMW007
Example
> file_stat geotrust_ca.pem
1236,6E5A,3.0.0.11,e,3,1,8
> file_stat e-8
1236,6E5A,3.0.0.11,e,3,1,8
force_safemode
Abbreviation
force_safemode
Description
Force the module into safe mode. This command is used by a host to test recovery procedures if the module enters safe mode. See Application Notes, Recovery from Safe Mode for further information.
This is a hidden command that does not appear in the list of commands returned by help commands.
Syntax
> force_safemode <module MAC address>
Platforms
- AMW007
Example
> force_safemode 4C:55:CC:10:10:98
Forcing safemode...
Rebooting
[Disassociated]
Gecko OS-2.1.0.9, Built:2015-01-25 15:58:14 for AMW004.3, Board:AMW004-E03.3
*** Max faults exceeded. Entering Safe Mode.
SAFEMODE>
format_flash
Abbreviation
format
Description
Format (i.e. erase all contents) of bulk or extended flash chip. If the extended flash is specified, ALL files BUT the wifi_fw.bin file are erased.
For details on enabling and using bulk flash, see File System, Flash Storage.
Syntax
> format_flash <module MAC address>
Platforms
- AMW007
Properties
- available in Safe Mode
Example
> format 4C:55:CC:10:10:98
Formatting flash...
get
Abbreviation
get
Description
Get the value of a Gecko OS variable or group of variables.
Syntax
> get <[variable name] / [variable group]> [options]
Properties
- available in Safe Mode
Platforms
- AMW007
Example 1
> get time.rtc utc
R000029
2014-03-23T23:54:33.021464Z
Example 2
> get bus
R000166
bus.data_bus: uart0
bus.log_bus: uart0
bus.mode: command
bus.stream.cmd_gpio: 0
bus.stream.cmd_seq: $$$
bus.stream.flush_count: 1500
bus.stream.flush_time: 20
gpio_dir
Abbreviation
gdi
Description
Set the direction of a general purpose I/O pin. To deregister the GPIO, set the direction to either -1
or none
.
Note : This is a run-time only setting: the value is not saved with the save command. To set the direction of a GPIO after a reboot, set the variable gpio_init. See Peripherals, Setting GPIO Function.
Syntax
> gpio_dir <GPIO#> <direction name/enum> [0/1]
where:
<GPIO#>
is the number of the GPIO. See Peripherals and GPIOs for your platform.<direction name/enum>
- see table below<0/1>
- initial value of the GPIO. The value is set before the direction is changed, to prevent glitches on the GPIO line.
For each I/O type there is a name and ab enum values. The <direction name/enum>
argument can specify either a name or an enum value:
I/O Type Description | Direction Name | Enum Value |
---|---|---|
Input, pull-up | ipu | 0 |
Input, pull-down | ipd | 1 |
Input, high-impedance | in | 2 |
Output, push-pull | out | 3 |
Output, open-drain no-pull | ood | 4 |
Output, open-drain pull-up | oodpu | 5 |
Deregister the GPIO | none | -1 |
Platforms
- AMW007
Example
> gdi 12 in
R000008
Set OK
gpio_get
Abbreviation
gge
Description
Get the current value of a general purpose I/O pin.
Syntax
> gpio_get <GPIO#>
Platforms
- AMW007
Example
> gge 12
R000003
0
gpio_set
Abbreviation
gse
Description
Immediately set the value of a general purpose I/O pin. When setting a GPIO, the GPIO direction must be also correctly set using the command gpio_dir
or the command will fail.
Syntax
> gpio_set <GPIO#> <value>
Platforms
- AMW007
Example
> gse 12 1
L000032
GPIO not configured for output
R100016
Command failed
gpios_get
Abbreviation
gges
Description
Get the current value of all general purpose I/O pins.
The value of standard GPIOs is returned as either 0
or 1
. Other GPIO types not configured for GPIO access (such as UART pins or system indicators) are returned as X
. GPIO values are in GPIO number order, increasing from left to right, with value for GPIO0 at left.
Syntax
> gpios_get
Platforms
- AMW007
Example
> gpios_get
R000031
0XX00X0000000XX10XXX000000000
gpios_dir
Abbreviation
gdis
Description
Set the direction of all general purpose I/O pins.
A direction for each GPIO must be provided in the <direction array>
. The <direction array>
is in GPIO number order, increasing from left to right, with the direction for GPIO0 in the first (left-most) position in the array.
Note : This is a run-time only setting. The value is not saved with the save command. To set the initial direction of a GPIO after a reboot, set the variable gpio_init. See Peripherals, Setting GPIO Function.
Syntax
> gpios_dir <direction array>
where each <direction array>
element may be one of the values in the following table
I/O Type Description | Enum Value |
---|---|
Input, pull-up | 0 |
Input, pull-down | 1 |
Input, high-impedance | 2 |
Output, push-pull | 3 |
Deregister the GPIO | f |
Platforms
- AMW007
Example
> gdis 0123ffff
R000008
Set OK
help
Abbreviation
help, ?
Description
Return a list of commands or variables; or return help for a specific command or variable.
Syntax
> help [all/commands/variables/<command>/<variable>]
Platforms
- AMW007
Example
> help
Usage : help [all/commands/variables/<command>/<variable>]
Shortcut: help
Brief : Return a list of commands or variables; or return
help for a specific command, variable or group of
variables.
http_add_header
Abbreviation
had
Description
Add a custom HTTP header to the HTTP stream specified by <handle>
.
See Networking and Security, HTTP Client.
Syntax
> http_add_header <handle> <key>[:extended] <value>
where:
Option | Description |
---|---|
<handle> | the stream handle supplied in response to the http_head or http_post commands (opened with -o option) |
<key> | header key |
<key>:extended | extended header: If the <key> argument has :extended appended to it (no spaces) then the <value> argument is omitted and the HTTP header value is entered in the following line.The extended HTTP header value may be up to 1024 characters. The extended HTTP header value is terminated with the \r\n characters. |
<value> | header value |
Options must be provided in the order shown.
Platforms
- AMW007
Example
> had 1 Content-type application/text
Success
http_download
Abbreviation
hdo
Description
Download one or more files from a remote HTTP server and save to the extended or bulk flash.
Timeout is determined by tcp.client.connect_timeout.
Note: The remote HTTP server must return the Content-length
header in the HTTP response. The file system must have the size of the file before creating it.
See Networking and Security, HTTP Client.
Syntax
Download a Single File
> http_download [-i <wlan/softap>] [-m <json_size>] [-d] [-[e]] [-c <CRC>] <url>
[<flash_file_name> [<version> [<type> [<cert_filename> ] ] ] ]
where parameters are as follows:
Option | Description |
---|---|
-i | Optional - Specify interface, MUST come first. If omitted uses network.default_interface. |
-m <json_size> | Optional - Download multiple files with a json specification of size <json_size> .MUST come first if -i option not used.No other parameters are valid with -m option.See Downloading Multiple Files below for more information. |
-d | Don't delete duplicate files. By default all duplicate file names are overwritten; with this option the command will fail on duplicates. |
-e | Optional flag - Indicates file is essential. |
-c <CRC> | Optional, CRC for file, in hex format*. On download, the file CRC is calculated and compared against this value. The file is not set 'valid' unless the CRCs match. See File System, File Checksum. |
<url> | Full path to a file on a http server. See below for more info about URL. |
<flash_file_name> | Optional - name to save file as. Use url filename if omitted |
<version> | Optional - default 1.0.0 if omitted, set to 0 to use default |
<type> | Optional - the type of file, default: miscellaneous text file, 0xFE . Type can be in hex or decimal format. See File System, File Types |
<cert_filename> | Optional - TLS certificate filename |
- hex format: upper or lower case, with or without leading
0x
, e.g.0xFE
,fe
,0xe1c8
Downloading Multiple Files
> http_download -m <json_size>
Immediately after issuing this command, send <json size>
bytes of a JSON formatted manifest file. An example of the manifest file is as follows:
{
"path" : "https://myserver.com/path/to/my/files/",
"cert" : "mycert.pem",
"files" : [
{
"remote" : "name_of_remote_file.html",
"local" : "name_of_flash_file.html",
"version" : "1.0.0",
"type" : 150,
"flags" : "eu",
"crc" : 23423
},
{ ... }
]
}
Notes:
- Only the "remote" parameter is mandatory. The other parameters are optional.
- In the manifest, the file type and crc are expressed in decimal, not hex, unlike in the
-c
parameter. - The file type
150
(hex0x96
) is a custom user type.
String Replacement
Gecko OS allows string replacement in the URL of the file for download, using a C-like or pythonesque syntax.
If the url contains %s
, then the supplied filename is substituted for %s
.
Example:
hdo 192.168.1.110:50007?id=%s&action=download my_file.txt
generates the URL:
http://192.168.1.110:50007?id=my_file.txt&action=download
and creates the file: my_file.txt
in the module file system.
String replacement is also available in the manifest. For example:
{
"path" : "http://myserver.com?file=%s&user=name&pass=1234",
"cert" : "mycert.pem",
"files" : [
{
"remote" : "my_file1.txt",
},
{
"remote" : "my_file2.txt",
},
]
}
generates the following URLs for download:
http://myserver.com?file=my_file1.txt&user=name&pass=1234
http://myserver.com?file=my_file2.txt&user=name&pass=1234
Platforms
- AMW007
Example
Save page at example.com to file test.html:
> hdo http://example.com test.html
Downloading: test.html to flash file system
Request GET /
Connecting (http): example.com:80
HTTP response: 200
Success
> ls -v
! # Type Flags Hnd Size Version Filename
...
# 8 e-FE 0021 108 1270 1.0.0.0 test.html
...
http_get
Abbreviation
hge
Description
Perform an HTTP(S) GET request and return a network stream handle if successful.
The protocol is assumed to be HTTP unless otherwise specified in the <url>
parameter.
For a URL longer than 124
characters the command and url exceed the maximum command line length.
In this case use the --long_url
option instead of including the URL as a command argument. Send the long URL, terminated by \r\n
, immediately after the terminating \r\n
of the command.
To allow custom headers, use the -o
option.
Timeout is determined by tcp.client.connect_timeout.
See:
Syntax
> http_get [-i <wlan/softap>] [-g < GPIO#>] [-o] <url> [ca_cert_filename]
where:
Parameter | Description |
---|---|
-i | Network interface. Possible values are wlan or softap . Overrides default specified by network.default_interface |
-g <GPIO#> | specify a GPIO to indicate buffered data is waiting to be read. Set to -1 to disable |
-o | Open the HTTP request but do not send. This enables custom header(s) to be added to the request using the http_add_header command. |
<url> | URL to which request is sent. The URL prefix http:// is optional for standard HTTP transactions, however https:* must be added for secure HTTPS transactions. |
Options must be provided in the order shown.
Platforms
- AMW007
Example
> hge https://www.google.com.au
[2014-04-02 | 13:27:20: Connecting: https://www.google.com.au]
Request GET /
Connecting (HTTP): www.google.com.au:443
Starting TLS
[2014-04-02 | 13:27:21: Connected: 0]
HTTP response: 200
Status: 200
0
> hge -o example.com:80
[2014-04-11 | 10:48:25: Opening: example.com:80]
Request GET /
Connecting (HTTP): example.com:80
[2014-04-11 | 10:48:25: Opened: 1]
1
> http_get --long_url
http://example.com/arbitrary_page?param1=abvcedfgssassssdfs¶m2=asdfadsfasd¶m3=11111111111111
[2016-05-10 | 02:26:50: Opening:http://example.com]
Request GET /arbitrary_page?param1=abvcedfgssassssdfs¶m2=asdfadsfasd¶m3=11111111111111
Connecting (http): example.com:80
[2016-05-10 | 02:26:50: Opened: 2]
Status: 200
2
http_head
Abbreviation
hhe
Description
Perform an HTTP(S) HEAD request and return a network stream handle if successful.
The protocol is assumed to be HTTP unless otherwise specified in the <url>
parameter.
To allow custom headers, use the -o
option.
Timeout is determined by tcp.client.connect_timeout.
See:
Syntax
> http_head [-i <wlan/softap>] -o <url> [ca_cert_filename]
where:
Parameter | Description |
---|---|
-i | Network interface. Possible values are wlan or softap . Overrides default specified by network.default_interface |
-o | Open the HTTP request but do not send. This enables custom header(s) to be added to the request using the http_add_header command. |
<url> | URL to which request is sent. The URL prefix http:// is optional for standard HTTP transactions, however https:* must be added for secure HTTPS transactions. |
[ca_cert_filename] | CA certificate file. Overrides default specified by network.ca_cert |
Options must be provided in the order shown.
Platforms
- AMW007
Example
> hhe example.com
[2014-04-02 | 13:32:28: Connecting: example.com]
Request HEAD /
Connecting (HTTP): example.com:80
[2014-04-02 | 13:32:29: Connected: 0]
HTTP response: 200
Status: 200
0
http_post
Abbreviation
hpo
Description
Perform an HTTP(S) POST request and return a network stream handle if successful.
The protocol is assumed to be HTTP unless otherwise specified in the <url>
parameter.
To allow custom headers, use the -o
option.
The HTTP Content-type must be provided.
Timeout is determined by tcp.client.connect_timeout.
See:
Syntax
> http_post [-i <wlan/softap>] [-g < GPIO#>] [-o] [-l <content-length>] <url> / --long_url<url> <content type> [ca_cert_filename]
where:
Parameter | Description |
---|---|
-i | Network interface. Possible values are wlan or softap . Overrides default specified by network.default_interface |
-o | Open the HTTP request but do not send. This enables custom header(s) to be added to the request using the http_add_header command. |
-l <content-length> | This replaces the default HTTP header Transfer-Encoding : chunked with the header Content-Length: XXX where XXX is the specified content_length .By default an HTTP request is sent with chunked encoding. If this option is specified then chunked encoding is not used. This may be necessary for HTTP servers that do not support chunked encoding. After issuing the command, the write command must be used to write <content-length> bytes of data.Note: If the -l option is specified then the connection will be left open, thus the -o option is not needed. |
<url> | URL to which request is sent. The URL prefix http:// is optional for standard HTTP transactions, however https:* must be added for secure HTTPS transactions. |
--long_url <url> | allows an aribitrary length URL string, with a maximum length of 1023 characters. The URL string follows the http_post command on the next line |
<content_type> | The Content-type, (Internet media type, MIME type), of the content to be posted (e.g. application/json ). |
[ca_cert_filename] | CA certificate file. Overrides default specified by network.tls.ca_cert |
Options must be provided in the order shown.
Platforms
- AMW007
Example
> hpo http://example.com application/json
[2014-04-02 | 13:35:19: Connecting: http://example.com]
Request POST /
Connecting (HTTP): example.com:80
[2014-04-02 | 13:35:20: Connected: 0]
HTTP response: 411
Status: 411
0
> hpo -o example.com:80 application/json
[2014-04-11 | 10:45:50: Opening: example.com:80]
Request POST /
Connecting (HTTP): example.com:80
[2014-04-11 | 10:45:50: Opened: 1]
1
http_read_status
Abbreviation
hre
Description
Read the HTTP response code returned by the last HTTP transaction on the stream specified by <handle>
. If the HTTP request is pending and the transaction is incomplete, http_read_status
sends the request and forces completion.
See Networking and Security, HTTP Client.
Syntax
> http_read_status <handle>
Platforms
- AMW007
Example
> hre 1
411
http_upload
Abbreviation
hup
Description
Upload file(s) from the device flash to a remote HTTP server using HTTP POST and file upload.
Timeout is determined by tcp.client.connect_timeout.
See:
Syntax
Upload a Single File
> http_upload [-i <softap/wlan>] <url> <local filename>
[<remote filename> [<content type>]]
where:
-i
- optional, specify interface, value 'wlan' or 'softap' MUST come first. If omitted uses network.default_interface.<url>
- URL of remote HTTP server<local filename>
- name of file on sflash to upload<remote filename>
- optional, name of file on remote server, use local filename if omitted.<content type>
- optional, HTTP header content-type, e.g.image/jpeg
Upload Multiple Files using JSON Manifest
> http_upload [-i <softap/wlan>] -m <json size>
where:
-i
- optional, specify interface, value 'wlan' or 'softap' MUST come first-m
- use JSON manifest for multi-file upload. MUST come first if-i
option not used
The manifest must be input directly after the command is issued. Manifest format:
{
"path" : "https://myserver.com/path/to/save/files",
"cert" : "mycert.pem",
"files" : [ {
"local" : "my_file_to_load.txt",
"remote" : "file_name_on_server.txt",
"name" : "file",
"type" : "application/octet-stream",
},
{ ... }
]
}
The manifest cannot contain javascript style commments.
If provided, the cert
must be the name of an existing file in the device sflash.
The following optional properties are given the specified default values only if the properties are completely omitted from the manifest. Leaving them blank results in blank values, not default values.
Property | Description | Default |
---|---|---|
remote | Name of file on remote system | local value - the name of the file on the module file system. |
name | Appears in the form-data "name" field | "file" |
type | Mime-type of file content | "application/octet-stream" |
For examples, see the http_upload application note.
Platforms
- AMW007
Example
> hup http://myserver.com/uploadpage ghm_capabilities.json testfile.json
Uploading: ghm_capabilities.json to server
Request POST /uploadpage
Connecting (http): myserver.com:80
HTTP response: 200
Success
The file is saved on the upload server at myserver.com:80
as testfile.json
ls
Abbreviation
ls
Description
Return a list of available files located in internal, extended and bulk flash.
Use the -v
(or equivalent -l
) option for full details.
The -m
, -b
and -c
support paging and limiting the output, for use when there are many files.
Syntax
> ls [-v/-l] [-m <i|e|b>] [-b <base sector>] [-c <max file count>]
where:
-m
the memory type to search. This is a concatenation of one or more of the following types:i
- internale
- extendedb
- bulk
-b
the lowest number file handle (Hnd) at which to begin searching for files on the given memories.-c
the max file count to return
Properties
- available in Safe Mode
Platforms
- AMW007
Example
Long listing, showing Type, Flags, and Handles (Hnd)
> ls -l
! # Type Flags Hnd Size Version Filename
# 0 e-FE 0041 54 7590 3.3.2.6 .recovery.html
# 1 e-FB 0001 85 44560 3.0.0.6 command_help.csv
# 2 e-FD 0001 62 135 3.0.0.6 default_setup.script
# 3 e-FE 0001 96 5430 3.3.2.6 favicon.ico.gz
# 4 e-03 0001 63 1216 3.0.0.6 geotrust_ca.pem
# 5 i-00 001B 170 327424 3.3.2.6 sys/kernel.bin
# 6 e-84 0005 52 820 3.2.0.0 sys/safemode.bin
# 7 i-81 001B 0 166096 3.3.2.6 sys/services.bin
# 8 e-01 0001 0 210412 5.26.230.12 sys/wifi_fw.bin
# 9 e-FE 0021 97 684 1.0.0.0 test1.html
# 10 e-FE 0001 53 1995 3.3.2.6 webapp/index.html
# 11 e-FE 0001 64 9530 3.3.2.6 webapp/unauthorized.html
# 12 e-FE 0001 56 22720 3.3.2.6 webapp/gecko-os.css.gz
# 13 e-FE 0001 67 72947 3.3.2.6 webapp/gecko-os.js.gz
Example
Listing showing extended memory files only, starting at file handle 56, count limited to 5 files:
> ls -l -m e -b 56 -c 5
! # Type Flags Hnd Size Version Filename
# 0 e-FE 0001 56 22720 3.3.2.6 webapp/gecko-os.css.gz
# 1 e-FD 0001 62 135 3.0.0.6 default_setup.script
# 2 e-03 0001 63 1216 3.0.0.6 geotrust_ca.pem
# 3 e-FE 0001 64 9530 3.3.2.6 webapp/unauthorized.html
# 4 e-FE 0001 67 72947 3.3.2.6 webapp/gecko-os.js.gz
>
load
Abbreviation
load
Description
Load a configuration from a file previously saved by the save command.
Syntax
> load [-v] <config_file>
where:
-v
: verbose: displays information including the set command for each variable and the corresponding result
Platforms
- AMW007
Example
> load config1.cfg
> Configuration successfully loaded
network_down
Abbreviation
ndo
Description
Bring down a network interface. If provided, the network interface overrides the default specified by the variable network.default_interface
. All open streams on the interface will be closed.
Syntax
> network_down [-i <wlan/softap>]
Platforms
- AMW007
Example
> ndo
L000040
[2014-03-24 | 00:08:48: Disassociated]
R000009
Success
network_lookup
Abbreviation
nlo
Description
Perform a DNS lookup for a domain using the specified interface.
Syntax
> network_lookup [-i <wlan/default>] <domain>
where:
-i
: optionally specify the network interface:wlan
: WLANdefault
: Use the default interface as specified by network.default_interface.
<domain>
: the domain to resolve into an IP address.
Platforms
- AMW007
Example
> nlo google.com
R000016
216.58.220.142
network_restart
Abbreviation
nre
Description
Restart the network. This command is equivalent to issuing the network_down command followed by the network_up command.
Note: This command is blocking. It does not return until the network has been brought up (or has failed to be brought up).
Syntax
> network_restart [-i <softap/wlan>]
where the -i
option specifies the network interface to be restarted.
Platforms
- AMW007
Example
The response shown is an example. Response varies depending on the network settings, time and date and other factors.
> nre
[2015-03-23 | 03:02:53: Disassociated]
[2015-03-23 | 03:02:53: Associating to Silabs]
Obtaining IPv4 address via DHCP
IPv4 address: 10.5.6.55
[2015-03-23 | 03:02:54: Associated]
Success
network_up
Abbreviation
nup
Description
Start the process to bring up a network interface.
The -s
option prompts the user to select from a list of available APs and supply a passkey. If the -s
option is used, Gecko OS automatically saves the credentials entered.
The -i
option overrides the default network interface specified by network.default_interface.
NOTE! Every command that needs access to the network will automatically bring up the network interface.
The network_up command is non-blocking (except when the -s
option is used) and provided for convenience only.
Syntax
> network_up [<-s> / <-i [wlan]/[softap]>]
Platforms
- AMW007
Example
> network_up -s
Scanning for networks...
! 3 networks found
! # Ch RSSI MAC (BSSID) Network (SSID)
# 0 6 -27 84:1B:5E:29:9D:F7 Take the blue pill
# 1 11 -68 EC:1A:59:36:5B:6C button_xt
# 2 11 -70 2C:B0:5D:31:6F:6A button
Type the number # that matches your Network: 0
Type the password for your Network : welcome-to-kansas
[Associating to Take the blue pill]
In progress
[Associated]
ota
Abbreviation
ota
Description
Note: This command is deprecated and will be removed in future versions. Use dfu_update and dfu_query instead.
Initiate a secure over-the-air update. The secure OTA protocol uses industry standard TLS/HTTPS security with both client-side and server-side certificate verification.
For details of this process and associated requirements, see Update and Recovery, Secure OTA Update. This process requires you to claim the device using the dms_claim command.
As an additional measure of security, the server authenticates each device using the universally unique system.uuid embedded inside the hardware of each device.
Downloaded bundle files overwrite local files only if the bundle file has a later version. To ensure that bundle files overwrite local files regardless of version, force an update with the -f
option.
Download a specific firmware bundle version with the -b
option. Specifying a bundle forces an update. Bundle files overwrite local files regardless of version. See the note for the -b
option in Syntax below.
To maintain a saved configuration through an OTA update, save the configuration as default_config.csv
.
Note: OTA requires a memory-intensive TLS connection, and may fail if memory is low. See Networking and Security, Increasing Available Memory for TLS.
Note: If the ota
command fails with the message:
{"result":"fail","message":"device not claimed"}
then you need to claim the device before running the ota
command. See Update and Recovery, the Silabs DMS Server.
Syntax
> ota [-q] [-f] [-b <full version>]
-q
: query database and return eitherUp-to-date
or bundle version string if newer release available. Must be the only option. Result codes and messages are:204, Up-to-date
200, <DMS generated bundle string version>
e.g.
-f
: force update. Bundle files overwrite local files, regardless of version.-b
: download a specified bundle, for example a previous version. For a Gecko OS bundle, specify only the full version number, e.g.ota -b 2.0.4
. For full versions of Gecko OS by platform, see DMS Products. For full versions of custom product bundles, refer to the DMS Products list for that product.- Note: the
-b
option is available only when you are updating a development product. From the moment you load a production product on your device, the device canota
only to the most recent release of the product, corresponding to the device's product release type (alpha, beta or release).
- Note: the
Properties
- available in Safe Mode
Platforms
- AMW007
Example
> ota
Connecting to network
Request POST /ota/05b300df003134534e394b8330393232323a3533/0
Connecting (HTTP): ota.zentri.com:443
Starting TLS
HTTP response: 200
Downloading new firmware...
Bundle version: Gecko OS-1.0.0.1, Built:2015-11-11 02:23:15 for AMW004.3
Downloading: command_help.csv-1.0.0.1 (25822, 0xFB, 0x1)
Downloading: default_setup.script-1.0.0.1 (189, 0xFD, 0x9)
Downloading: /setup/index.html-1.0.0.1 (9266, 0xFE, 0x1)
Downloading: /setup/images.png-1.0.0.1 (18067, 0xFE, 0x1)
Downloading: /sys/kernel.bin-1.0.0.1 (352804, 0x0, 0x801F)
Downloading: wifi_fw.bin-1.0.0.1 (191677, 0x1, 0x8009)
Downloading: /sys/services.bin-1.0.0.1 (83848, 0x80, 0x801F)
Downloading: geotrust_ca.pem-1.0.0.1 (1162, 0x3, 0x9)
Downloading: /favicon.ico.gz-1.0.0.1 (1853, 0xFE, 0x1)
Downloading: /setup/index.css.gz-1.0.0.1 (10539, 0xFE, 0x1)
Downloading: /setup/index.js.gz-1.0.0.1 (38771, 0xFE, 0x1)
Updating kernel to version: 1.0.0.1
Updating firmware files...
Updating file: wifi_fw.bin to version: 1.0.0.1
Updating file: /sys/services.bin to version: 1.0.0.1
Found new bootable app: /sys/services.bin (47), booting to it now!
OTA completed successfully
[Ready]
ping
Abbreviation
ping
Description
Send one or more ICMP pings to an IP address
or the network gateway using the -g
option. If provided, the network interface overrides the default specified by the variable network.default_interface
. Options must be provided in the order shown.
Syntax
> ping [-i <wlan/softap>] <[IP address]/[-g]> [# retries]
Platforms
- AMW007
Example
> ping example.com 3
R000021
Ping reply in 183ms
R000021
Ping reply in 178ms
R000021
Ping reply in 177ms
reboot
Abbreviation
reboot
Description
Reboot the application.
Note: the response displayed on reboot depends on the system.cmd.format setting.
In human
command mode, the response is similar to:
Rebooting
[2015-08-05 | 00:38:19: Disassociated]
Gecko OS-2.3.1.2, Built:2015-07-21 09:16:43 for AMW004.3, Board:AMW004-E03.3
[Ready]
There may be other messages depending on system settings.
In machine
command mode, the response to the reboot
command, followed by the reboot and a CR-LF
sequence, is similar to:
R000079
Gecko OS-2.3.1.2, Built:2015-07-21 09:16:43 for AMW004.3, Board:AMW004-E03.3
Syntax
> reboot
Properties
- available in Safe Mode
Platforms
- AMW007
Example
> reboot
Rebooting
[2015-08-05 | 00:38:19: Disassociated]
Gecko OS-2.3.1.2, Built:2015-07-21 09:16:43 for AMW004.3, Board:AMW004-E03.3
[Ready]
save
Abbreviation
save
Description
Save all Gecko OS variables to non-volatile flash memory.
If a file name is supplied, the saved configuration can be restored with the load command.
Note: During the save operation, interrupts are disabled. In particular, the UART rx interrupt may not be serviced during save. To ensure the save operation is completed, wait for the save command response before issuing further commands via the UART.
Syntax
> save [<config_file>]
where parameters are as follows:
Option | Description |
---|---|
<config_file> | Optional. Name of the configuration file to be saved |
Properties
- available in Safe Mode
Platforms
- AMW007
Example
> save
L000007
Saved
R000009
Success
Example 2
save config1.cfg
R000009
Success
ls
! # Size Version Filename
...
# 5 3868 1.0.0 config1.cfg
...
set
Abbreviation
set
Description
Set the value of a Gecko OS variable.
Syntax
> set <variable> <args>
Note: The set
command displays the Too many args
error only if the number of space-separated arguments exceeds the maximum for all variables (5). However the number of arguments for the set
command depends on the variable being set, and the form in which the variable is specified: abbreviations for variables vary from one to three arguments in length, and variable settings may require one or two arguments. If you specify too many arguments when setting a specific variable, surplus arguments are ignored. Refer to the variable documentation for the number of arguments for a specific variable.
Properties
- available in Safe Mode
Platforms
- AMW007
Example
> set wlan.ssid "My Home Network"
R000008
Set OK
setup
Abbreviation
setup
Description
Note: The setup web
option of this command is deprecated and will be removed in future versions. Use setup_web instead.
The setup command simplifies the process of connecting a Gecko OS device to a Wi-Fi network.
It can be run automatically on boot or in response to asserting a GPIO. It also allows for setup from the Gecko OS terminal.
The setup command allows for setting up network credentials via a web browser. See Configuration and Setup, Setup with a Web Browser.
Syntax
> setup <web/status/stop>
Option | Description |
---|---|
web | When called with the web option, setup starts a Wi-Fi Access Point and a web server, the Wi-Fi AP credentials are configured using the variables setup.web.ssid and setup.web.passkey . Once connected to the Gecko OS Setup AP, a Wi-Fi client uses a web browser to setup Gecko OS variables and connect to your local Wi-Fi network. Web setup is non-blocking. The root of the web app is configured with the setup.web.root_filename variable. |
status | The status option allows an MCU host to determine whether setup is in-progress. Response is 1 if setup is in progress, otherwise 0 . |
stop | The stop option terminates any in-progress setup activity. |
Platforms
- AMW007
Example
Setup via Soft AP and Web App
> setup_web
In progress
Rebooting
SILABS-AMW007-2.0.0.4, 2018-08-18T05:32:24Z, Gecko-OS-2.0.0.4, Board:AMW007-E03.2
While In progress
is displayed, connect a computer or mobile device to Soft AP, enter password (default password
), in web browser go to web setup DNS (default setup.com
), choose network from scan list and enter network password. See
setup_web
Abbreviation
setupw
Description
The setup_web
command simplifies the process of connecting a Gecko OS device to a Wi-Fi network.
It can be run automatically on boot or in response to asserting a GPIO.
The setup_web
command allows for setting up network credentials via a web browser. See Configuration and Setup, Setup with a Web Browser.
The setup_web
command starts a Wi-Fi Access Point and a web server, the Wi-Fi AP credentials are configured using the variables setup.web.ssid
and setup.web.passkey
. Once connected to the Gecko OS Setup AP, a Wi-Fi client uses a web browser to setup Gecko OS variables and connect to your local Wi-Fi network. Web setup is non-blocking. The root of the web app is configured with the setup.web.root_filename variable.
Syntax
> setup_web [status/stop]
Option | Description |
---|---|
status | The status option allows an MCU host to determine whether setup_web is in-progress. Response is 1 if setup is in progress, otherwise 0 . |
stop | The stop option terminates any in-progress setup_web activity. |
Platforms
- AMW007
Example
> setup_web
In progress
Rebooting
SILABS-AMW007-2.0.0.4, 2018-08-18T05:32:24Z, Gecko-OS-2.0.0.4, Board:AMW007-E03.2
While In progress
is displayed, connect a computer or mobile device to Soft AP, enter password (default password
), in web browser go to web setup DNS (default setup.com
), choose network from scan list and enter network password. See Web App, Setup Web.
sleep
Abbreviation
sleep
Description
Put the application into a low-power sleep state. The application sleeps until the wakeup timeout (system.wakeup.timeout) expires.
Syntax
> sleep
Platforms
- AMW007
Example
> set system.wakeup.timeout 10
Set OK
> sleep
... wait 10 seconds ...
SILABS-AMW007-2.0.0, Gecko_OS-2.0.0, AMW007-W0001
stream_close
Abbreviation
close
Description
Close an open network or file stream specified by [handle]
, or alternatively close all open streams.
See Networking and Security, Network Connections and Streams.
Syntax
> stream_close <[handle]/[all]>
Platforms
- AMW007
Example
> close all
[2014-04-02 | 13:32:04: Disconnected: 0]
[2014-04-02 | 13:32:04: Disconnected: 1]
Success
stream_list
Abbreviation
list
Description
Return a list of open streams.
See Networking and Security, Network Connections and Streams.
Syntax
> stream_list
Platforms
- AMW007
Example
> list
!# Type Info
#0 TCPC google.com:80 (32288)
#1 HTTP example.com:80 (37289)
stream_poll
Abbreviation
poll
Description
Poll a stream to check if data is available. Returns 0 if open with no data to read, 1 if data is available and 2 if the stream has been closed remotely. Use the all
option to return the status of all open streams. To avoid polling, use a GPIO (may be assigned when the stream is opened) as an interrupt line to the host.
Determine the number of RX or TX bytes that can be buffered with the -r
or -t
arguments.
Syntax
> stream_poll [all] <handle> [-r]
where:
-c
- Deprecated - response includes number of Rx bytes available. Use-r
instead.-r
- response includes number of Rx bytes available: the number of bytes that can be immediately returned by the read command
If -r
argument is included in the command, the response format is as follows:
Poll specific connection
> poll 0 -r
<status>,<Rx bytes available>
Poll all connections
> poll all -r
<handle>,<status>,<Rx bytes available>|<handle>,<status>,<Rx bytes available>|...
where:
<handle>
- stream handle<status>
-0
- no data available1
- data available2
- remote closed connection
<bytes available>
- the total number of bytes that can be buffered
Platforms
- AMW007
Example
> poll 0
1
> read 0 100
hello!
> poll 0
0
> poll all
0,0|2,1|3,1
stream_read
Abbreviation
read
Description
Read up to <size>
bytes from a network or file stream specified by <handle>
. Returns data immediately (if available), does not wait to receive data.
To check for data, use the stream_poll command or the GPIO (assigned when the stream was opened) as an interrupt line to the host.
For file streams, the file is automatically closed if the end of file is reached.
Data Size Returned by stream_read
The stream_read
command size
parameter is limited to a maximum of 1000
bytes. If a larger size
parameter is specified, stream_read
returns only 1000
bytes.
See Networking and Security, Network Connections and Streams.
Syntax
> stream_read <handle> <size>
where
<handle>
is the stream handle number returned by the command that opened the stream<size>
is the bytes to read. Effective maximum:1000
. See Data Size Returned by stream_read above.
Platforms
- AMW007
Example
> read 0 200
R000202
<!doctype html><html itemscope="" itemtype="http://schema.org/WebPage"
lang="en-AU"><head><meta content="/images/google_favicon_128.png"
itemprop="image"><title>Google</title><script>(function(){
wind
stream_write
Abbreviation
write
Description
Write data to a network or file stream. As described in Serial Interface, Command Protocol, the command must be terminated by \r\n
.
If no option is specified, Gecko OS waits for <size>
number of data bytes then immediately sends the data to the stream before returning a response.
If the -f
(flush) option is specified, then the written data is buffered to the maximum packet size before being automatically flushed to the remote side.
The -f
option can be used for the following stream types:
- TCP client/server
- TLS client/server
For TCP and TLS streams, the maximum packet size is an MTU (1460 bytes).
See Networking and Security, Network Connections and Streams.
Syntax
> stream_write <handle> <size> [-f]
where:
<handle>
: previously opened stream handle<size>
: the size of the data to be written to the stream-f
: optional. Buffer to maximum packet size before flushing, as described above.-c
: optional. Enable automatic continuation frames for large writes to WebSocket client/server streams. Writes greater than 1460 are chunked with the websocket 'continuation frame' flag set; the last chunk has the 'final frame' flag set.
Platforms
- AMW007
Example
> write 3 10
Success
tcp_client
Abbreviation
tcpc
Description
Open a TCP stream to a remote server at the specified network location.
Timeout is determined by tcp.client.connect_timeout.
See Networking and Security, Network Connections and Streams.
Note: You cannot use the tcp_client
command to open a stream when tcp.client.auto_start is enabled. See the tcp.client.auto_start description and note.
Syntax
> tcp_client [-i <wlan/softap>] [-l <local port>] [-g GPIO#] <host> <port>
where:
-i
- specify interface. MUST come first. If omitted uses network.default_interface.-l
- optionally specify<local port>
. If not specified local port is random unused port-g GPIO#
- specify a GPIO to indicate buffered data is waiting to be read. Set to-1
to disablehost
- specify the remote host. If value is0
, orhost
omitted, use the host value in tcp.client.remote_host.port
- specify the remote port. If value is0
, orport
omitted, use the port value in tcp.client.remote_port.
Options must be provided in the order shown.
Platforms
- AMW007
Example
> tcpc google.com 80
L000028
Resolving host: google.com
L000052
[2014-03-24 | 01:07:12: Connecting: google.com:80]
L000036
Connecting (TCP): 74.125.237.96:80
L000039
[2014-03-24 | 01:07:12: Connected: 0]
R000003
0
tcp_server
Abbreviation
tcps
Description
Start/stop a TCP server specified by the variables tcp.server.*
. If provided, the network interface and port override defaults specified by the variables network.default_interface
and tcp.server.port
respectively.
Syntax
> tcp_server [-i <wlan/softap>] <start/stop> [port]
where:
-i
- specify interface. MUST come first. If omitted uses network.default_interface.start/stop
start
- start the serverstop
- stop the server
port
: (optional) Specify port. If value is0
, orport
omitted, use the port value in tcp.server.port.
Options must be provided in the order shown.
See Networking and Security, Network Connections and Streams.
Platforms
- AMW007
Example
> tcps start
L000036
TCP server listening on port: 3000
R000009
Success
tls_client
Abbreviation
tlsc
Description
Open a secure TCP stream to a remote server with the specified properties.
Timeout is determined by tcp.client.connect_timeout.
See Networking and Security, Network Connections and Streams.
Syntax
> tls_client [-i <wlan/softap>] [-l <local_port>] <host> <port> [ca_cert_filename]
where:
-i
- specify interface. MUST come first. If omitted uses network.default_interface.-l
- optionally specify<local port>
. If not specified local port is random unused port-g GPIO#
- specify a GPIO to indicate buffered data is waiting to be read. Set to-1
to disable.host
- specify the remote host. If value is0
, orhost
omitted, use the host value in tcp.client.remote_host.port
- specify the remote port. If value is0
, orport
omitted, use the port value in tcp.client.remote_port.[<ca cert filename>]
- if omitted, use network.tls.ca_cert
Platforms
- AMW007
Example
> tlsc www.google.com 443
L000032
Resolving host: www.google.com
L000057
[2014-03-24 | 01:15:53: Connecting: www.google.com:443]
L000038
Connecting (TLS): 74.125.237.211:443
L000039
[2014-03-24 | 01:15:55: Connected: 1]
R000003
1
uart_update
Abbreviation
uartu
Description
Update the UART to the current UART variable settings without rebooting the device.
For this command to have an effect, the values of one or more of the uart variables must first be changed:
Syntax
> uart_update <uart#>
Platforms
- AMW007
Example
> uart_update 0
Success
udp_client
Abbreviation
udpc
Description
Open a UDP stream to a remote server at the network location <host>:<port>
. If provided, the network interface overrides the default specified by the variable network.default_interface
.
The option -g GPIO#
specifies which GPIO indicates buffered data is waiting to be read. See also system.oob.gpio.
The [local port]
may also be provided if desired. Options must be provided in the order shown.
See Networking and Security, Network Connections and Streams.
Syntax
> udp_client [-i wlan/softap] [-g GPIO#] <host> <remote port> [local port]
Platforms
- AMW007
Example
> udpc 192.168.45.67 3000
L000057
[2014-03-24 | 01:16:40: Connecting: 192.168.45.67:3000]
L000031
Resolving host: 192.168.45.67
L000032
Connecting: 192.168.45.67:3000
L000039
[2014-03-24 | 01:16:40: Connected: 2]
R000003
2
udp_server
Abbreviation
udps
Description
Start and stop the UDP server.
When the UDP server is started the read
and write
sub-commands are available.
When the UDP server is started, it is assigned a stream handle, indicated in the Gecko OS response by Opened: <stream>
.
This allows for the equivalent stream read and write commands.
The read command is functionally the same as udps read
.
The write command is functionally the same as udps write
without the <address>
and <port>
options. The write command writes to the single UDP server stream, and consequently writes to all clients connected to the UDP server.
See:
Syntax
start, stop
> udp_server <start/stop> [port]
Start and stop the UDP server. Port may be optionally specified. If no port is specified the default is udp.server.port.
read
> udp_server read [-q] [<byte_count>]
where :
-q
- optionally prepend the client's IP address and port before the data bytes, in a comma-separated list:ip,port,data
<byte_count>
- The number of bytes to read. Note that only a single packet's worth of data is returned
i.e. data returned = MIN(<byte count>
, len(packet))
write
> udp_server write <byte_count> [<address> <port>]
where :
<byte_count>
- the number of data bytes to write<address>
,<port>
- optional, the remote client's address and port. If omitted, write to last client whose data has been read.
Platforms
- AMW007
Example
> udp_server start 5000
[2014-11-28 | 07:14:49: Opened: 0]
0
UDP server listening on port: 5000
> read 0 100
Hello server
> udp_server write 12
Hello client
Success
> udp_server read -q 100
10.5.6.60,52333,Hello again server
> write 0 18
Hello again client
Success
> udps stop
[2014-11-28 | 07:15:31: Closed: 0]
UDP server stopped
Success
version
Abbreviation
ver
Description
Returns the Gecko OS firmware bundle version. This is a convenience command that is equivalent to reading the system.version
variable.
Syntax
version
Properties
- available in Safe Mode
Platforms
- AMW007
Example
> ver
R000052
SILABS-AMW007-2.1.5, Gecko OS-2.1.5, AMW007-W00001
wlan_get_rssi
Abbreviation
rssi
Description
Get the received signal level (RSSI, in dBm) of the Access Point the wlan interface is connected to.
Syntax
> wlan_get_rssi
Platforms
- AMW007
Example
> rssi
R000005
-47
wlan_scan
Abbreviation
scan
Description
Initiate a Wi-Fi scan and return results; optionally specify a channel and AP SSID to scan for. For verbose scans, -v must be the first argument. Information returned by scan results is described in the following table.
Name | Description |
---|---|
Ch | The WLAN radio channel the AP is operating on |
RSSI | Signal strength of the AP in units of dBm |
BSSID | MAC address of the AP |
Rate | The maximum data rate supported by the AP in kilobits/s |
0 = not supported | |
e.g. 54000 = 54Mbit/s | |
Security | Security type used by the AP e.g. Open, WPA2-AES, etc. |
Mode | AP mode. Inf = Infrastructure, Ad = Ad-hoc, |
- = not supported | |
Len | Number of characters in the SSID |
SSID | AP name. APs with a hidden SSID are displayed as |
Verbose scans return all columns of data.
Non-verbose scans return only columns:# Ch RSSI MAC (BSSID) Network (SSID)
In Gecko OS, the Rate and Mode columns are not supported. These columns are filled with the values of 0
and -
respectively.
Syntax
> wlan_scan [-v] [<channel-spec> [ssid]]
where:
-v
: verbose scan - must be first argument<channel-spec>
- can be one of the following:- channel: a specific channel, e.g.
scan 5
all
: all channels, e.g.scan -v all
- channel: a specific channel, e.g.
Platforms
- AMW007
Example
> scan -v
R000196
! 2 found
! # Ch RSSI BSSID Rate Security Mode Len SSID
# 0 01 -24 EC:1A:59:36:5B:6C 0 Open - 13 Ch1_Nearby_AP
# 1 06 -85 84:1B:5E:29:9D:F7 0 WPA2-AES - 14 Ch6_Distant_AP
hboot
Abbreviation
hboot
Description
The host boot command downloads a firmware image from the Gecko OS device file system to the host MCU. If a firmware filename is not supplied, hboot
downloads the default firmware image set in the hboot.filename variable.
The download process uses the EFM8 Factory Bootloader protocol described in AN945 EFM8 Factory Bootloader User Guide.
See also: hboot.filename variable.
Syntax
> hboot [<filename>]
where:
<filename>
: Name of firmware image to download from the Gecko OS device file system to the host MCU. If a filename is not supplied, downloads the default firmware image set in the hboot.filename variable.
Platforms
- AMW007
Example
> hboot EFM8/UB1/SpaceInvaders.efm8
Success