HTTP Server
http.server.api_enabled
Abbreviation
ht s a
Access
get/set
Description
Enable the HTTP Server RESTful API.
See Networking and Security, HTTP Server.
The API is enabled by default, so enabling the HTTP server with http.server.enabled also allows access to the API. To disable HTTP RESTful API calls when the HTTP server is running, set http.server.api_enabled
to 0
.
Arguments
<0/1>
Default
1
Platforms
- AMW007
Get example
> get http.server.api_enabled
1
Set example
> set ht s a 0
Set OK
http.server.cors_origin
Abbreviation
ht s c
Access
get/set
Description
Specifies origins for which the web browser same-origin policy is relaxed.
If <origin>
is set to an empty string, then CORS is completely disabled.
For requests without credentials, a value of *
acts as a wildcard, allowing any origin to access the resource.
See HTTP Server RESTful API, CORS.
Arguments
<origin>
Default
""
(empty string). To set the http.server.cors_origin
variable to the empty string, supply an argument with two double quotes: ""
Platforms
- AMW007
Get example
> get http.server.cors_origin
Set example
> set ht s c *
Set OK
http.server.enabled
Abbreviation
ht s e
Access
get/set
Description
Enable the HTTP server.
See Networking and Security, HTTP Server.
Arguments
<1/0>
Default
0
Platforms
- AMW007
Get example
> get ht s e
0
Set example
> set ht s e 1
Set OK
http.server.interface
Abbreviation
ht s i
Access
get/set
Description
Specifies the network interface used by the HTTP server.
See Networking and Security, HTTP Server.
Arguments
<default/softap/wlan>
Default
default
Platforms
- AMW007
Get example
> get http.server.interface
default
Set example
> set ht s i wlan
Set OK
http.server.max_clients
Abbreviation
ht s m
Access
get/set
Description
Specifies the maximum number of clients the HTTP server allows to connect.
Restricting connected clients may be necessary to limit memory usage. See Memory.
See Networking and Security, HTTP Server.
Arguments
<clients>
Default
3
Range: 1 - 8
Platforms
- AMW007
Get example
> get http.server.max_clients
3
Set example
> set ht s m 1
Set OK
http.server.notfound_filename
Abbreviation
ht s n
Access
get/set
Description
Specifies the filename of the web page to be displayed in the event that the HTTP server reports a 404 - not found error.
<filename>
See Networking and Security, HTTP Server.
Default
''
Platforms
- AMW007
Get example
> get http.server.notfound_filename
Set example
> set ht s n notfound.html
Set OK
http.server.port
Abbreviation
ht s p
Access
get/set
Description
Set the port on which the HTTP server listens.
See Networking and Security, HTTP Server.
Arguments
<listening port>
Default
80
Platforms
- AMW007
Get example
> get ht s p
80
Set example
> set http.server.port 8080
Set OK
http.server.root_filename
Abbreviation
ht s r
Access
get/set
Description
This sets or gets the root file of the HTTP server. If a plain request to
See Networking and Security, HTTP Server.
Arguments
<filename>
Default
/setup/index.html
Platforms
- AMW007
Get example
> get ht s r
/setup/index.html
Set example
> set http.server.root_filename /setup/home.html
Set OK