Host Boot
hboot.filename
Abbreviation
hb f
Access
get/set
Description
Set the default value of the host boot filename.
See hboot command.
Arguments
<filename>
where filename
is name of the firmware file from which to boot.
Default
host_firmware.bin
Properties
Get example
> get hb f
R000019
host_firmware.bin
Set example
> set hb f EFM8/UB1/SpaceInvaders.efm8
R000008
Set OK
hboot.gpio
Abbreviation
hb g
Access
get/set
Description
Set the host boot GPIO.
See hboot command.
Arguments
<GPIO#>
where GPIO#
is the number of an available GPIO.
Set to -1
to disable the host boot GPIO.
Default
-1
Properties
Get example
> get hb g
R000004
-1
Set example
> set hb g 3
R000008
Set OK