Bus
bus.command.rx_bufsize
Abbreviation
bu c r
Access
get/set
Description
Configure the size of the UART rx buffer in command mode.
Arguments
<buffer size>
Default
256
(bytes)
Range 256 to 10000 bytes
Properties
Get example
> get bu c r
R000005
256
Set example
> set bu c r 512
R000008
Set OK
bus.command.tx_bufsize
Abbreviation
bu c t
Access
get/set
Description
Configure the size of the UART tx buffer in command mode.
Arguments
<buffer size>
Default
256
(bytes)
Range 256 to 10000 bytes
Get example
> get bu c t
R000005
256
Set example
> set bu c t 512
R000008
Set OK
bus.mode
Abbreviation
bu m
Access
get/set
Description
The serial bus mode.
Arguments
<command/stream>
Default
command
Properties
- save and reboot to apply change
- available in Safe Mode
- preserved by NVM Backup
Get example
> get bu m
R000009
command
Set example
> set bu m command
R000008
Set OK
bus.stream.cmd_gpio
Abbreviation
bu s g
Access
get/set
Description
The GPIO used to force the module into command mode (from stream mode). A value of -1 disables this feature.
Arguments
<[GPIO#]/[-1]>
Default
0
Properties
Get example
> get bu s g
R000003
0
Set example
> set bu s g 6
R000008
Set OK
bus.stream.cmd_seq
Abbreviation
bu s s
Access
get/set
Description
Break-in sequence for stream mode. After 3 seconds of inactivity on the serial interface, sending the break-in sequence changes stream mode to command mode; send 'exit' to return to stream mode.
Note: The length of the break-in sequence affects the allowed minimum value of bus.stream.flush_count.
This feature may be disabled with the following command:
set bus.stream.cmd_seq ""
When disabled, the break-in sequence is disabled. This allows for binary data streams or for any streams which may be interpreted incorrectly as the break-in sequence.
Note: If this feature is disabled it's strongly recommended to enable bus.stream.cmd_gpio and/or another remote command feature, such as the remote terminal or the Web App.
Otherwise the Gecko OS command console will be inaccessible until the module is factory reset.
Arguments
<1-15 characters>
Default
$$$
Properties
Get example
> get bu s s
R000005
$$$
Set example
> set bu s s ###
R000008
Set OK
bus.stream.flush_count
Abbreviation
bu s c
Access
get/set
Description
Number of bytes received on the serial bus before flushing to the network stream.
Arguments
<count>
where <count>
can range from minimum value to maximum value:
- minimum value:
MAX(16, len(bus.stream.cmd_seq)*2)
i.e. the minimum value is the maximum of 16 and 2 x the length of the bus.stream.cmd_seq variable
For example, ifbus.stream.cmd_seq
is the default$$$
, its length is 3, so minimum value is the maximum of 16 and 2*3 = 16. - maximum value: 1460
Default
1460
Properties
Get example
> get bu s c
R000006
1460
Set example
> set bu s c 1450
R000008
Set OK
bus.stream.flush_time
Abbreviation
bu s t
Access
get/set
Description
Timeout in milliseconds before bytes are automatically flushed to the network stream.
If set to 0, automatic flush is disabled.
To achieve optimal throughput, set flush time to 0. Gecko OS transfers data with 'Zero Copy'. i.e. a data packet is directly transferred from the bus to network or network to bus.
Arguments
<0-65535>
Default
50
Properties
Get example
> get bu s t
R000004
20
Set example
> set bu s t 10
R000008
Set OK
bus.stream.flush_time_reset
Abbreviation
bu s r
Access
get/set
Description
Flag whether to reset the flush timer if data is received before the flush timeout expires. When this variable is set and data is streaming, data is flushed only when the buffer is full. This allows for efficient use of the packet buffer and prevents packet fragmentation. When the variable is reset, the buffer is flushed at intervals of bus.stream.flush_time and also when the buffer is full. This allows data to be sent at consistent intervals.
Arguments
<1/0>
Default
0
Properties
Get example
> get bus.stream.flush_time_reset
0
Set example
> set bus.stream.flush_time_reset 1
Set OK