sl_se_status_t Struct Reference
SE status.
#include <sl_se_manager_types.h>
Data Fields | |
uint32_t | boot_status |
Boot status code / error code (Bits [7:0]). | |
uint32_t | se_fw_version |
SE firmware version. | |
uint32_t | host_fw_version |
Host firmware version (if available). | |
sl_se_debug_status_t | debug_status |
Debug lock status. | |
bool | secure_boot_enabled |
Secure boot enabled. | |
uint32_t | tamper_status |
Recorded tamper status. Reset on status read. | |
uint32_t | tamper_status_raw |
Currently active tamper sources. | |
SE status.
Field Documentation
◆ boot_status
uint32_t sl_se_status_t::boot_status |
Boot status code / error code (Bits [7:0]).
◆ se_fw_version
uint32_t sl_se_status_t::se_fw_version |
SE firmware version.
◆ host_fw_version
uint32_t sl_se_status_t::host_fw_version |
Host firmware version (if available).
◆ debug_status
sl_se_debug_status_t sl_se_status_t::debug_status |
Debug lock status.
◆ secure_boot_enabled
bool sl_se_status_t::secure_boot_enabled |
Secure boot enabled.
◆ tamper_status
uint32_t sl_se_status_t::tamper_status |
Recorded tamper status. Reset on status read.
◆ tamper_status_raw
uint32_t sl_se_status_t::tamper_status_raw |
Currently active tamper sources.