BURTC_Init_TypeDef Struct Reference
BURTC initialization structure for Series 2 devices.
#include <em_burtc.h>
Data Fields |
|
bool | start |
Start BURTC after initialization.
|
|
bool | debugRun |
If true, counter will keep running under debug halt.
|
|
uint32_t | clkDiv |
Clock divider.
|
|
bool | compare0Top |
Set if Compare Value 0 is also top value (counter restart)
|
|
bool | em4comp |
Enable EM4 wakeup on compare match.
|
|
bool | em4overflow |
Enable EM4 wakeup on counter overflow.
|
|
BURTC initialization structure for Series 2 devices.
Field Documentation
◆ start
bool BURTC_Init_TypeDef::start |
Start BURTC after initialization.
◆ debugRun
bool BURTC_Init_TypeDef::debugRun |
If true, counter will keep running under debug halt.
◆ clkDiv
uint32_t BURTC_Init_TypeDef::clkDiv |
Clock divider.
Supported range is 1-32768
◆ compare0Top
bool BURTC_Init_TypeDef::compare0Top |
Set if Compare Value 0 is also top value (counter restart)
◆ em4comp
bool BURTC_Init_TypeDef::em4comp |
Enable EM4 wakeup on compare match.
◆ em4overflow
bool BURTC_Init_TypeDef::em4overflow |
Enable EM4 wakeup on counter overflow.