Real Time Counter (RTC) Peripheral API.
This module contains functions to control the RTC peripheral of Silicon Labs 32-bit MCUs and SoCs. The RTC ensures timekeeping in low energy modes.
|
|
|
uint32_t
|
RTC_CompareGet
(unsigned int comp)
|
|
|
Get the RTC compare register value.
|
|
|
|
void
|
RTC_CompareSet
(unsigned int comp, uint32_t value)
|
|
|
Set the RTC compare register value.
|
|
|
|
void
|
RTC_Enable
(bool enable)
|
|
|
Enable/disable RTC.
|
|
|
|
void
|
RTC_FreezeEnable
(bool enable)
|
|
|
RTC register synchronization freeze control.
|
|
|
|
void
|
RTC_Init
(const
RTC_Init_TypeDef
*init)
|
|
|
Initialize RTC.
|
|
|
|
void
|
RTC_Reset
(void)
|
|
|
Restore RTC to reset state.
|
|
|
|
void
|
RTC_CounterReset
(void)
|
|
|
Restart the RTC counter from zero.
|
|
|
|
uint32_t
|
RTC_CounterGet
(void)
|
|
|
Get RTC counter value.
|
|
|
|
void
|
RTC_IntClear
(uint32_t flags)
|
|
|
Clear one or more pending RTC interrupts.
|
|
|
|
void
|
RTC_IntDisable
(uint32_t flags)
|
|
|
Disable one or more RTC interrupts.
|
|
|
|
void
|
RTC_IntEnable
(uint32_t flags)
|
|
|
Enable one or more RTC interrupts.
|
|
|
|
uint32_t
|
RTC_IntGet
(void)
|
|
|
Get pending RTC interrupt flags.
|
|
|
|
uint32_t
|
RTC_IntGetEnabled
(void)
|
|
|
Get enabled and pending RTC interrupt flags.
|
|
|
|
void
|
RTC_IntSet
(uint32_t flags)
|
|
|
Set one or more pending RTC interrupts from SW.
|
|
|
|
|
|
#define
|
NUM_RTC_CHANNELS
2U
|
|
|
The RTC peripheral on series 0 devices support 2 compare channels while the RTC peripheral on series 1 devices support 6 compare channels.
|
|
|
|
#define
|
RTC_INIT_DEFAULT
|
|
|
Suggested default configuration for RTC initialization structure.
|
|
|
◆
RTC_CompareGet()
|
uint32_t RTC_CompareGet
|
(
|
unsigned int
|
comp
|
)
|
|
Get the RTC compare register value.
-
Parameters
-
|
[in]
|
comp
|
A compare register to get. This value must be less than
NUM_RTC_CHANNELS
.
|
-
Returns
-
A compare register value, 0 if invalid register selected.
◆
RTC_CompareSet()
|
void RTC_CompareSet
|
(
|
unsigned int
|
comp,
|
|
|
|
uint32_t
|
value
|
|
|
)
|
|
|
Set the RTC compare register value.
-
Note
-
The setting of a compare register requires synchronization into the low-frequency domain. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the regSync() internal function call.
-
Parameters
-
|
[in]
|
comp
|
A compare register to set. This value must be less than
NUM_RTC_CHANNELS
.
|
|
[in]
|
value
|
An initialization value (<= 0x00ffffff).
|
◆
RTC_Enable()
|
void RTC_Enable
|
(
|
bool
|
enable
|
)
|
|
Enable/disable RTC.
-
Note
-
The enabling/disabling of RTC modifies the RTC CTRL register which requires synchronization into the low-frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the regSync() internal function call.
-
Parameters
-
|
[in]
|
enable
|
True to enable counting, false to disable.
|
◆
RTC_FreezeEnable()
|
void RTC_FreezeEnable
|
(
|
bool
|
enable
|
)
|
|
RTC register synchronization freeze control.
Some RTC registers require synchronization into the low-frequency (LF) domain. The freeze feature allows for several registers to be modified before passing them to the LF domain simultaneously (which takes place when the freeze mode is disabled).
-
Note
-
When enabling freeze mode, this function will wait for all current ongoing RTC synchronization to LF domain to complete (normally synchronization will not be in progress.) However, for this reason, when using freeze mode, modifications of registers requiring LF synchronization should be done within one freeze enable/disable block to avoid unnecessary stalling. This only applies to the Gecko Family. See the reference manual chapter about Access to Low Energy Peripherals (Asynchronos Registers) for details.
-
Parameters
-
|
[in]
|
enable
|
-
True - enable freeze, modified registers are not propagated to the LF domain
-
False - disables freeze, modified registers are propagated to LF domain
|
◆
RTC_Init()
Initialize RTC.
Note that the compare values must be set separately with
RTC_CompareSet()
prior to the use of this function if configuring the RTC to start when initialization is completed.
-
Note
-
The initialization of the RTC modifies the RTC CTRL register which requires synchronization into the low-frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the regSync() internal function call.
-
Parameters
-
|
[in]
|
init
|
A pointer to the RTC initialization structure.
|
◆
RTC_Reset()
Restore RTC to reset state.
◆
RTC_CounterReset()
|
void RTC_CounterReset
|
(
|
void
|
|
)
|
|
Restart the RTC counter from zero.
◆
RTC_CounterGet()
|
uint32_t RTC_CounterGet
|
(
|
void
|
|
)
|
|
|
inline
|
Get RTC counter value.
-
Returns
-
Current RTC counter value.
◆
RTC_IntClear()
|
void RTC_IntClear
|
(
|
uint32_t
|
flags
|
)
|
|
|
inline
|
Clear one or more pending RTC interrupts.
-
Parameters
-
|
[in]
|
flags
|
RTC interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources for the RTC module (RTC_IFS_nnn).
|
◆
RTC_IntDisable()
|
void RTC_IntDisable
|
(
|
uint32_t
|
flags
|
)
|
|
|
inline
|
Disable one or more RTC interrupts.
-
Parameters
-
|
[in]
|
flags
|
RTC interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt sources for the RTC module (RTC_IFS_nnn).
|
◆
RTC_IntEnable()
|
void RTC_IntEnable
|
(
|
uint32_t
|
flags
|
)
|
|
|
inline
|
Enable one or more RTC interrupts.
-
Note
-
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using
RTC_IntClear()
prior to enabling the interrupt.
-
Parameters
-
|
[in]
|
flags
|
RTC interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the RTC module (RTC_IFS_nnn).
|
◆
RTC_IntGet()
|
uint32_t RTC_IntGet
|
(
|
void
|
|
)
|
|
|
inline
|
Get pending RTC interrupt flags.
-
Note
-
Event bits are not cleared by using this function.
-
Returns
-
Pending RTC interrupt sources. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the RTC module (RTC_IFS_nnn).
◆
RTC_IntGetEnabled()
|
uint32_t RTC_IntGetEnabled
|
(
|
void
|
|
)
|
|
|
inline
|
Get enabled and pending RTC interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
-
Note
-
Interrupt flags are not cleared by using this function.
-
Returns
-
Pending and enabled RTC interrupt sources. The return value is the bitwise AND of
-
the enabled interrupt sources in RTC_IEN and
-
the pending interrupt flags RTC_IF.
◆
RTC_IntSet()
|
void RTC_IntSet
|
(
|
uint32_t
|
flags
|
)
|
|
|
inline
|
Set one or more pending RTC interrupts from SW.
-
Parameters
-
|
[in]
|
flags
|
RTC interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the RTC module (RTC_IFS_nnn).
|
◆
NUM_RTC_CHANNELS
|
#define NUM_RTC_CHANNELS 2U
|
The RTC peripheral on series 0 devices support 2 compare channels while the RTC peripheral on series 1 devices support 6 compare channels.
◆
RTC_INIT_DEFAULT
Value:
{ \
true,
\
false,
\
true
\
}
Suggested default configuration for RTC initialization structure.