IADC - Incremental ADC

Description

Incremental Analog to Digital Converter (IADC) Peripheral API.

This module contains functions to control the IADC peripheral of Silicon Labs 32-bit MCUs and SoCs. The IADC is used to convert analog signals into a digital representation.

Data Structures

struct  IADC_Init_t
 IADC init structure, common for single conversion and scan sequence.
 
struct  IADC_Config_t
 IADC config structure.
 
struct  IADC_AllConfigs_t
 Structure for all IADC configs.
 
struct  IADC_InitScan_t
 IADC scan init structure.
 
struct  IADC_InitSingle_t
 IADC single init structure.
 
struct  IADC_SingleInput_t
 IADC single input selection structure.
 
struct  IADC_ScanTableEntry_t
 IADC scan table entry structure.
 
struct  IADC_ScanTable_t
 Structure for IADC scan table.
 
struct  IADC_Result_t
 Structure holding IADC result, including data and ID.
 

Functions

void IADC_init (IADC_TypeDef *iadc, const IADC_Init_t *init, const IADC_AllConfigs_t *allConfigs)
 Initialize IADC.
 
void IADC_reset (IADC_TypeDef *iadc)
 Reset IADC to same state as after a HW reset.
 
void IADC_initScan (IADC_TypeDef *iadc, const IADC_InitScan_t *init, const IADC_ScanTable_t *scanTable)
 Initialize IADC scan sequence.
 
void IADC_updateScanEntry (IADC_TypeDef *iadc, uint8_t id, IADC_ScanTableEntry_t *entry)
 Add/update entry in scan table.
 
void IADC_setScanMask (IADC_TypeDef *iadc, uint32_t mask)
 Set mask of IADC scan table entries to include in scan.
 
void IADC_initSingle (IADC_TypeDef *iadc, const IADC_InitSingle_t *init, const IADC_SingleInput_t *input)
 Initialize single IADC conversion.
 
void IADC_updateSingleInput (IADC_TypeDef *iadc, const IADC_SingleInput_t *input)
 Update IADC single input selection.
 
uint8_t IADC_calcSrcClkPrescale (IADC_TypeDef *iadc, uint32_t srcClkFreq, uint32_t cmuClkFreq)
 Calculate prescaler for CLK_SRC_ADC high speed clock.
 
uint32_t IADC_calcAdcClkPrescale (IADC_TypeDef *iadc, uint32_t adcClkFreq, uint32_t cmuClkFreq, IADC_CfgAdcMode_t adcMode, uint8_t srcClkPrescaler)
 Calculate prescaler for ADC_CLK clock.
 
uint8_t IADC_calcTimebase (IADC_TypeDef *iadc, uint32_t cmuClkFreq)
 Calculate timebase value in order to get a timebase providing at least 1us.
 
IADC_Result_t IADC_readSingleResult (IADC_TypeDef *iadc)
 Read most recent single conversion result.
 
IADC_Result_t IADC_pullSingleFifoResult (IADC_TypeDef *iadc)
 Pull result from single data FIFO.
 
IADC_Result_t IADC_readScanResult (IADC_TypeDef *iadc)
 Read most recent scan conversion result.
 
IADC_Result_t IADC_pullScanFifoResult (IADC_TypeDef *iadc)
 Pull result from scan data FIFO.
 
uint32_t IADC_getReferenceVoltage (IADC_CfgReference_t reference)
 Get reference voltage selection.
 
uint32_t IADC_pullSingleFifoData (IADC_TypeDef *iadc)
 Pull data from single data FIFO.
 
uint32_t IADC_readSingleData (IADC_TypeDef *iadc)
 Read most recent single conversion data.
 
uint32_t IADC_pullScanFifoData (IADC_TypeDef *iadc)
 Pull data from scan data FIFO.
 
uint32_t IADC_readScanData (IADC_TypeDef *iadc)
 Read most recent scan conversion data.
 
void IADC_clearInt (IADC_TypeDef *iadc, uint32_t flags)
 Clear one or more pending IADC interrupts.
 
void IADC_disableInt (IADC_TypeDef *iadc, uint32_t flags)
 Disable one or more IADC interrupts.
 
void IADC_enableInt (IADC_TypeDef *iadc, uint32_t flags)
 Enable one or more IADC interrupts.
 
uint32_t IADC_getInt (IADC_TypeDef *iadc)
 Get pending IADC interrupt flags.
 
uint32_t IADC_getEnabledInt (IADC_TypeDef *iadc)
 Get enabled and pending IADC interrupt flags.
 
void IADC_setInt (IADC_TypeDef *iadc, uint32_t flags)
 Set one or more pending IADC interrupts from SW.
 
void IADC_command (IADC_TypeDef *iadc, IADC_Cmd_t cmd)
 Start/stop scan sequence, single conversion and/or timer.
 
uint32_t IADC_getScanMask (IADC_TypeDef *iadc)
 Get the scan mask currently used in the IADC.
 
uint32_t IADC_getStatus (IADC_TypeDef *iadc)
 Get status bits of IADC.
 
uint8_t IADC_getSingleFifoCnt (IADC_TypeDef *iadc)
 Get the number of elements in the IADC single FIFO.
 
uint8_t IADC_getScanFifoCnt (IADC_TypeDef *iadc)
 Get the number of elements in the IADC scan FIFO.
 
IADC_NegInput_t IADC_portPinToNegInput (GPIO_Port_TypeDef port, uint8_t pin)
 Convert the GPIO port/pin to IADC negative input selection.
 
IADC_PosInput_t IADC_portPinToPosInput (GPIO_Port_TypeDef port, uint8_t pin)
 Convert the GPIO port/pin to IADC positive input selection.
 

Macros

#define IADC_INIT_DEFAULT
 Default config for IADC init structure.
 
#define IADC_CONFIG_DEFAULT
 Default IADC config structure.
 
#define IADC_ALLCONFIGS_DEFAULT
 Default IADC sructure for all configs.
 
#define IADC_INITSCAN_DEFAULT
 Default config for IADC scan init structure.
 
#define IADC_INITSINGLE_DEFAULT
 Default config for IADC single init structure.
 
#define IADC_SINGLEINPUT_DEFAULT
 Default config for IADC single input structure.
 
#define IADC_SCANTABLEENTRY_DEFAULT
 Default config for IADC scan table entry structure.
 
#define IADC_SCANTABLE_DEFAULT
 Default IADC structure for scan table.
 

Enumerations

enum  IADC_Warmup_t {
  iadcWarmupNormal = _IADC_CTRL_WARMUPMODE_NORMAL,
  iadcWarmupKeepInStandby = _IADC_CTRL_WARMUPMODE_KEEPINSTANDBY,
  iadcWarmupKeepWarm = _IADC_CTRL_WARMUPMODE_KEEPWARM
}
 Warm-up mode.
 
enum  IADC_Alignment_t {
  iadcAlignRight12 = _IADC_SCANFIFOCFG_ALIGNMENT_RIGHT12,
  iadcAlignLeft12 = _IADC_SCANFIFOCFG_ALIGNMENT_LEFT12,
  iadcAlignRight16 = _IADC_SCANFIFOCFG_ALIGNMENT_RIGHT16,
  iadcAlignLeft16 = _IADC_SCANFIFOCFG_ALIGNMENT_LEFT16,
  iadcAlignRight20 = _IADC_SCANFIFOCFG_ALIGNMENT_RIGHT20,
  iadcAlignLeft20 = _IADC_SCANFIFOCFG_ALIGNMENT_LEFT20
}
 IADC result alignment.
 
enum  IADC_NegInput_t {
  iadcNegInputGnd,
  iadcNegInputGndaux = (_IADC_SCAN_PORTNEG_GND << (_IADC_SCAN_PORTNEG_SHIFT - _IADC_SCAN_PINNEG_SHIFT)),
  iadcNegInputDac1 = (_IADC_SCAN_PORTNEG_DAC1 << (_IADC_SCAN_PORTNEG_SHIFT - _IADC_SCAN_PINNEG_SHIFT)),
  iadcNegInputPadAna1 = (_IADC_SCAN_PORTNEG_PADANA1 << (_IADC_SCAN_PORTNEG_SHIFT - _IADC_SCAN_PINNEG_SHIFT)),
  iadcNegInputPortAPin0 = (_IADC_SCAN_PORTNEG_PORTA << (_IADC_SCAN_PORTNEG_SHIFT - _IADC_SCAN_PINNEG_SHIFT)),
  iadcNegInputPortAPin1,
  iadcNegInputPortAPin2,
  iadcNegInputPortAPin3,
  iadcNegInputPortAPin4,
  iadcNegInputPortAPin5,
  iadcNegInputPortAPin6,
  iadcNegInputPortAPin7,
  iadcNegInputPortAPin8,
  iadcNegInputPortAPin9,
  iadcNegInputPortAPin10,
  iadcNegInputPortAPin11,
  iadcNegInputPortAPin12,
  iadcNegInputPortAPin13,
  iadcNegInputPortAPin14,
  iadcNegInputPortAPin15,
  iadcNegInputPortBPin0,
  iadcNegInputPortBPin1,
  iadcNegInputPortBPin2,
  iadcNegInputPortBPin3,
  iadcNegInputPortBPin4,
  iadcNegInputPortBPin5,
  iadcNegInputPortBPin6,
  iadcNegInputPortBPin7,
  iadcNegInputPortBPin8,
  iadcNegInputPortBPin9,
  iadcNegInputPortBPin10,
  iadcNegInputPortBPin11,
  iadcNegInputPortBPin12,
  iadcNegInputPortBPin13,
  iadcNegInputPortBPin14,
  iadcNegInputPortBPin15,
  iadcNegInputPortCPin0,
  iadcNegInputPortCPin1,
  iadcNegInputPortCPin2,
  iadcNegInputPortCPin3,
  iadcNegInputPortCPin4,
  iadcNegInputPortCPin5,
  iadcNegInputPortCPin6,
  iadcNegInputPortCPin7,
  iadcNegInputPortCPin8,
  iadcNegInputPortCPin9,
  iadcNegInputPortCPin10,
  iadcNegInputPortCPin11,
  iadcNegInputPortCPin12,
  iadcNegInputPortCPin13,
  iadcNegInputPortCPin14,
  iadcNegInputPortCPin15,
  iadcNegInputPortDPin0,
  iadcNegInputPortDPin1,
  iadcNegInputPortDPin2,
  iadcNegInputPortDPin3,
  iadcNegInputPortDPin4,
  iadcNegInputPortDPin5,
  iadcNegInputPortDPin6,
  iadcNegInputPortDPin7,
  iadcNegInputPortDPin8,
  iadcNegInputPortDPin9,
  iadcNegInputPortDPin10,
  iadcNegInputPortDPin11,
  iadcNegInputPortDPin12,
  iadcNegInputPortDPin13,
  iadcNegInputPortDPin14,
  iadcNegInputPortDPin15
}
 IADC negative input selection.
 
enum  IADC_PosInput_t {
  iadcPosInputGnd = (_IADC_SCAN_PORTPOS_GND << (_IADC_SCAN_PORTPOS_SHIFT - _IADC_SCAN_PINPOS_SHIFT)),
  iadcPosInputAvdd,
  iadcPosInputVddio,
  iadcPosInputVss,
  iadcPosInputVssaux,
  iadcPosInputDvdd,
  iadcPosInputDecouple,
  iadcPosInputDac0 = (_IADC_SCAN_PORTPOS_DAC0 << (_IADC_SCAN_PORTPOS_SHIFT - _IADC_SCAN_PINPOS_SHIFT)),
  iadcPosInputPadAna0 = (_IADC_SCAN_PORTPOS_PADANA0 << (_IADC_SCAN_PORTPOS_SHIFT - _IADC_SCAN_PINPOS_SHIFT)),
  iadcPosInputPortAPin0 = (_IADC_SCAN_PORTPOS_PORTA << (_IADC_SCAN_PORTPOS_SHIFT - _IADC_SCAN_PINPOS_SHIFT)),
  iadcPosInputPortAPin1,
  iadcPosInputPortAPin2,
  iadcPosInputPortAPin3,
  iadcPosInputPortAPin4,
  iadcPosInputPortAPin5,
  iadcPosInputPortAPin6,
  iadcPosInputPortAPin7,
  iadcPosInputPortAPin8,
  iadcPosInputPortAPin9,
  iadcPosInputPortAPin10,
  iadcPosInputPortAPin11,
  iadcPosInputPortAPin12,
  iadcPosInputPortAPin13,
  iadcPosInputPortAPin14,
  iadcPosInputPortAPin15,
  iadcPosInputPortBPin0,
  iadcPosInputPortBPin1,
  iadcPosInputPortBPin2,
  iadcPosInputPortBPin3,
  iadcPosInputPortBPin4,
  iadcPosInputPortBPin5,
  iadcPosInputPortBPin6,
  iadcPosInputPortBPin7,
  iadcPosInputPortBPin8,
  iadcPosInputPortBPin9,
  iadcPosInputPortBPin10,
  iadcPosInputPortBPin11,
  iadcPosInputPortBPin12,
  iadcPosInputPortBPin13,
  iadcPosInputPortBPin14,
  iadcPosInputPortBPin15,
  iadcPosInputPortCPin0,
  iadcPosInputPortCPin1,
  iadcPosInputPortCPin2,
  iadcPosInputPortCPin3,
  iadcPosInputPortCPin4,
  iadcPosInputPortCPin5,
  iadcPosInputPortCPin6,
  iadcPosInputPortCPin7,
  iadcPosInputPortCPin8,
  iadcPosInputPortCPin9,
  iadcPosInputPortCPin10,
  iadcPosInputPortCPin11,
  iadcPosInputPortCPin12,
  iadcPosInputPortCPin13,
  iadcPosInputPortCPin14,
  iadcPosInputPortCPin15,
  iadcPosInputPortDPin0,
  iadcPosInputPortDPin1,
  iadcPosInputPortDPin2,
  iadcPosInputPortDPin3,
  iadcPosInputPortDPin4,
  iadcPosInputPortDPin5,
  iadcPosInputPortDPin6,
  iadcPosInputPortDPin7,
  iadcPosInputPortDPin8,
  iadcPosInputPortDPin9,
  iadcPosInputPortDPin10,
  iadcPosInputPortDPin11,
  iadcPosInputPortDPin12,
  iadcPosInputPortDPin13,
  iadcPosInputPortDPin14,
  iadcPosInputPortDPin15
}
 IADC positive port selection.
 
enum  IADC_Cmd_t {
  iadcCmdStartSingle = IADC_CMD_SINGLESTART,
  iadcCmdStopSingle = IADC_CMD_SINGLESTOP,
  iadcCmdStartScan = IADC_CMD_SCANSTART,
  iadcCmdStopScan = IADC_CMD_SCANSTOP,
  iadcCmdEnableTimer = IADC_CMD_TIMEREN,
  iadcCmdDisableTimer = IADC_CMD_TIMERDIS
}
 IADC Commands.
 
enum  IADC_CfgAdcMode_t {
  iadcCfgModeNormal = _IADC_CFG_ADCMODE_NORMAL,
  iadcCfgModeHighSpeed = _IADC_CFG_ADCMODE_HIGHSPEED,
  iadcCfgModeHighAccuracy = _IADC_CFG_ADCMODE_HIGHACCURACY
}
 IADC Configuration.
 
enum  IADC_CfgOsrHighSpeed_t {
  iadcCfgOsrHighSpeed2x = _IADC_CFG_OSRHS_HISPD2,
  iadcCfgOsrHighSpeed4x = _IADC_CFG_OSRHS_HISPD4,
  iadcCfgOsrHighSpeed8x = _IADC_CFG_OSRHS_HISPD8,
  iadcCfgOsrHighSpeed16x = _IADC_CFG_OSRHS_HISPD16,
  iadcCfgOsrHighSpeed32x = _IADC_CFG_OSRHS_HISPD32,
  iadcCfgOsrHighSpeed64x = _IADC_CFG_OSRHS_HISPD64
}
 IADC Over sampling rate for high speed.
 
enum  IADC_CfgOsrHighAccuracy_t {
  iadcCfgOsrHighAccuracy16x = _IADC_CFG_OSRHA_HIACC16,
  iadcCfgOsrHighAccuracy32x = _IADC_CFG_OSRHA_HIACC32,
  iadcCfgOsrHighAccuracy64x = _IADC_CFG_OSRHA_HIACC64,
  iadcCfgOsrHighAccuracy92x = _IADC_CFG_OSRHA_HIACC92,
  iadcCfgOsrHighAccuracy128x = _IADC_CFG_OSRHA_HIACC128,
  iadcCfgOsrHighAccuracy256x = _IADC_CFG_OSRHA_HIACC256
}
 IADC Over sampling rate for high accuracy.
 
enum  IADC_CfgAnalogGain_t {
  iadcCfgAnalogGain0P5x = _IADC_CFG_ANALOGGAIN_ANAGAIN0P5,
  iadcCfgAnalogGain1x = _IADC_CFG_ANALOGGAIN_ANAGAIN1,
  iadcCfgAnalogGain2x = _IADC_CFG_ANALOGGAIN_ANAGAIN2,
  iadcCfgAnalogGain3x = _IADC_CFG_ANALOGGAIN_ANAGAIN3,
  iadcCfgAnalogGain4x = _IADC_CFG_ANALOGGAIN_ANAGAIN4
}
 IADC Analog Gain.
 
enum  IADC_CfgReference_t {
  iadcCfgReferenceInt1V2 = _IADC_CFG_REFSEL_VBGR,
  iadcCfgReferenceExt1V25 = _IADC_CFG_REFSEL_VREF,
  iadcCfgReferenceExt2V5 = _IADC_CFG_REFSEL_VREF2P5,
  iadcCfgReferenceVddx = _IADC_CFG_REFSEL_VDDX,
  iadcCfgReferenceVddX0P8Buf = _IADC_CFG_REFSEL_VDDX0P8BUF
}
 IADC Reference.
 
enum  IADC_CfgTwosComp_t {
  iadcCfgTwosCompAuto = _IADC_CFG_TWOSCOMPL_AUTO,
  iadcCfgTwosCompUnipolar = _IADC_CFG_TWOSCOMPL_FORCEUNIPOLAR,
  iadcCfgTwosCompBipolar = _IADC_CFG_TWOSCOMPL_FORCEBIPOLAR
}
 IADC Two's complement results.
 
enum  IADC_TriggerSel_t {
  iadcTriggerSelImmediate = _IADC_TRIGGER_SCANTRIGSEL_IMMEDIATE,
  iadcTriggerSelTimer = _IADC_TRIGGER_SCANTRIGSEL_TIMER,
  iadcTriggerSelPrs0SameClk = _IADC_TRIGGER_SCANTRIGSEL_PRSCLKGRP,
  iadcTriggerSelPrs0PosEdge = _IADC_TRIGGER_SCANTRIGSEL_PRSPOS,
  iadcTriggerSelPrs0NegEdge = _IADC_TRIGGER_SCANTRIGSEL_PRSNEG,
  iadcTriggerSelLesense = _IADC_TRIGGER_SCANTRIGSEL_LESENSE
}
 IADC trigger action.
 
enum  IADC_TriggerAction_t {
  iadcTriggerActionOnce = _IADC_TRIGGER_SCANTRIGACTION_ONCE,
  iadcTriggerActionContinuous = _IADC_TRIGGER_SCANTRIGACTION_CONTINUOUS
}
 IADC trigger action.
 
enum  IADC_FifoCfgDvl_t {
  iadcFifoCfgDvl1 = _IADC_SCANFIFOCFG_DVL_VALID1,
  iadcFifoCfgDvl2 = _IADC_SCANFIFOCFG_DVL_VALID2,
  iadcFifoCfgDvl3 = _IADC_SCANFIFOCFG_DVL_VALID3,
  iadcFifoCfgDvl4 = _IADC_SCANFIFOCFG_DVL_VALID4,
  iadcFifoCfgDvl5 = _IADC_SCANFIFOCFG_DVL_VALID5,
  iadcFifoCfgDvl6 = _IADC_SCANFIFOCFG_DVL_VALID6,
  iadcFifoCfgDvl7 = _IADC_SCANFIFOCFG_DVL_VALID7
}
 IADC data valid level before requesting DMA transfer.
 
enum  IADC_DigitalAveraging_t {
  iadcDigitalAverage1 = _IADC_CFG_DIGAVG_AVG1,
  iadcDigitalAverage2 = _IADC_CFG_DIGAVG_AVG2,
  iadcDigitalAverage4 = _IADC_CFG_DIGAVG_AVG4,
  iadcDigitalAverage8 = _IADC_CFG_DIGAVG_AVG8,
  iadcDigitalAverage16 = _IADC_CFG_DIGAVG_AVG16
}
 IADC digital averaging function.
 

Function Documentation

◆ IADC_init()

void IADC_init ( IADC_TypeDef *  iadc,
const IADC_Init_t init,
const IADC_AllConfigs_t allConfigs 
)

Initialize IADC.

Initializes common parts for both single conversion and scan sequence. In addition, single and/or scan control configuration must be done, please refer to IADC_initSingle() and IADC_initScan() respectively.

Note
This function will stop any ongoing conversions.
Parameters
[in]iadcPointer to IADC peripheral register block.
[in]initPointer to IADC initialization structure.
[in]allConfigsPointer to structure holding all configs.

◆ IADC_reset()

void IADC_reset ( IADC_TypeDef *  iadc)

Reset IADC to same state as after a HW reset.

Parameters
[in]iadcPointer to IADC peripheral register block.

◆ IADC_initScan()

void IADC_initScan ( IADC_TypeDef *  iadc,
const IADC_InitScan_t init,
const IADC_ScanTable_t scanTable 
)

Initialize IADC scan sequence.

This function will configure scan mode and set up entries in the scan table. The scan table mask can be updated by calling IADC_updateScanMask.

Note
This function will stop any ongoing conversions.
If an even numbered pin is selected for the positive input, the negative input must use an odd numbered pin and vice versa.
Parameters
[in]iadcPointer to IADC peripheral register block.
[in]initPointer to IADC initialization structure.
[in]scanTablePointer to IADC scan table structure.

◆ IADC_updateScanEntry()

void IADC_updateScanEntry ( IADC_TypeDef *  iadc,
uint8_t  id,
IADC_ScanTableEntry_t entry 
)

Add/update entry in scan table.

This function will update or add an entry in the scan table with a specific ID.

Note
This function will stop any ongoing conversions.
Parameters
[in]iadcPointer to IADC peripheral register block.
[in]idID of scan table entry to add.
[in]entryPointer to scan table entry structure.

◆ IADC_setScanMask()

void IADC_setScanMask ( IADC_TypeDef *  iadc,
uint32_t  mask 
)

Set mask of IADC scan table entries to include in scan.

Set mask of scan table entries to include in next scan. This function can be called while scan conversions are ongoing, but the new scan mask will take effect once the ongoing scan is completed.

Parameters
[in]iadcPointer to IADC peripheral register block.
[in]maskMask of scan table entries to include in scan.

◆ IADC_initSingle()

void IADC_initSingle ( IADC_TypeDef *  iadc,
const IADC_InitSingle_t init,
const IADC_SingleInput_t input 
)

Initialize single IADC conversion.

This function will initialize the single conversion and configure the single input selection.

Note
This function will stop any ongoing conversions.
If an even numbered pin is selected for the positive input, the negative input must use an odd numbered pin and vice versa.
Parameters
[in]iadcPointer to IADC peripheral register block.
[in]initPointer to IADC single initialization structure.
[in]inputPointer to IADC single input selection initialization structure.

◆ IADC_updateSingleInput()

void IADC_updateSingleInput ( IADC_TypeDef *  iadc,
const IADC_SingleInput_t input 
)

Update IADC single input selection.

This function updates the single input selection. The function can be called while single and/or scan conversions are ongoing and the new input configuration will take place on the next single conversion.

Note
If an even numbered pin is selected for the positive input, the negative input must use an odd numbered pin and vice versa.
Parameters
[in]iadcPointer to IADC peripheral register block.
[in]inputPointer to single input selection structure.

◆ IADC_calcSrcClkPrescale()

uint8_t IADC_calcSrcClkPrescale ( IADC_TypeDef *  iadc,
uint32_t  srcClkFreq,
uint32_t  cmuClkFreq 
)

Calculate prescaler for CLK_SRC_ADC high speed clock.

The IADC high speed clock is given by: CLK_SRC_ADC / (srcClkPrescaler + 1).

Parameters
[in]iadcPointer to IADC peripheral register block.
[in]srcClkFreqCLK_SRC_ADC frequency wanted. The frequency will automatically be adjusted to be within valid range according to reference manual.
[in]cmuClkFreqFrequency in Hz of reference CLK_CMU_ADC. Set to 0 to use currently defined CMU clock setting for the IADC.
Returns
Divider value to use for IADC in order to achieve a high speed clock value <= srcClkFreq.

◆ IADC_calcAdcClkPrescale()

uint32_t IADC_calcAdcClkPrescale ( IADC_TypeDef *  iadc,
uint32_t  adcClkFreq,
uint32_t  cmuClkFreq,
IADC_CfgAdcMode_t  adcMode,
uint8_t  srcClkPrescaler 
)

Calculate prescaler for ADC_CLK clock.

The ADC_CLK is given by: CLK_SRC_ADC / (adcClkprescale + 1).

Parameters
[in]iadcPointer to IADC peripheral register block.
[in]adcClkFreqADC_CLK frequency wanted. The frequency will automatically be adjusted to be within valid range according to reference manual.
[in]cmuClkFreqFrequency in Hz of CLK_CMU_ADC Set to 0 to use currently defined IADC clock setting (in CMU).
[in]adcModeMode for IADC config.
[in]srcClkPrescalerPrecaler setting for ADC_CLK
Returns
Divider value to use for IADC in order to achieve a ADC_CLK frequency <= adcClkFreq.

◆ IADC_calcTimebase()

uint8_t IADC_calcTimebase ( IADC_TypeDef *  iadc,
uint32_t  cmuClkFreq 
)

Calculate timebase value in order to get a timebase providing at least 1us.

Parameters
[in]iadcPointer to IADC peripheral register block.
[in]cmuClkFreqFrequency in Hz of reference CLK_CMU_ADC clock. Set to 0 to use currently defined CMU clock setting for the IADC.
Returns
Timebase value to use for IADC in order to achieve at least 1 us.

◆ IADC_readSingleResult()

IADC_Result_t IADC_readSingleResult ( IADC_TypeDef *  iadc)

Read most recent single conversion result.

The result struct includes both the data and the ID (0x20) if showId was set when initializing single mode. Calling this function will not affect the state of the single data FIFO.

Note
Check data valid flag before calling this function.
Parameters
[in]iadcPointer to IADC peripheral register block.
Returns
Single conversion result struct holding data and id.

◆ IADC_pullSingleFifoResult()

IADC_Result_t IADC_pullSingleFifoResult ( IADC_TypeDef *  iadc)

Pull result from single data FIFO.

The result struct includes both the data and the ID (0x20) if showId was set when initializing single mode.

Note
Check data valid flag before calling this function.
Parameters
[in]iadcPointer to IADC peripheral register block.
Returns
Single conversion result struct holding data and id.

◆ IADC_readScanResult()

IADC_Result_t IADC_readScanResult ( IADC_TypeDef *  iadc)

Read most recent scan conversion result.

The result struct includes both the data and the ID (0x20) if showId was set when initializing scan entry. Calling this function will not affect the state of the scan data FIFO.

Note
Check data valid flag before calling this function.
Parameters
[in]iadcPointer to IADC peripheral register block.
Returns
Scan conversion result struct holding data and id.

◆ IADC_pullScanFifoResult()

IADC_Result_t IADC_pullScanFifoResult ( IADC_TypeDef *  iadc)

Pull result from scan data FIFO.

The result struct includes both the data and the ID (0x20) if showId was set when initializing scan entry.

Note
Check data valid flag before calling this function.
Parameters
[in]iadcPointer to IADC peripheral register block.
Returns
Scan conversion result struct holding data and id.

◆ IADC_getReferenceVoltage()

uint32_t IADC_getReferenceVoltage ( IADC_CfgReference_t  reference)

Get reference voltage selection.

Parameters
[in]referenceIADC Reference selection.
Returns
IADC reference voltage in millivolts.

◆ IADC_pullSingleFifoData()

uint32_t IADC_pullSingleFifoData ( IADC_TypeDef *  iadc)
inline

Pull data from single data FIFO.

If showId was set when initializing single mode, the results will contain the ID (0x20).

Note
Check data valid flag before calling this function.
Parameters
[in]iadcPointer to IADC peripheral register block.
Returns
Single conversion data.

◆ IADC_readSingleData()

uint32_t IADC_readSingleData ( IADC_TypeDef *  iadc)
inline

Read most recent single conversion data.

If showId was set when initializing single mode, the data will contain the ID (0x20). Calling this function will not affect the state of the single data FIFO.

Note
Check data valid flag before calling this function.
Parameters
[in]iadcPointer to IADC peripheral register block.
Returns
Single conversion data.

◆ IADC_pullScanFifoData()

uint32_t IADC_pullScanFifoData ( IADC_TypeDef *  iadc)
inline

Pull data from scan data FIFO.

If showId was set for the scan entry initialization, the data will contain the ID of the scan entry.

Note
Check data valid flag before calling this function.
Parameters
[in]iadcPointer to IADC peripheral register block.
Returns
Scan conversion data.

◆ IADC_readScanData()

uint32_t IADC_readScanData ( IADC_TypeDef *  iadc)
inline

Read most recent scan conversion data.

If showId was set for the scan entry initialization, the data will contain the ID of the scan entry. Calling this function will not affect the state of the scan data FIFO.

Note
Check data valid flag before calling this function.
Parameters
[in]iadcPointer to IADC peripheral register block.
Returns
Scan conversion data.

◆ IADC_clearInt()

void IADC_clearInt ( IADC_TypeDef *  iadc,
uint32_t  flags 
)
inline

Clear one or more pending IADC interrupts.

Parameters
[in]iadcPointer to IADC peripheral register block.
[in]flagsPending IADC interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the IADC module (IADC_IF_nnn).

◆ IADC_disableInt()

void IADC_disableInt ( IADC_TypeDef *  iadc,
uint32_t  flags 
)
inline

Disable one or more IADC interrupts.

Parameters
[in]iadcPointer to IADC peripheral register block.
[in]flagsIADC interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the IADC module (IADC_IF_nnn).

◆ IADC_enableInt()

void IADC_enableInt ( IADC_TypeDef *  iadc,
uint32_t  flags 
)
inline

Enable one or more IADC interrupts.

Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. Consider using IADC_intClear() prior to enabling if such a pending interrupt should be ignored.
Parameters
[in]iadcPointer to IADC peripheral register block.
[in]flagsIADC interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the IADC module (IADC_IF_nnn).

◆ IADC_getInt()

uint32_t IADC_getInt ( IADC_TypeDef *  iadc)
inline

Get pending IADC interrupt flags.

Note
The event bits are not cleared by the use of this function.
Parameters
[in]iadcPointer to IADC peripheral register block.
Returns
IADC interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the IADC module (IADC_IF_nnn).

◆ IADC_getEnabledInt()

uint32_t IADC_getEnabledInt ( IADC_TypeDef *  iadc)
inline

Get enabled and pending IADC interrupt flags.

Useful for handling more interrupt sources in the same interrupt handler.

Note
Interrupt flags are not cleared by the use of this function.
Parameters
[in]iadcPointer to IADC peripheral register block.
Returns
Pending and enabled IADC interrupt sources. The return value is the bitwise AND combination of
  • the OR combination of enabled interrupt sources in IADCx_IEN_nnn register (IADCx_IEN_nnn) and
  • the OR combination of valid interrupt flags of the IADC module (IADCx_IF_nnn).

◆ IADC_setInt()

void IADC_setInt ( IADC_TypeDef *  iadc,
uint32_t  flags 
)
inline

Set one or more pending IADC interrupts from SW.

Parameters
[in]iadcPointer to IADC peripheral register block.
[in]flagsIADC interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the IADC module (IADC_IF_nnn).

◆ IADC_command()

void IADC_command ( IADC_TypeDef *  iadc,
IADC_Cmd_t  cmd 
)
inline

Start/stop scan sequence, single conversion and/or timer.

Parameters
[in]iadcPointer to IADC peripheral register block.
[in]cmdCommand to be performed.

◆ IADC_getScanMask()

uint32_t IADC_getScanMask ( IADC_TypeDef *  iadc)
inline

Get the scan mask currently used in the IADC.

Parameters
[in]iadcPointer to IADC peripheral register block.
Returns
Mask of scan table entries currently included in scan.

◆ IADC_getStatus()

uint32_t IADC_getStatus ( IADC_TypeDef *  iadc)
inline

Get status bits of IADC.

Parameters
[in]iadcPointer to IADC peripheral register block.
Returns
IADC status bits

◆ IADC_getSingleFifoCnt()

uint8_t IADC_getSingleFifoCnt ( IADC_TypeDef *  iadc)
inline

Get the number of elements in the IADC single FIFO.

Parameters
[in]iadcPointer to IADC peripheral register block.
Returns
Number of elements in single FIFO

◆ IADC_getScanFifoCnt()

uint8_t IADC_getScanFifoCnt ( IADC_TypeDef *  iadc)
inline

Get the number of elements in the IADC scan FIFO.

Parameters
[in]iadcPointer to IADC peripheral register block.
Returns
Number of elements in scan FIFO

◆ IADC_portPinToNegInput()

IADC_NegInput_t IADC_portPinToNegInput ( GPIO_Port_TypeDef  port,
uint8_t  pin 
)
inline

Convert the GPIO port/pin to IADC negative input selection.

Parameters
[in]portGPIO port
[in]pinGPIO in
Returns
IADC negative input selection

◆ IADC_portPinToPosInput()

IADC_PosInput_t IADC_portPinToPosInput ( GPIO_Port_TypeDef  port,
uint8_t  pin 
)
inline

Convert the GPIO port/pin to IADC positive input selection.

Parameters
[in]portGPIO port
[in]pinGPIO in
Returns
IADC positive input selection

Macro Definition Documentation

◆ IADC_INIT_DEFAULT

#define IADC_INIT_DEFAULT
Value:
{ \
false, /* IADC clock not disabled on PRS0*/ \
false, /* IADC clock not disabled on PRS1 */ \
false, /* Do not halt during debug */ \
iadcWarmupNormal, /* IADC shutdown after each conversion. */ \
0, /* Calculate timebase. */ \
0, /* Max IADC clock rate. */ \
_IADC_TIMER_TIMER_DEFAULT, /* Use HW default value. */ \
_IADC_CMPTHR_ADGT_DEFAULT, /* Use HW default value. */ \
_IADC_CMPTHR_ADLT_DEFAULT, /* Use HW default value. */ \
}

Default config for IADC init structure.

◆ IADC_CONFIG_DEFAULT

#define IADC_CONFIG_DEFAULT
Value:
{ \
iadcCfgModeNormal, /* Normal mode for IADC. */ \
iadcCfgOsrHighSpeed2x, /* 2x high speed over sampling. */ \
iadcCfgOsrHighAccuracy92x, /* 92x high accuracy over sampling. */ \
iadcCfgAnalogGain1x, /* 1x analog gain. */ \
iadcCfgReferenceInt1V2, /* Internal 1.2V band gap reference. */ \
iadcCfgTwosCompAuto, /* Automatic Two's Complement. */ \
0, /* Max IADC analog clock rate. */ \
1210, /* Vref expressed in millivolts. */ \
iadcDigitalAverage1 /* No averaging. */ \
}

Default IADC config structure.

◆ IADC_ALLCONFIGS_DEFAULT

#define IADC_ALLCONFIGS_DEFAULT
Value:
{ \
{ \
IADC_CONFIG_DEFAULT, \
IADC_CONFIG_DEFAULT \
} \
}

Default IADC sructure for all configs.

◆ IADC_INITSCAN_DEFAULT

#define IADC_INITSCAN_DEFAULT
Value:
{ \
iadcAlignRight12, /* Results 12-bit right aligned */ \
false, /* Do not show ID in result */ \
iadcFifoCfgDvl4, /* Use HW default value. */ \
false, /* Do not wake up DMA on scan FIFO DVL */ \
iadcTriggerSelImmediate, /* Start scan immediately on trigger */ \
iadcTriggerActionOnce, /* Convert once on scan trigger */ \
false /* Do not start scan queue */ \
}

Default config for IADC scan init structure.

◆ IADC_INITSINGLE_DEFAULT

#define IADC_INITSINGLE_DEFAULT
Value:
{ \
iadcAlignRight12, /* Results 12-bit right aligned */ \
false, /* Do not show ID in result */ \
iadcFifoCfgDvl4, /* Use HW default value. */ \
false, /* Do not wake up DMA on single FIFO DVL */ \
iadcTriggerSelImmediate, /* Start single immediately on trigger */ \
iadcTriggerActionOnce, /* Convert once on single trigger */ \
false, /* No tailgating */ \
false /* Do not start single queue */ \
}

Default config for IADC single init structure.

◆ IADC_SINGLEINPUT_DEFAULT

#define IADC_SINGLEINPUT_DEFAULT
Value:
{ \
iadcNegInputGnd, /* Negative input GND */ \
iadcPosInputGnd, /* Positive input GND */ \
0, /* Config 0 */ \
false /* Do not compare results */ \
}

Default config for IADC single input structure.

◆ IADC_SCANTABLEENTRY_DEFAULT

#define IADC_SCANTABLEENTRY_DEFAULT
Value:
{ \
iadcNegInputGnd,/* Negative input GND */ \
iadcPosInputGnd,/* Positive input GND */ \
0, /* Config 0 */ \
false, /* Do not compare results */ \
false /* Do not include in scan */ \
}

Default config for IADC scan table entry structure.

◆ IADC_SCANTABLE_DEFAULT

#define IADC_SCANTABLE_DEFAULT
Value:
{ \
{ \
IADC_SCANTABLEENTRY_DEFAULT, \
IADC_SCANTABLEENTRY_DEFAULT, \
IADC_SCANTABLEENTRY_DEFAULT, \
IADC_SCANTABLEENTRY_DEFAULT, \
IADC_SCANTABLEENTRY_DEFAULT, \
IADC_SCANTABLEENTRY_DEFAULT, \
IADC_SCANTABLEENTRY_DEFAULT, \
IADC_SCANTABLEENTRY_DEFAULT, \
IADC_SCANTABLEENTRY_DEFAULT, \
IADC_SCANTABLEENTRY_DEFAULT, \
IADC_SCANTABLEENTRY_DEFAULT, \
IADC_SCANTABLEENTRY_DEFAULT, \
IADC_SCANTABLEENTRY_DEFAULT, \
IADC_SCANTABLEENTRY_DEFAULT, \
IADC_SCANTABLEENTRY_DEFAULT, \
IADC_SCANTABLEENTRY_DEFAULT \
} \
}

Default IADC structure for scan table.

Enumeration Type Documentation

◆ IADC_Warmup_t

Warm-up mode.

Enumerator
iadcWarmupNormal 

IADC shutdown after each conversion.

iadcWarmupKeepInStandby 

ADC is kept in standby mode between conversion.


iadcWarmupKeepWarm 

ADC and reference selected for scan mode kept warmup, allowing continuous conversion.

◆ IADC_Alignment_t

IADC result alignment.

Enumerator
iadcAlignRight12 

IADC results 12-bit right aligned

iadcAlignLeft12 

IADC results 12-bit left aligned

iadcAlignRight16 

IADC results 16-bit right aligned

iadcAlignLeft16 

IADC results 16-bit left aligned

iadcAlignRight20 

IADC results 20-bit right aligned

iadcAlignLeft20 

IADC results 20-bit left aligned

◆ IADC_NegInput_t

IADC negative input selection.

Enumerator
iadcNegInputGnd 

Ground

iadcNegInputGndaux 

Ground using even mux.

iadcNegInputDac1 

Direct connection to DAC_1 input pin.

iadcNegInputPadAna1 

Direct connection to Pad_ana_1 input pin.

iadcNegInputPortAPin0 

GPIO port A pin 0.

iadcNegInputPortAPin1 

GPIO port A pin 1.

iadcNegInputPortAPin2 

GPIO port A pin 2.

iadcNegInputPortAPin3 

GPIO port A pin 3.

iadcNegInputPortAPin4 

GPIO port A pin 4.

iadcNegInputPortAPin5 

GPIO port A pin 5.

iadcNegInputPortAPin6 

GPIO port A pin 6.

iadcNegInputPortAPin7 

GPIO port A pin 7.

iadcNegInputPortAPin8 

GPIO port A pin 8.

iadcNegInputPortAPin9 

GPIO port A pin 9.

iadcNegInputPortAPin10 

GPIO port A pin 10.

iadcNegInputPortAPin11 

GPIO port A pin 11.

iadcNegInputPortAPin12 

GPIO port A pin 12.

iadcNegInputPortAPin13 

GPIO port A pin 13.

iadcNegInputPortAPin14 

GPIO port A pin 14.

iadcNegInputPortAPin15 

GPIO port A pin 15.

iadcNegInputPortBPin0 

GPIO port B pin 0.

iadcNegInputPortBPin1 

GPIO port B pin 1.

iadcNegInputPortBPin2 

GPIO port B pin 2.

iadcNegInputPortBPin3 

GPIO port B pin 3.

iadcNegInputPortBPin4 

GPIO port B pin 4.

iadcNegInputPortBPin5 

GPIO port B pin 5.

iadcNegInputPortBPin6 

GPIO port B pin 6.

iadcNegInputPortBPin7 

GPIO port B pin 7.

iadcNegInputPortBPin8 

GPIO port B pin 8.

iadcNegInputPortBPin9 

GPIO port B pin 9.

iadcNegInputPortBPin10 

GPIO port B pin 10.

iadcNegInputPortBPin11 

GPIO port B pin 11.

iadcNegInputPortBPin12 

GPIO port B pin 12.

iadcNegInputPortBPin13 

GPIO port B pin 13.

iadcNegInputPortBPin14 

GPIO port B pin 14.

iadcNegInputPortBPin15 

GPIO port B pin 15.

iadcNegInputPortCPin0 

GPIO port C pin 0.

iadcNegInputPortCPin1 

GPIO port C pin 1.

iadcNegInputPortCPin2 

GPIO port C pin 2.

iadcNegInputPortCPin3 

GPIO port C pin 3.

iadcNegInputPortCPin4 

GPIO port C pin 4.

iadcNegInputPortCPin5 

GPIO port C pin 5.

iadcNegInputPortCPin6 

GPIO port C pin 6.

iadcNegInputPortCPin7 

GPIO port C pin 7.

iadcNegInputPortCPin8 

GPIO port C pin 8.

iadcNegInputPortCPin9 

GPIO port C pin 9.

iadcNegInputPortCPin10 

GPIO port C pin 10.

iadcNegInputPortCPin11 

GPIO port C pin 11.

iadcNegInputPortCPin12 

GPIO port C pin 12.

iadcNegInputPortCPin13 

GPIO port C pin 13.

iadcNegInputPortCPin14 

GPIO port C pin 14.

iadcNegInputPortCPin15 

GPIO port C pin 15.

iadcNegInputPortDPin0 

GPIO port D pin 0.

iadcNegInputPortDPin1 

GPIO port D pin 1.

iadcNegInputPortDPin2 

GPIO port D pin 2.

iadcNegInputPortDPin3 

GPIO port D pin 3.

iadcNegInputPortDPin4 

GPIO port D pin 4.

iadcNegInputPortDPin5 

GPIO port D pin 5.

iadcNegInputPortDPin6 

GPIO port D pin 6.

iadcNegInputPortDPin7 

GPIO port D pin 7.

iadcNegInputPortDPin8 

GPIO port D pin 8.

iadcNegInputPortDPin9 

GPIO port D pin 9.

iadcNegInputPortDPin10 

GPIO port D pin 10.

iadcNegInputPortDPin11 

GPIO port D pin 11.

iadcNegInputPortDPin12 

GPIO port D pin 12.

iadcNegInputPortDPin13 

GPIO port D pin 13.

iadcNegInputPortDPin14 

GPIO port D pin 14.

iadcNegInputPortDPin15 

GPIO port D pin 15.

◆ IADC_PosInput_t

IADC positive port selection.

Enumerator
iadcPosInputGnd 

Ground

iadcPosInputAvdd 

Avdd / 4

iadcPosInputVddio 

Vddio / 4

iadcPosInputVss 

Vss

iadcPosInputVssaux 

Vss

iadcPosInputDvdd 

Dvdd / 4

iadcPosInputDecouple 

Decouple

iadcPosInputDac0 

Direct connection to DAC_0 input pin.

iadcPosInputPadAna0 

Direct connection to Pad_ana_0 input pin.

iadcPosInputPortAPin0 

GPIO port A pin 0.

iadcPosInputPortAPin1 

GPIO port A pin 1.

iadcPosInputPortAPin2 

GPIO port A pin 2.

iadcPosInputPortAPin3 

GPIO port A pin 3.

iadcPosInputPortAPin4 

GPIO port A pin 4.

iadcPosInputPortAPin5 

GPIO port A pin 5.

iadcPosInputPortAPin6 

GPIO port A pin 6.

iadcPosInputPortAPin7 

GPIO port A pin 7.

iadcPosInputPortAPin8 

GPIO port A pin 8.

iadcPosInputPortAPin9 

GPIO port A pin 9.

iadcPosInputPortAPin10 

GPIO port A pin 10.

iadcPosInputPortAPin11 

GPIO port A pin 11.

iadcPosInputPortAPin12 

GPIO port A pin 12.

iadcPosInputPortAPin13 

GPIO port A pin 13.

iadcPosInputPortAPin14 

GPIO port A pin 14.

iadcPosInputPortAPin15 

GPIO port A pin 15.

iadcPosInputPortBPin0 

GPIO port B pin 0.

iadcPosInputPortBPin1 

GPIO port B pin 1.

iadcPosInputPortBPin2 

GPIO port B pin 2.

iadcPosInputPortBPin3 

GPIO port B pin 3.

iadcPosInputPortBPin4 

GPIO port B pin 4.

iadcPosInputPortBPin5 

GPIO port B pin 5.

iadcPosInputPortBPin6 

GPIO port B pin 6.

iadcPosInputPortBPin7 

GPIO port B pin 7.

iadcPosInputPortBPin8 

GPIO port B pin 8.

iadcPosInputPortBPin9 

GPIO port B pin 9.

iadcPosInputPortBPin10 

GPIO port B pin 10.

iadcPosInputPortBPin11 

GPIO port B pin 11.

iadcPosInputPortBPin12 

GPIO port B pin 12.

iadcPosInputPortBPin13 

GPIO port B pin 13.

iadcPosInputPortBPin14 

GPIO port B pin 14.

iadcPosInputPortBPin15 

GPIO port B pin 15.

iadcPosInputPortCPin0 

GPIO port C pin 0.

iadcPosInputPortCPin1 

GPIO port C pin 1.

iadcPosInputPortCPin2 

GPIO port C pin 2.

iadcPosInputPortCPin3 

GPIO port C pin 3.

iadcPosInputPortCPin4 

GPIO port C pin 4.

iadcPosInputPortCPin5 

GPIO port C pin 5.

iadcPosInputPortCPin6 

GPIO port C pin 6.

iadcPosInputPortCPin7 

GPIO port C pin 7.

iadcPosInputPortCPin8 

GPIO port C pin 8.

iadcPosInputPortCPin9 

GPIO port C pin 9.

iadcPosInputPortCPin10 

GPIO port C pin 10.

iadcPosInputPortCPin11 

GPIO port C pin 11.

iadcPosInputPortCPin12 

GPIO port C pin 12.

iadcPosInputPortCPin13 

GPIO port C pin 13.

iadcPosInputPortCPin14 

GPIO port C pin 14.

iadcPosInputPortCPin15 

GPIO port C pin 15.

iadcPosInputPortDPin0 

GPIO port D pin 0.

iadcPosInputPortDPin1 

GPIO port D pin 1.

iadcPosInputPortDPin2 

GPIO port D pin 2.

iadcPosInputPortDPin3 

GPIO port D pin 3.

iadcPosInputPortDPin4 

GPIO port D pin 4.

iadcPosInputPortDPin5 

GPIO port D pin 5.

iadcPosInputPortDPin6 

GPIO port D pin 6.

iadcPosInputPortDPin7 

GPIO port D pin 7.

iadcPosInputPortDPin8 

GPIO port D pin 8.

iadcPosInputPortDPin9 

GPIO port D pin 9.

iadcPosInputPortDPin10 

GPIO port D pin 10.

iadcPosInputPortDPin11 

GPIO port D pin 11.

iadcPosInputPortDPin12 

GPIO port D pin 12.

iadcPosInputPortDPin13 

GPIO port D pin 13.

iadcPosInputPortDPin14 

GPIO port D pin 14.

iadcPosInputPortDPin15 

GPIO port D pin 15.

◆ IADC_Cmd_t

enum IADC_Cmd_t

IADC Commands.

Enumerator
iadcCmdStartSingle 

Start single queue

iadcCmdStopSingle 

Stop single queue

iadcCmdStartScan 

Start scan queue

iadcCmdStopScan 

Stop scan queue

iadcCmdEnableTimer 

Enable Timer

iadcCmdDisableTimer 

Disable Timer

◆ IADC_CfgAdcMode_t

IADC Configuration.

Enumerator
iadcCfgModeNormal 

Normal mode

iadcCfgModeHighSpeed 

High Speed mode

iadcCfgModeHighAccuracy 

High Accuracy mode

◆ IADC_CfgOsrHighSpeed_t

IADC Over sampling rate for high speed.

Enumerator
iadcCfgOsrHighSpeed2x 

High speed oversampling of 2x.

iadcCfgOsrHighSpeed4x 

High speed oversampling of 4x.

iadcCfgOsrHighSpeed8x 

High speed oversampling of 8x.

iadcCfgOsrHighSpeed16x 

High speed oversampling of 16x.

iadcCfgOsrHighSpeed32x 

High speed oversampling of 32x.

iadcCfgOsrHighSpeed64x 

High speed oversampling of 64x.

◆ IADC_CfgOsrHighAccuracy_t

IADC Over sampling rate for high accuracy.

Enumerator
iadcCfgOsrHighAccuracy16x 

High accuracy oversampling of 16x.

iadcCfgOsrHighAccuracy32x 

High accuracy oversampling of 32x.

iadcCfgOsrHighAccuracy64x 

High accuracy oversampling of 64x.

iadcCfgOsrHighAccuracy92x 

High accuracy oversampling of 92x.

iadcCfgOsrHighAccuracy128x 

High accuracy oversampling of 128x.

iadcCfgOsrHighAccuracy256x 

High accuracy oversampling of 256x.

◆ IADC_CfgAnalogGain_t

IADC Analog Gain.

Enumerator
iadcCfgAnalogGain0P5x 

Analog gain of 0.5x.

iadcCfgAnalogGain1x 

Analog gain of 1x.

iadcCfgAnalogGain2x 

Analog gain of 2x.

iadcCfgAnalogGain3x 

Analog gain of 3x.

iadcCfgAnalogGain4x 

Analog gain of 4x.

◆ IADC_CfgReference_t

IADC Reference.

Enumerator
iadcCfgReferenceInt1V2 

Internal 1.2V Band Gap Reference (buffered) to ground.

iadcCfgReferenceExt1V25 

External reference (unbuffered) VREFP to VREFN.

Up to 1.25V.

iadcCfgReferenceExt2V5 

External reference (unbuffered) VREFP to VREFN.

Up to 1.25V.

iadcCfgReferenceVddx 

VDDX (unbuffered) to ground.

iadcCfgReferenceVddX0P8Buf 

0.8 * VDDX (buffered) to ground.

◆ IADC_CfgTwosComp_t

IADC Two's complement results.

Enumerator
iadcCfgTwosCompAuto 

Automatic.

Single ended => Unipolar, Differential => Bipolar

iadcCfgTwosCompUnipolar 

All results in unipolar format.

Negative diff input gives 0 as result.

iadcCfgTwosCompBipolar 

All results in bipolar (2's complement) format.

Half range for SE.

◆ IADC_TriggerSel_t

IADC trigger action.

Enumerator
iadcTriggerSelImmediate 

Start single/scan queue immediately.

iadcTriggerSelTimer 

Timer starts single/scan queue.

iadcTriggerSelPrs0SameClk 

PRS0 from timer in same clock group starts single/scan queue

iadcTriggerSelPrs0PosEdge 

PRS0 positive edge starts single/scan queue

iadcTriggerSelPrs0NegEdge 

PRS0 negative edge starts single/scan queue

iadcTriggerSelLesense 

LESENSE starts scan queue

◆ IADC_TriggerAction_t

IADC trigger action.

Enumerator
iadcTriggerActionOnce 

Convert single/scan queue once per trigger

iadcTriggerActionContinuous 

Convert single/scan queue continuously

◆ IADC_FifoCfgDvl_t

IADC data valid level before requesting DMA transfer.

Enumerator
iadcFifoCfgDvl1 

Data valid level is 1 before requesting DMA transfer.

iadcFifoCfgDvl2 

Data valid level is 2 before requesting DMA transfer.

iadcFifoCfgDvl3 

Data valid level is 3 before requesting DMA transfer.

iadcFifoCfgDvl4 

Data valid level is 4 before requesting DMA transfer.

iadcFifoCfgDvl5 

Data valid level is 5 before requesting DMA transfer.

iadcFifoCfgDvl6 

Data valid level is 6 before requesting DMA transfer.

iadcFifoCfgDvl7 

Data valid level is 7 before requesting DMA transfer.

◆ IADC_DigitalAveraging_t

IADC digital averaging function.

Enumerator
iadcDigitalAverage1 

Average over 1 sample (no averaging).

iadcDigitalAverage2 

Average over 2 samples.

iadcDigitalAverage4 

Average over 4 samples.

iadcDigitalAverage8 

Average over 8 samples.

iadcDigitalAverage16 

Average over 16 samples.