MSC_ExecConfig_TypeDef Struct Reference
Code execution configuration.
#include <em_msc.h>
Data Fields | |
bool | scbtEn |
Enable Suppressed Conditional Branch Target Prefetch. | |
bool | prefetchEn |
Enable MSC prefetching. | |
bool | ifcDis |
Disable instruction cache. | |
bool | aiDis |
Disable automatic cache invalidation on write or erase. | |
bool | iccDis |
Disable automatic caching of fetches in interrupt context. | |
bool | useHprot |
Use ahb_hprot to determine if the instruction is cacheable or not. | |
Code execution configuration.
Field Documentation
◆ scbtEn
bool MSC_ExecConfig_TypeDef::scbtEn |
Enable Suppressed Conditional Branch Target Prefetch.
◆ prefetchEn
bool MSC_ExecConfig_TypeDef::prefetchEn |
Enable MSC prefetching.
◆ ifcDis
bool MSC_ExecConfig_TypeDef::ifcDis |
Disable instruction cache.
◆ aiDis
bool MSC_ExecConfig_TypeDef::aiDis |
Disable automatic cache invalidation on write or erase.
◆ iccDis
bool MSC_ExecConfig_TypeDef::iccDis |
Disable automatic caching of fetches in interrupt context.
◆ useHprot
bool MSC_ExecConfig_TypeDef::useHprot |
Use ahb_hprot to determine if the instruction is cacheable or not.