KEYSCAN - Keyboard Scan
Description
Keyscan (KEYSCAN) Peripheral API.
This module contains functions to control the KEYSCAN peripheral of Silicon Labs 32-bit MCUs and SoCs. The KEYSCAN module connects through rows and columns of GPIOs to an external mechanical keypad.
Data Structures |
|
| struct | sl_keyscan_config_t |
|
KEYSCAN configuration structure.
|
|
Functions |
|
| void | sl_keyscan_init (const sl_keyscan_config_t *p_config) |
|
Initializes KEYSCAN module.
|
|
| void | sl_keyscan_enable (void) |
|
Enables KEYSCAN module.
|
|
| void | sl_keyscan_disable (void) |
|
Disables KEYSCAN module.
|
|
| void | sl_keyscan_reset (void) |
|
Restores KEYSCAN to its reset state.
|
|
| void | sl_keyscan_wait_ready (void) |
|
Waits for the KEYSCAN to complete reseting or disabling procedure.
|
|
| void | sl_keyscan_wait_sync (void) |
|
Waits for the KEYSCAN to complete all synchronization of register changes and commands.
|
|
| void | sl_keyscan_start_scan (void) |
|
Starts KEYSCAN scan.
|
|
| void | sl_keyscan_stop_scan (void) |
|
Stops the KEYSCAN scan.
|
|
| uint32_t | sl_keyscan_get_status (void) |
|
Gets KEYSCAN STATUS register value.
|
|
| void | sl_keyscan_enable_interrupts (uint32_t flags) |
|
Enables one or more KEYSCAN interrupts.
|
|
| void | sl_keyscan_disable_interrupts (uint32_t flags) |
|
Disables one or more KEYSCAN interrupts.
|
|
| void | sl_keyscan_clear_interrupts (uint32_t flags) |
|
Clears one or more pending KEYSCAN interrupts.
|
|
| uint32_t | sl_keyscan_get_interrupts (void) |
|
Gets pending KEYSCAN interrupt flags.
|
|
| uint32_t | sl_keyscan_get_enabled_interrupts (void) |
|
Gets enabled and pending KEYSCAN interrupt flags.
|
|
| void | sl_keyscan_set_interrupts (uint32_t flags) |
|
Sets one or more pending KEYSCAN interrupts from Software.
|
|
Macros |
|
| #define | KEYSCAN_CONFIG_DEFAULT |
|
Suggested default values for KEYSCAN configuration structure.
|
|
Enumerations |
|
| enum |
sl_keyscan_delay_t
{
SL_KEYSCAN_DELAY_2MS = 0, SL_KEYSCAN_DELAY_4MS , SL_KEYSCAN_DELAY_6MS , SL_KEYSCAN_DELAY_8MS , SL_KEYSCAN_DELAY_10MS , SL_KEYSCAN_DELAY_12MS , SL_KEYSCAN_DELAY_14MS , SL_KEYSCAN_DELAY_16MS , SL_KEYSCAN_DELAY_18MS , SL_KEYSCAN_DELAY_20MS , SL_KEYSCAN_DELAY_22MS , SL_KEYSCAN_DELAY_24MS , SL_KEYSCAN_DELAY_26MS , SL_KEYSCAN_DELAY_28MS , SL_KEYSCAN_DELAY_30MS , SL_KEYSCAN_DELAY_32MS } |
|
KEYSCAN configuration delay values.
|
|
Function Documentation
◆ sl_keyscan_init()
| void sl_keyscan_init | ( | const sl_keyscan_config_t * |
p_config
|
) |
Initializes KEYSCAN module.
- Parameters
-
[in] p_configA pointer to the KEYSCAN initialization structure variable.
◆ sl_keyscan_enable()
| void sl_keyscan_enable | ( | void |
|
) |
Enables KEYSCAN module.
◆ sl_keyscan_disable()
| void sl_keyscan_disable | ( | void |
|
) |
Disables KEYSCAN module.
- Note
- The disabling of the module could take some time. This function will not wait for the disabling to finish before returning. Use the function sl_keyscan_wait_ready to wait for the module to be fully disable.
◆ sl_keyscan_reset()
| void sl_keyscan_reset | ( | void |
|
) |
Restores KEYSCAN to its reset state.
- Note
- The register STATUS get reset value after enabling the module because it is of type RSYNC
- The resetting of the module could take some time. This function will not wait for the resetting to finish before returning. Use the function sl_keyscan_wait_ready to wait for the module to be fully reset.
◆ sl_keyscan_wait_ready()
|
inline |
Waits for the KEYSCAN to complete reseting or disabling procedure.
◆ sl_keyscan_wait_sync()
|
inline |
Waits for the KEYSCAN to complete all synchronization of register changes and commands.
◆ sl_keyscan_start_scan()
|
inline |
Starts KEYSCAN scan.
- Note
- This function will send a start command to the KEYSCAN peripheral. The sl_keyscan_wait_sync function can be used to wait for the start command to be executed.
- This function requires the KEYSCAN to be enabled.
◆ sl_keyscan_stop_scan()
|
inline |
Stops the KEYSCAN scan.
- Note
- This function will send a stop command to the KEYSCAN peripheral. The sl_keyscan_wait_sync function can be used to wait for the stop command to be executed.
- This function requires the KEYSCAN to be enabled.
◆ sl_keyscan_get_status()
|
inline |
Gets KEYSCAN STATUS register value.
- Returns
- Current STATUS register value.
◆ sl_keyscan_enable_interrupts()
|
inline |
Enables one or more KEYSCAN interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using sl_keyscan_clear_interrupts prior to enabling the interrupt.
- Parameters
-
[in] flagsKEYSCAN interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources.
◆ sl_keyscan_disable_interrupts()
|
inline |
Disables one or more KEYSCAN interrupts.
- Parameters
-
[in] flagsKEYSCAN interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt sources.
◆ sl_keyscan_clear_interrupts()
|
inline |
Clears one or more pending KEYSCAN interrupts.
- Parameters
-
[in] flagsKEYSCAN interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources.
◆ sl_keyscan_get_interrupts()
|
inline |
Gets pending KEYSCAN interrupt flags.
- Note
- Event bits are not cleared by using this function.
- Returns
- Pending KEYSCAN interrupt sources. Returns a set of interrupt flags OR-ed together for multiple interrupt sources.
◆ sl_keyscan_get_enabled_interrupts()
|
inline |
Gets enabled and pending KEYSCAN interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Note
- Interrupt flags are not cleared by using this function.
- Returns
-
Pending and enabled KEYSCAN interrupt sources. The return value is the bitwise AND of
- the enabled interrupt sources in KEYSCAN_IEN and
- the pending interrupt flags KEYSCAN_IF.
◆ sl_keyscan_set_interrupts()
|
inline |
Sets one or more pending KEYSCAN interrupts from Software.
- Parameters
-
[in] flagsKEYSCAN interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources.
Macro Definition Documentation
◆ KEYSCAN_CONFIG_DEFAULT
| #define KEYSCAN_CONFIG_DEFAULT |
Suggested default values for KEYSCAN configuration structure.
Enumeration Type Documentation
◆ sl_keyscan_delay_t
| enum sl_keyscan_delay_t |
KEYSCAN configuration delay values.