ACMP_Init_TypeDef Struct Reference
ACMP initialization structure.
#include <em_acmp.h>
Data Fields |
|
| uint32_t | biasProg |
|
Bias current.
|
|
| ACMP_InputRange_TypeDef | inputRange |
|
Input range.
|
|
| ACMP_Accuracy_TypeDef | accuracy |
|
ACMP accuracy mode.
|
|
| ACMP_HysteresisLevel_TypeDef | hysteresisLevel |
|
Hysteresis level.
|
|
| bool | inactiveValue |
|
Inactive value emitted by ACMP during warmup.
|
|
| uint32_t | vrefDiv |
|
VDD division factor.
|
|
| bool | enable |
|
If true, ACMP is enabled after configuration.
|
|
ACMP initialization structure.
Field Documentation
◆ biasProg
| uint32_t ACMP_Init_TypeDef::biasProg |
Bias current.
See the ACMP chapter about bias and response time in the reference manual for details. Valid values are in the range 0-7.
◆ inputRange
| ACMP_InputRange_TypeDef ACMP_Init_TypeDef::inputRange |
Input range.
Adjust this setting to optimize the performance for a given input voltage range.
◆ accuracy
| ACMP_Accuracy_TypeDef ACMP_Init_TypeDef::accuracy |
ACMP accuracy mode.
Select the accuracy mode that matches the required current usage and accuracy requirement. Low accuracy consumes less current while high accuracy consumes more current.
◆ hysteresisLevel
| ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel |
Hysteresis level.
◆ inactiveValue
| bool ACMP_Init_TypeDef::inactiveValue |
Inactive value emitted by ACMP during warmup.
◆ vrefDiv
| uint32_t ACMP_Init_TypeDef::vrefDiv |
VDD division factor.
VREFOUT = VREFIN * (VREFDIV / 63). Valid values are in the 0-63 range.
◆ enable
| bool ACMP_Init_TypeDef::enable |
If true, ACMP is enabled after configuration.