sl_led_rgb_pwm_t Struct Reference
A Simple RGB LED PWM instance.
#include <sl_simple_rgb_pwm_led.h>
Data Fields | |
sl_led_t | led_common |
Inherit from the Common LED Driver. | |
void(* | set_rgb_color )(void *context, uint16_t red, uint16_t green, uint16_t blue) |
Member function to set RGB. | |
void(* | get_rgb_color )(void *context, uint16_t *red, uint16_t *green, uint16_t *blue) |
Member function to get RGB. | |
A Simple RGB LED PWM instance.
Field Documentation
◆ led_common
sl_led_t sl_led_rgb_pwm_t::led_common |
Inherit from the Common LED Driver.
◆ set_rgb_color
void(* sl_led_rgb_pwm_t::set_rgb_color) (void *context, uint16_t red, uint16_t green, uint16_t blue) |
Member function to set RGB.
◆ get_rgb_color
void(* sl_led_rgb_pwm_t::get_rgb_color) (void *context, uint16_t *red, uint16_t *green, uint16_t *blue) |
Member function to get RGB.