sl_simple_button_context_t Struct Reference
A Simple BUTTON instance.
#include <sl_simple_button.h>
Data Fields | |
sl_button_state_t | state |
Current button state. | |
uint16_t | history |
History of button states. | |
GPIO_Port_TypeDef | port |
Button port. | |
uint8_t | pin |
Button pin. | |
sl_button_mode_t | mode |
Mode of operation */. | |
A Simple BUTTON instance.
Field Documentation
◆ state
sl_button_state_t sl_simple_button_context_t::state |
Current button state.
◆ history
uint16_t sl_simple_button_context_t::history |
History of button states.
◆ port
GPIO_Port_TypeDef sl_simple_button_context_t::port |
Button port.
◆ pin
uint8_t sl_simple_button_context_t::pin |
Button pin.
◆ mode
sl_button_mode_t sl_simple_button_context_t::mode |
Mode of operation */.