Board Control
Description
Functions to control Silicon Labs board features.
Functions | |
sl_status_t | sl_board_configure_vcom (void) |
Configure Virtual COM UART. | |
sl_status_t | sl_board_enable_vcom (void) |
Enable Virtual COM UART. | |
sl_status_t | sl_board_disable_vcom (void) |
Disable Virtual COM UART. | |
sl_status_t | sl_board_enable_sensor (sl_board_sensor_t sensor) |
Enable a sensor. | |
sl_status_t | sl_board_disable_sensor (sl_board_sensor_t sensor) |
Disable a sensor. | |
sl_status_t | sl_board_enable_display (void) |
Enable display. | |
sl_status_t | sl_board_disable_display (void) |
Disable display. | |
sl_status_t | sl_board_enable_memory (sl_board_memory_t memory) |
Enable memory. | |
sl_status_t | sl_board_disable_memory (sl_board_memory_t memory) |
Disable memory. | |
sl_status_t | sl_board_enable_oscillator (sl_board_oscillator_t oscillator) |
Enable an oscillator. | |
sl_status_t | sl_board_disable_oscillator (sl_board_oscillator_t oscillator) |
Disable a oscillator. | |
Enumerations | |
enum | sl_board_sensor_t { SL_BOARD_SENSOR_RHT = (1UL << 0UL), SL_BOARD_SENSOR_LIGHT = (1UL << 1UL), SL_BOARD_SENSOR_PRESSURE = (1UL << 2UL), SL_BOARD_SENSOR_HALL = (1UL << 3UL), SL_BOARD_SENSOR_GAS = (1UL << 4UL), SL_BOARD_SENSOR_IMU = (1UL << 5UL), SL_BOARD_SENSOR_MICROPHONE = (1UL << 6UL) } |
Board Sensor Type. | |
enum | sl_board_memory_t { SL_BOARD_MEMORY_SDCARD = (1UL << 0UL), SL_BOARD_MEMORY_QSPI = (1UL << 1UL) } |
Board Memory Type. | |
enum | sl_board_oscillator_t { SL_BOARD_OSCILLATOR_TCXO = (1UL << 0UL) } |
Board Oscillator Type. | |
Function Documentation
◆ sl_board_configure_vcom()
sl_status_t sl_board_configure_vcom | ( | void |
| ) |
Configure Virtual COM UART.
- Returns
- Status code
- Return values
-
SL_STATUS_OK
VCOM was successfully enabled SL_STATUS_FAIL
Enabling VCOM failed SL_STATUS_NOT_AVAILABLE
VCOM control is not available on this board SL_STATUS_NOT_SUPPORTED
VCOM enabled was not configured
◆ sl_board_enable_vcom()
sl_status_t sl_board_enable_vcom | ( | void |
| ) |
Enable Virtual COM UART.
- Returns
- Status code
- Return values
-
SL_STATUS_OK
VCOM was successfully enabled SL_STATUS_FAIL
Enabling VCOM failed SL_STATUS_NOT_AVAILABLE
VCOM control is not available on this board
◆ sl_board_disable_vcom()
sl_status_t sl_board_disable_vcom | ( | void |
| ) |
Disable Virtual COM UART.
- Returns
- Status code
- Return values
-
SL_STATUS_OK
VCOM was successfully disabled SL_STATUS_FAIL
Disabling VCOM failed SL_STATUS_NOT_AVAILABLE
VCOM control is not available on this board
◆ sl_board_enable_sensor()
sl_status_t sl_board_enable_sensor | ( | sl_board_sensor_t | sensor | ) |
Enable a sensor.
- Warning
- On boards 4166A, 4184A, and 4184B sensors
- Pressure Sensor, RH/Temp Sensor, and UV/Ambient Light Sensor;
- UV/Ambient Light Sensor, Hall-effect Sensor, and RH/Temp Sensor;
- Ambient Light Sensor, Hall-effect Sensor, and RH/Temp Sensor respectively, are tied to the same enable pin. Calling the enable function for only one of these sensors has the side-effect of enabling all three; and calling the disable function for only one of them has the side-effect of disabling all three. The latter scenario seems less than desirable.
- Parameters
-
[in] sensor
Sensor to enable
- Returns
- Status code
- Return values
-
SL_STATUS_OK
Sensor was successfully enabled SL_STATUS_FAIL
Enabling sensor failed SL_STATUS_NOT_AVAILABLE
Sensor control is not available on this board
◆ sl_board_disable_sensor()
sl_status_t sl_board_disable_sensor | ( | sl_board_sensor_t | sensor | ) |
Disable a sensor.
- Warning
- On boards 4166A, 4184A, and 4184B sensors
- Pressure Sensor, RH/Temp Sensor, and UV/Ambient Light Sensor;
- UV/Ambient Light Sensor, Hall-effect Sensor, and RH/Temp Sensor;
- Ambient Light Sensor, Hall-effect Sensor, and RH/Temp Sensor respectively, are tied to the same enable pin. Calling the enable function for only one of these sensors has the side-effect of enabling all three; and calling the disable function for only one of them has the side-effect of disabling all three. The latter scenario seems less than desirable.
- Parameters
-
[in] sensor
Sensors to disable
- Returns
- Status code
- Return values
-
SL_STATUS_OK
Sensor was successfully disabled SL_STATUS_FAIL
Disabling sensor failed SL_STATUS_NOT_AVAILABLE
Sensor control is not available on this board
◆ sl_board_enable_display()
sl_status_t sl_board_enable_display | ( | void |
| ) |
Enable display.
- Returns
- Status code
- Return values
-
SL_STATUS_OK
Display was successfully enabled SL_STATUS_FAIL
Enabling display failed SL_STATUS_NOT_AVAILABLE
Display control is not available on this board
◆ sl_board_disable_display()
sl_status_t sl_board_disable_display | ( | void |
| ) |
Disable display.
- Returns
- Status code
- Return values
-
SL_STATUS_OK
Display was successfully disabled SL_STATUS_FAIL
Disabling display failed SL_STATUS_NOT_AVAILABLE
Display control is not available on this board
◆ sl_board_enable_memory()
sl_status_t sl_board_enable_memory | ( | sl_board_memory_t | memory | ) |
Enable memory.
- Parameters
-
[in] memory
Memory to enable
- Returns
- Status code
- Return values
-
SL_STATUS_OK
Memory was successfully enabled SL_STATUS_FAIL
Enabling memory failed SL_STATUS_NOT_AVAILABLE
Memory control is not available on this board
◆ sl_board_disable_memory()
sl_status_t sl_board_disable_memory | ( | sl_board_memory_t | memory | ) |
Disable memory.
- Parameters
-
[in] memory
Memory to disable
- Returns
- Status code
- Return values
-
SL_STATUS_OK
Memory was successfully disabled SL_STATUS_FAIL
Disabling memory failed SL_STATUS_NOT_AVAILABLE
Memory control is not available on this board
◆ sl_board_enable_oscillator()
sl_status_t sl_board_enable_oscillator | ( | sl_board_oscillator_t | oscillator | ) |
Enable an oscillator.
- Parameters
-
[in] oscillator
Oscillator to enable
- Returns
- Status code
- Return values
-
SL_STATUS_OK
Oscillator was successfully enabled SL_STATUS_FAIL
Enabling oscillator failed SL_STATUS_NOT_AVAILABLE
Oscillator control is not available on this board
◆ sl_board_disable_oscillator()
sl_status_t sl_board_disable_oscillator | ( | sl_board_oscillator_t | oscillator | ) |
Disable a oscillator.
- Parameters
-
[in] oscillator
Oscillator to disable
- Returns
- Status code
- Return values
-
SL_STATUS_OK
Oscillator was successfully disabled SL_STATUS_FAIL
Disabling oscillator failed SL_STATUS_NOT_AVAILABLE
Oscillator control is not available on this board
Enumeration Type Documentation
◆ sl_board_sensor_t
enum sl_board_sensor_t |
Board Sensor Type.
◆ sl_board_memory_t
enum sl_board_memory_t |