Asymmetric cryptography
Description
Functions | |
psa_status_t | psa_sign_message (mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *input, size_t input_length, uint8_t *signature, size_t signature_size, size_t *signature_length) |
Sign a message with a private key. | |
psa_status_t | psa_verify_message (mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *input, size_t input_length, const uint8_t *signature, size_t signature_length) |
Verify the signature of a message with a public key, using a hash-and-sign verification algorithm. | |
psa_status_t | psa_sign_hash (mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *hash, size_t hash_length, uint8_t *signature, size_t signature_size, size_t *signature_length) |
Sign a hash or short message with a private key. | |
psa_status_t | psa_verify_hash (mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *hash, size_t hash_length, const uint8_t *signature, size_t signature_length) |
Verify the signature of a hash or short message using a public key. | |
psa_status_t | psa_asymmetric_encrypt (mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *input, size_t input_length, const uint8_t *salt, size_t salt_length, uint8_t *output, size_t output_size, size_t *output_length) |
Encrypt a short message with a public key. | |
psa_status_t | psa_asymmetric_decrypt (mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *input, size_t input_length, const uint8_t *salt, size_t salt_length, uint8_t *output, size_t output_size, size_t *output_length) |
Decrypt a short message with a private key. | |
Function Documentation
◆ psa_sign_message()
psa_status_t psa_sign_message | ( | mbedtls_svc_key_id_t | key, |
psa_algorithm_t | alg, |
||
const uint8_t * | input, |
||
size_t | input_length, |
||
uint8_t * | signature, |
||
size_t | signature_size, |
||
size_t * | signature_length |
||
) |
Sign a message with a private key.
For hash-and-sign algorithms, this includes the hashing step.
- Note
- To perform a multi-part hash-and-sign signature algorithm, first use a multi-part hash operation and then pass the resulting hash to psa_sign_hash(). PSA_ALG_GET_HASH(
alg
) can be used to determine the hash algorithm to use.
- Parameters
-
[in] key
Identifier of the key to use for the operation. It must be an asymmetric key pair. The key must allow the usage PSA_KEY_USAGE_SIGN_MESSAGE. [in] alg
An asymmetric signature algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_SIGN_MESSAGE( alg
) is true), that is compatible with the type ofkey
.[in] input
The input message to sign. [in] input_length
Size of the input
buffer in bytes.[out] signature
Buffer where the signature is to be written. [in] signature_size
Size of the signature
buffer in bytes. This must be appropriate for the selected algorithm and key:- The required signature size is #PSA_SIGN_OUTPUT_SIZE(
key_type
,key_bits
,alg
) wherekey_type
andkey_bits
are the type and bit-size respectively of key. - #PSA_SIGNATURE_MAX_SIZE evaluates to the maximum signature size of any supported signature algorithm.
[out] signature_length
On success, the number of bytes that make up the returned signature value. - The required signature size is #PSA_SIGN_OUTPUT_SIZE(
- Return values
-
PSA_SUCCESS
PSA_ERROR_INVALID_HANDLE
PSA_ERROR_NOT_PERMITTED
The key does not have the PSA_KEY_USAGE_SIGN_MESSAGE flag, or it does not permit the requested algorithm. PSA_ERROR_BUFFER_TOO_SMALL
The size of the signature
buffer is too small. You can determine a sufficient buffer size by calling #PSA_SIGN_OUTPUT_SIZE(key_type
,key_bits
,alg
) wherekey_type
andkey_bits
are the type and bit-size respectively ofkey
.PSA_ERROR_NOT_SUPPORTED
PSA_ERROR_INVALID_ARGUMENT
PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_DATA_CORRUPT
PSA_ERROR_DATA_INVALID
PSA_ERROR_INSUFFICIENT_ENTROPY
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
◆ psa_verify_message()
psa_status_t psa_verify_message | ( | mbedtls_svc_key_id_t | key, |
psa_algorithm_t | alg, |
||
const uint8_t * | input, |
||
size_t | input_length, |
||
const uint8_t * | signature, |
||
size_t | signature_length |
||
) |
Verify the signature of a message with a public key, using a hash-and-sign verification algorithm.
- Note
- To perform a multi-part hash-and-sign signature verification algorithm, first use a multi-part hash operation to hash the message and then pass the resulting hash to psa_verify_hash(). PSA_ALG_GET_HASH(
alg
) can be used to determine the hash algorithm to use.
- Parameters
-
[in] key
Identifier of the key to use for the operation. It must be a public key or an asymmetric key pair. The key must allow the usage PSA_KEY_USAGE_VERIFY_MESSAGE. [in] alg
An asymmetric signature algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_SIGN_MESSAGE( alg
) is true), that is compatible with the type ofkey
.[in] input
The message whose signature is to be verified. [in] input_length
Size of the input
buffer in bytes.[out] signature
Buffer containing the signature to verify. [in] signature_length
Size of the signature
buffer in bytes.
- Return values
-
PSA_SUCCESS
PSA_ERROR_INVALID_HANDLE
PSA_ERROR_NOT_PERMITTED
The key does not have the PSA_KEY_USAGE_SIGN_MESSAGE flag, or it does not permit the requested algorithm. PSA_ERROR_INVALID_SIGNATURE
The calculation was performed successfully, but the passed signature is not a valid signature. PSA_ERROR_NOT_SUPPORTED
PSA_ERROR_INVALID_ARGUMENT
PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_DATA_CORRUPT
PSA_ERROR_DATA_INVALID
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
◆ psa_sign_hash()
psa_status_t psa_sign_hash | ( | mbedtls_svc_key_id_t | key, |
psa_algorithm_t | alg, |
||
const uint8_t * | hash, |
||
size_t | hash_length, |
||
uint8_t * | signature, |
||
size_t | signature_size, |
||
size_t * | signature_length |
||
) |
Sign a hash or short message with a private key.
Note that to perform a hash-and-sign signature algorithm, you must first calculate the hash by calling psa_hash_setup(), psa_hash_update() and psa_hash_finish(), or alternatively by calling psa_hash_compute(). Then pass the resulting hash as the hash
parameter to this function. You can use PSA_ALG_SIGN_GET_HASH(alg
) to determine the hash algorithm to use.
- Parameters
-
key
Identifier of the key to use for the operation. It must be an asymmetric key pair. The key must allow the usage PSA_KEY_USAGE_SIGN_HASH. alg
A signature algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_SIGN_HASH( alg
) is true), that is compatible with the type ofkey
.[in] hash
The hash or message to sign. hash_length
Size of the hash
buffer in bytes.[out] signature
Buffer where the signature is to be written. signature_size
Size of the signature
buffer in bytes.[out] signature_length
On success, the number of bytes that make up the returned signature value.
- Return values
-
PSA_SUCCESS
PSA_ERROR_INVALID_HANDLE
PSA_ERROR_NOT_PERMITTED
PSA_ERROR_BUFFER_TOO_SMALL
The size of the signature
buffer is too small. You can determine a sufficient buffer size by calling #PSA_SIGN_OUTPUT_SIZE(key_type
,key_bits
,alg
) wherekey_type
andkey_bits
are the type and bit-size respectively ofkey
.PSA_ERROR_NOT_SUPPORTED
PSA_ERROR_INVALID_ARGUMENT
PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_INSUFFICIENT_ENTROPY
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
◆ psa_verify_hash()
psa_status_t psa_verify_hash | ( | mbedtls_svc_key_id_t | key, |
psa_algorithm_t | alg, |
||
const uint8_t * | hash, |
||
size_t | hash_length, |
||
const uint8_t * | signature, |
||
size_t | signature_length |
||
) |
Verify the signature of a hash or short message using a public key.
Note that to perform a hash-and-sign signature algorithm, you must first calculate the hash by calling psa_hash_setup(), psa_hash_update() and psa_hash_finish(), or alternatively by calling psa_hash_compute(). Then pass the resulting hash as the hash
parameter to this function. You can use PSA_ALG_SIGN_GET_HASH(alg
) to determine the hash algorithm to use.
- Parameters
-
key
Identifier of the key to use for the operation. It must be a public key or an asymmetric key pair. The key must allow the usage PSA_KEY_USAGE_VERIFY_HASH. alg
A signature algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_SIGN_HASH( alg
) is true), that is compatible with the type ofkey
.[in] hash
The hash or message whose signature is to be verified. hash_length
Size of the hash
buffer in bytes.[in] signature
Buffer containing the signature to verify. signature_length
Size of the signature
buffer in bytes.
- Return values
-
PSA_SUCCESS
The signature is valid. PSA_ERROR_INVALID_HANDLE
PSA_ERROR_NOT_PERMITTED
PSA_ERROR_INVALID_SIGNATURE
The calculation was perfomed successfully, but the passed signature is not a valid signature. PSA_ERROR_NOT_SUPPORTED
PSA_ERROR_INVALID_ARGUMENT
PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
◆ psa_asymmetric_encrypt()
psa_status_t psa_asymmetric_encrypt | ( | mbedtls_svc_key_id_t | key, |
psa_algorithm_t | alg, |
||
const uint8_t * | input, |
||
size_t | input_length, |
||
const uint8_t * | salt, |
||
size_t | salt_length, |
||
uint8_t * | output, |
||
size_t | output_size, |
||
size_t * | output_length |
||
) |
Encrypt a short message with a public key.
- Parameters
-
key
Identifer of the key to use for the operation. It must be a public key or an asymmetric key pair. It must allow the usage PSA_KEY_USAGE_ENCRYPT. alg
An asymmetric encryption algorithm that is compatible with the type of key
.[in] input
The message to encrypt. input_length
Size of the input
buffer in bytes.[in] salt
A salt or label, if supported by the encryption algorithm. If the algorithm does not support a salt, pass NULL
. If the algorithm supports an optional salt and you do not want to pass a salt, passNULL
.
- For PSA_ALG_RSA_PKCS1V15_CRYPT, no salt is supported.
- Parameters
-
salt_length
Size of the salt
buffer in bytes. Ifsalt
isNULL
, pass 0.[out] output
Buffer where the encrypted message is to be written. output_size
Size of the output
buffer in bytes.[out] output_length
On success, the number of bytes that make up the returned output.
- Return values
-
PSA_SUCCESS
PSA_ERROR_INVALID_HANDLE
PSA_ERROR_NOT_PERMITTED
PSA_ERROR_BUFFER_TOO_SMALL
The size of the output
buffer is too small. You can determine a sufficient buffer size by calling #PSA_ASYMMETRIC_ENCRYPT_OUTPUT_SIZE(key_type
,key_bits
,alg
) wherekey_type
andkey_bits
are the type and bit-size respectively ofkey
.PSA_ERROR_NOT_SUPPORTED
PSA_ERROR_INVALID_ARGUMENT
PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_INSUFFICIENT_ENTROPY
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
◆ psa_asymmetric_decrypt()
psa_status_t psa_asymmetric_decrypt | ( | mbedtls_svc_key_id_t | key, |
psa_algorithm_t | alg, |
||
const uint8_t * | input, |
||
size_t | input_length, |
||
const uint8_t * | salt, |
||
size_t | salt_length, |
||
uint8_t * | output, |
||
size_t | output_size, |
||
size_t * | output_length |
||
) |
Decrypt a short message with a private key.
- Parameters
-
key
Identifier of the key to use for the operation. It must be an asymmetric key pair. It must allow the usage PSA_KEY_USAGE_DECRYPT. alg
An asymmetric encryption algorithm that is compatible with the type of key
.[in] input
The message to decrypt. input_length
Size of the input
buffer in bytes.[in] salt
A salt or label, if supported by the encryption algorithm. If the algorithm does not support a salt, pass NULL
. If the algorithm supports an optional salt and you do not want to pass a salt, passNULL
.
- For PSA_ALG_RSA_PKCS1V15_CRYPT, no salt is supported.
- Parameters
-
salt_length
Size of the salt
buffer in bytes. Ifsalt
isNULL
, pass 0.[out] output
Buffer where the decrypted message is to be written. output_size
Size of the output
buffer in bytes.[out] output_length
On success, the number of bytes that make up the returned output.
- Return values
-
PSA_SUCCESS
PSA_ERROR_INVALID_HANDLE
PSA_ERROR_NOT_PERMITTED
PSA_ERROR_BUFFER_TOO_SMALL
The size of the output
buffer is too small. You can determine a sufficient buffer size by calling #PSA_ASYMMETRIC_DECRYPT_OUTPUT_SIZE(key_type
,key_bits
,alg
) wherekey_type
andkey_bits
are the type and bit-size respectively ofkey
.PSA_ERROR_NOT_SUPPORTED
PSA_ERROR_INVALID_ARGUMENT
PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_INSUFFICIENT_ENTROPY
PSA_ERROR_INVALID_PADDING
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.