Hashing
Description
Provides cryptographic hash functions (SHA-1, SHA-224, SHA-256, SHA-384, SHA-512).
Provides API for one-way hashing functions.
Data Structures | |
struct | sl_se_hash_streaming_context_t |
Generic hash streaming context. Deprecated. | |
struct | sl_se_sha1_multipart_context_t |
SHA-1 streaming context. Safe to use. | |
struct | sl_se_sha1_streaming_context_t |
SHA-1 streaming context. Deprecated. | |
struct | sl_se_sha224_multipart_context_t |
SHA-224 streaming context. Safe to use. | |
struct | sl_se_sha224_streaming_context_t |
SHA-224 streaming context. Deprecated. | |
struct | sl_se_sha256_multipart_context_t |
SHA-256 streaming context. Safe to use. | |
struct | sl_se_sha256_streaming_context_t |
SHA-256 streaming context. Deprecated. | |
struct | sl_se_sha384_multipart_context_t |
SHA-384 streaming context. Safe to use. | |
struct | sl_se_sha384_streaming_context_t |
SHA-384 streaming context. Deprecated. | |
struct | sl_se_sha512_multipart_context_t |
SHA-512 streaming context. Safe to use. | |
struct | sl_se_sha512_streaming_context_t |
SHA-512 streaming context. Deprecated. | |
Functions | |
sl_status_t | sl_se_hash (sl_se_command_context_t *cmd_ctx, sl_se_hash_type_t hash_type, const uint8_t *message, unsigned int message_size, uint8_t *digest, size_t digest_len) |
Produce a message digest (a hash block) using the input data. | |
sl_status_t | sl_se_hash_sha1_multipart_starts (sl_se_sha1_multipart_context_t *sha1_ctx, sl_se_command_context_t *cmd_ctx) |
Prepare a SHA1 hash streaming command context object. | |
sl_status_t | sl_se_hash_sha1_starts (sl_se_hash_streaming_context_t *hash_ctx, sl_se_command_context_t *cmd_ctx, sl_se_sha1_streaming_context_t *sha1_ctx) SL_DEPRECATED_API_SDK_3_3 |
Deprecated, please switch to using sl_se_hash1_multipart_starts(). | |
sl_status_t | sl_se_hash_sha224_multipart_starts (sl_se_sha224_multipart_context_t *sha224_ctx, sl_se_command_context_t *cmd_ctx) |
Prepare a SHA224 hash streaming command context object. | |
sl_status_t | sl_se_hash_sha224_starts (sl_se_hash_streaming_context_t *hash_ctx, sl_se_command_context_t *cmd_ctx, sl_se_sha224_streaming_context_t *sha224_ctx) SL_DEPRECATED_API_SDK_3_3 |
Deprecated, please switch to using sl_se_hash224_multipart_starts(). | |
sl_status_t | sl_se_hash_sha256_multipart_starts (sl_se_sha256_multipart_context_t *sha256_ctx, sl_se_command_context_t *cmd_ctx) |
Prepare a SHA256 hash streaming command context object. | |
sl_status_t | sl_se_hash_sha256_starts (sl_se_hash_streaming_context_t *hash_ctx, sl_se_command_context_t *cmd_ctx, sl_se_sha256_streaming_context_t *sha256_ctx) SL_DEPRECATED_API_SDK_3_3 |
Deprecated, please switch to using sl_se_hash256_multipart_starts(). | |
sl_status_t | sl_se_hash_sha384_multipart_starts (sl_se_sha384_multipart_context_t *sha384_ctx, sl_se_command_context_t *cmd_ctx) |
Prepare a SHA384 streaming command context object. | |
sl_status_t | sl_se_hash_sha384_starts (sl_se_hash_streaming_context_t *hash_ctx, sl_se_command_context_t *cmd_ctx, sl_se_sha384_streaming_context_t *sha384_ctx) SL_DEPRECATED_API_SDK_3_3 |
Deprecated, please switch to using sl_se_hash384_multipart_starts(). | |
sl_status_t | sl_se_hash_sha512_multipart_starts (sl_se_sha512_multipart_context_t *sha512_ctx, sl_se_command_context_t *cmd_ctx) |
Prepare a SHA512 streaming command context object. | |
sl_status_t | sl_se_hash_sha512_starts (sl_se_hash_streaming_context_t *hash_ctx, sl_se_command_context_t *cmd_ctx, sl_se_sha512_streaming_context_t *sha512_ctx) SL_DEPRECATED_API_SDK_3_3 |
Deprecated, please switch to using sl_se_hash512_multipart_starts(). | |
sl_status_t | sl_se_hash_multipart_starts (void *hash_type_ctx, sl_se_command_context_t *cmd_ctx, sl_se_hash_type_t hash_type) |
Prepare a hash streaming command context object. | |
sl_status_t | sl_se_hash_starts (sl_se_hash_streaming_context_t *hash_ctx, sl_se_command_context_t *cmd_ctx, sl_se_hash_type_t hash_type, void *hash_type_ctx) SL_DEPRECATED_API_SDK_3_3 |
Deprecated, please switch to using sl_se_hash_multipart_starts(). | |
sl_status_t | sl_se_hash_multipart_update (void *hash_type_ctx, sl_se_command_context_t *cmd_ctx, const uint8_t *input, size_t input_len) |
Feeds an input buffer into an ongoing hash computation. | |
sl_status_t | sl_se_hash_update (sl_se_hash_streaming_context_t *hash_ctx, const uint8_t *input, size_t input_len) SL_DEPRECATED_API_SDK_3_3 |
Deprecated, please switch to using sl_se_hash_multipart_update(). | |
sl_status_t | sl_se_hash_multipart_finish (void *hash_type_ctx, sl_se_command_context_t *cmd_ctx, uint8_t *digest_out, size_t digest_len) |
Finish a hash streaming operation and return the resulting hash digest. | |
sl_status_t | sl_se_hash_finish (sl_se_hash_streaming_context_t *hash_ctx, uint8_t *digest_out, size_t digest_len) SL_DEPRECATED_API_SDK_3_3 |
Deprecated, please switch to using sl_se_hash_multipart_finish(). | |
Macros | |
#define | SL_SE_HASH_STREAMING_INIT_DEFAULT { NULL, 0, 0, NULL } |
Default streaming hash context. | |
#define | SL_SE_SHA1_STREAMING_INIT_DEFAULT { { 0 }, { 0 }, { 0 } } |
SHA1 streaming hash context. | |
#define | SL_SE_SHA224_STREAMING_INIT_DEFAULT { { 0 }, { 0 }, { 0 } } |
SHA224 streaming hash context. | |
#define | SL_SE_SHA256_STREAMING_INIT_DEFAULT { { 0 }, { 0 }, { 0 } } |
SHA256 streaming hash context. | |
#define | SL_SE_SHA384_STREAMING_INIT_DEFAULT { { 0 }, { 0 }, { 0 } } |
SHA384 streaming hash context. | |
#define | SL_SE_SHA512_STREAMING_INIT_DEFAULT { { 0 }, { 0 }, { 0 } } |
SHA512 streaming hash context. | |
Enumerations | |
enum | sl_se_hash_type_t { SL_SE_HASH_NONE, SL_SE_HASH_SHA1, SL_SE_HASH_SHA224, SL_SE_HASH_SHA256, SL_SE_HASH_SHA384, SL_SE_HASH_SHA512 } |
Hash algorithms. | |
Function Documentation
◆ sl_se_hash()
sl_status_t sl_se_hash | ( | sl_se_command_context_t * | cmd_ctx, |
sl_se_hash_type_t | hash_type, |
||
const uint8_t * | message, |
||
unsigned int | message_size, |
||
uint8_t * | digest, |
||
size_t | digest_len |
||
) |
Produce a message digest (a hash block) using the input data.
This function generates a message digest adhering to the given inputs. For instance, if the algorithm is chosen to be SHA-256, it will generate a 32 bytes message digest computed based on the input message. This function supports SHA-1, SHA-256 and SHA-512 algorithms.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] hash_type
Which hashing algorithm to use. [in] message
Pointer to the message buffer to compute the hash/digest from. [in] message_size
Number of bytes in message. [out] digest
Pointer to block of memory to store the final digest. [in] digest_len
The length of the message digest (hash), must be at least the size of the corresponding hash type.
- Returns
- Status code, sl_status.h.
◆ sl_se_hash_sha1_multipart_starts()
sl_status_t sl_se_hash_sha1_multipart_starts | ( | sl_se_sha1_multipart_context_t * | sha1_ctx, |
sl_se_command_context_t * | cmd_ctx |
||
) |
Prepare a SHA1 hash streaming command context object.
Prepare a SHA1 hash streaming command context object to be used in subsequent calls to hash streaming functions sl_se_hash_multipart_update() and sl_se_hash_multipart_finish().
- Parameters
-
[in] sha1_ctx
Pointer to a SHA1 streaming context object. [in] cmd_ctx
Pointer to an SE command context object.
- Returns
- Status code, sl_status.h.
◆ sl_se_hash_sha1_starts()
sl_status_t sl_se_hash_sha1_starts | ( | sl_se_hash_streaming_context_t * | hash_ctx, |
sl_se_command_context_t * | cmd_ctx, |
||
sl_se_sha1_streaming_context_t * | sha1_ctx |
||
) |
Deprecated, please switch to using sl_se_hash1_multipart_starts().
Prepare a SHA1 hash streaming command context object.
Prepare a SHA1 hash streaming command context object to be used in subsequent calls to hash streaming functions sl_se_hash_update() and sl_se_hash_finish().
- Parameters
-
[in] hash_ctx
Pointer to a generic hash streaming context object. [in] cmd_ctx
Pointer to an SE command context object. [in] sha1_ctx
Pointer to a SHA1 streaming context object.
- Returns
- Status code, sl_status.h.
◆ sl_se_hash_sha224_multipart_starts()
sl_status_t sl_se_hash_sha224_multipart_starts | ( | sl_se_sha224_multipart_context_t * | sha224_ctx, |
sl_se_command_context_t * | cmd_ctx |
||
) |
Prepare a SHA224 hash streaming command context object.
Prepare a SHA224 hash streaming command context object to be used in subsequent calls to hash streaming functions sl_se_hash_multipart_update() and sl_se_hash_multipart_finish().
- Parameters
-
[in] sha224_ctx
Pointer to a SHA224 streaming context object. [in] cmd_ctx
Pointer to an SE command context object.
- Returns
- Status code, sl_status.h.
◆ sl_se_hash_sha224_starts()
sl_status_t sl_se_hash_sha224_starts | ( | sl_se_hash_streaming_context_t * | hash_ctx, |
sl_se_command_context_t * | cmd_ctx, |
||
sl_se_sha224_streaming_context_t * | sha224_ctx |
||
) |
Deprecated, please switch to using sl_se_hash224_multipart_starts().
Prepare a SHA224 hash streaming command context object.
Prepare a SHA224 hash streaming command context object to be used in subsequent calls to hash streaming functions sl_se_hash_update() and sl_se_hash_finish().
- Parameters
-
[in] hash_ctx
Pointer to a generic hash streaming context object. [in] cmd_ctx
Pointer to an SE command context object. [in] sha224_ctx
Pointer to a SHA224 streaming context object.
- Returns
- Status code, sl_status.h.
◆ sl_se_hash_sha256_multipart_starts()
sl_status_t sl_se_hash_sha256_multipart_starts | ( | sl_se_sha256_multipart_context_t * | sha256_ctx, |
sl_se_command_context_t * | cmd_ctx |
||
) |
Prepare a SHA256 hash streaming command context object.
Prepare a SHA256 hash streaming command context object to be used in subsequent calls to hash streaming functions sl_se_hash_multipart_update() and sl_se_hash_multipart_finish().
- Parameters
-
[in] sha256_ctx
Pointer to a SHA256 streaming context object. [in] cmd_ctx
Pointer to an SE command context object.
- Returns
- Status code, sl_status.h.
◆ sl_se_hash_sha256_starts()
sl_status_t sl_se_hash_sha256_starts | ( | sl_se_hash_streaming_context_t * | hash_ctx, |
sl_se_command_context_t * | cmd_ctx, |
||
sl_se_sha256_streaming_context_t * | sha256_ctx |
||
) |
Deprecated, please switch to using sl_se_hash256_multipart_starts().
Prepare a SHA256 hash streaming command context object.
Prepare a SHA256 hash streaming command context object to be used in subsequent calls to hash streaming functions sl_se_hash_update() and sl_se_hash_finish().
- Parameters
-
[in] hash_ctx
Pointer to a generic hash streaming context object. [in] cmd_ctx
Pointer to an SE command context object. [in] sha256_ctx
Pointer to a SHA256 streaming context object.
- Returns
- Status code, sl_status.h.
◆ sl_se_hash_sha384_multipart_starts()
sl_status_t sl_se_hash_sha384_multipart_starts | ( | sl_se_sha384_multipart_context_t * | sha384_ctx, |
sl_se_command_context_t * | cmd_ctx |
||
) |
Prepare a SHA384 streaming command context object.
Prepare a SHA384 hash streaming command context object to be used in subsequent calls to hash streaming functions sl_se_hash_multipart_update() and sl_se_hash_multipart_finish().
- Parameters
-
[in] sha384_ctx
Pointer to a SHA384 streaming context object. [in] cmd_ctx
Pointer to an SE command context object.
- Returns
- Status code, sl_status.h.
◆ sl_se_hash_sha384_starts()
sl_status_t sl_se_hash_sha384_starts | ( | sl_se_hash_streaming_context_t * | hash_ctx, |
sl_se_command_context_t * | cmd_ctx, |
||
sl_se_sha384_streaming_context_t * | sha384_ctx |
||
) |
Deprecated, please switch to using sl_se_hash384_multipart_starts().
Prepare a SHA384 streaming command context object.
Prepare a SHA384 hash streaming command context object to be used in subsequent calls to hash streaming functions sl_se_hash_update() and sl_se_hash_finish().
- Parameters
-
[in] hash_ctx
Pointer to a generic hash streaming context object. [in] cmd_ctx
Pointer to an SE command context object. [in] sha384_ctx
Pointer to a SHA384 streaming context object.
- Returns
- Status code, sl_status.h.
◆ sl_se_hash_sha512_multipart_starts()
sl_status_t sl_se_hash_sha512_multipart_starts | ( | sl_se_sha512_multipart_context_t * | sha512_ctx, |
sl_se_command_context_t * | cmd_ctx |
||
) |
Prepare a SHA512 streaming command context object.
Prepare a SHA512 hash streaming command context object to be used in subsequent calls to hash streaming functions sl_se_hash_multipart_update() and sl_se_hash_multipart_finish().
- Parameters
-
[in] sha512_ctx
Pointer to a SHA512 streaming context object. [in] cmd_ctx
Pointer to an SE command context object.
- Returns
- Status code, sl_status.h.
◆ sl_se_hash_sha512_starts()
sl_status_t sl_se_hash_sha512_starts | ( | sl_se_hash_streaming_context_t * | hash_ctx, |
sl_se_command_context_t * | cmd_ctx, |
||
sl_se_sha512_streaming_context_t * | sha512_ctx |
||
) |
Deprecated, please switch to using sl_se_hash512_multipart_starts().
Prepare a SHA512 streaming command context object.
Prepare a SHA512 hash streaming command context object to be used in subsequent calls to hash streaming functions sl_se_hash_update() and sl_se_hash_finish().
- Parameters
-
[in] hash_ctx
Pointer to a generic hash streaming context object. [in] cmd_ctx
Pointer to an SE command context object. [in] sha512_ctx
Pointer to a SHA512 streaming context object.
- Returns
- Status code, sl_status.h.
◆ sl_se_hash_multipart_starts()
sl_status_t sl_se_hash_multipart_starts | ( | void * | hash_type_ctx, |
sl_se_command_context_t * | cmd_ctx, |
||
sl_se_hash_type_t | hash_type |
||
) |
Prepare a hash streaming command context object.
Prepare a hash (message digest) streaming command context object to be used in subsequent calls to hash streaming functions sl_se_hash_multipart_update() and sl_se_hash_multipart_finish().
- Parameters
-
[in] hash_type_ctx
Pointer to a hash streaming context object specific to the hash type specified by hash_type
.[in] cmd_ctx
Pointer to an SE command context object. [in] hash_type
Type of hash algoritm
- Returns
- Status code, sl_status.h.
◆ sl_se_hash_starts()
sl_status_t sl_se_hash_starts | ( | sl_se_hash_streaming_context_t * | hash_ctx, |
sl_se_command_context_t * | cmd_ctx, |
||
sl_se_hash_type_t | hash_type, |
||
void * | hash_type_ctx |
||
) |
Deprecated, please switch to using sl_se_hash_multipart_starts().
Prepare a hash streaming command context object.
Prepare a hash (message digest) streaming command context object to be used in subsequent calls to hash streaming functions sl_se_hash_update() and sl_se_hash_finish().
- Parameters
-
[in] hash_ctx
Pointer to a generic hash streaming context object. [in] cmd_ctx
Pointer to an SE command context object. [in] hash_type
Type of hash algoritm [in] hash_type_ctx
Pointer to a hash streaming context object specific to the hash type specified by hash_type
.
- Returns
- Status code, sl_status.h.
◆ sl_se_hash_multipart_update()
sl_status_t sl_se_hash_multipart_update | ( | void * | hash_type_ctx, |
sl_se_command_context_t * | cmd_ctx, |
||
const uint8_t * | input, |
||
size_t | input_len |
||
) |
Feeds an input buffer into an ongoing hash computation.
This function is called between sl_se_hash_multipart_starts() and sl_se_hash_multipart_finish(). This function can be called repeatedly.
- Parameters
-
[in] hash_type_ctx
Pointer to a hash streaming context object specific to the hash type specified by hash_type
.[in] cmd_ctx
Pointer to an SE command context object. [in] input
Buffer holding the input data, must be at least ilen
bytes wide.[in] input_len
The length of the input data in bytes.
- Returns
- Status code, sl_status.h.
◆ sl_se_hash_update()
sl_status_t sl_se_hash_update | ( | sl_se_hash_streaming_context_t * | hash_ctx, |
const uint8_t * | input, |
||
size_t | input_len |
||
) |
Deprecated, please switch to using sl_se_hash_multipart_update().
Feeds an input buffer into an ongoing hash computation.
This function is called between sl_se_hash_starts() and sl_se_hash_finish(). This function can be called repeatedly.
- Parameters
-
[in] hash_ctx
Pointer to a generic hash streaming context object. [in] input
Buffer holding the input data, must be at least ilen
bytes wide.[in] input_len
The length of the input data in bytes.
- Returns
- Status code, sl_status.h.
◆ sl_se_hash_multipart_finish()
sl_status_t sl_se_hash_multipart_finish | ( | void * | hash_type_ctx, |
sl_se_command_context_t * | cmd_ctx, |
||
uint8_t * | digest_out, |
||
size_t | digest_len |
||
) |
Finish a hash streaming operation and return the resulting hash digest.
This function is called after sl_se_hash_multipart_update().
- Parameters
-
[in] hash_type_ctx
Pointer to a hash streaming context object specific to the hash type specified by hash_type
.[in] cmd_ctx
Pointer to an SE command context object. [out] digest_out
Buffer for holding the message digest (hash), must be at least the size of the corresponding message digest type. [in] digest_len
The length of the message digest (hash), must be at least the size of the corresponding hash type.
- Returns
- Status code, sl_status.h.
◆ sl_se_hash_finish()
sl_status_t sl_se_hash_finish | ( | sl_se_hash_streaming_context_t * | hash_ctx, |
uint8_t * | digest_out, |
||
size_t | digest_len |
||
) |
Deprecated, please switch to using sl_se_hash_multipart_finish().
Finish a hash streaming operation and return the resulting hash digest.
This function is called after sl_se_hash_update().
- Parameters
-
[in] hash_ctx
Pointer to a generic hash streaming context object. [out] digest_out
Buffer for holding the message digest (hash), must be at least the size of the corresponding message digest type. [in] digest_len
The length of the message digest (hash), must be at least the size of the corresponding hash type.
- Returns
- Status code, sl_status.h.
Macro Definition Documentation
◆ SL_SE_HASH_STREAMING_INIT_DEFAULT
#define SL_SE_HASH_STREAMING_INIT_DEFAULT { NULL, 0, 0, NULL } |
Default streaming hash context.
◆ SL_SE_SHA1_STREAMING_INIT_DEFAULT
#define SL_SE_SHA1_STREAMING_INIT_DEFAULT { { 0 }, { 0 }, { 0 } } |
SHA1 streaming hash context.
◆ SL_SE_SHA224_STREAMING_INIT_DEFAULT
#define SL_SE_SHA224_STREAMING_INIT_DEFAULT { { 0 }, { 0 }, { 0 } } |
SHA224 streaming hash context.
◆ SL_SE_SHA256_STREAMING_INIT_DEFAULT
#define SL_SE_SHA256_STREAMING_INIT_DEFAULT { { 0 }, { 0 }, { 0 } } |
SHA256 streaming hash context.
◆ SL_SE_SHA384_STREAMING_INIT_DEFAULT
#define SL_SE_SHA384_STREAMING_INIT_DEFAULT { { 0 }, { 0 }, { 0 } } |
SHA384 streaming hash context.
◆ SL_SE_SHA512_STREAMING_INIT_DEFAULT
#define SL_SE_SHA512_STREAMING_INIT_DEFAULT { { 0 }, { 0 }, { 0 } } |
SHA512 streaming hash context.
Enumeration Type Documentation
◆ sl_se_hash_type_t
enum sl_se_hash_type_t |