DMD - Dot Matrix Display
Description
Hardware abstraction layer for dot matrix displays.
The DMD interface is the hardware abstraction layer for a physical display. The DMD interface provides functions for treating a connected display as a matrix of pixels of a specific size. The DMD provides functions for initializing the display hardware interface by calling DMD_init() and writing pixel data to the display by calling the function DMD_writeData().
DMD Drivers
GLIB provides a DMD driver for the Sharp Memory LCD screens used on the Silicon Labs Starter Kits. This driver must be used together with the kit display drivers.
Data Structures | |
struct | __DMD_DisplayGeometry |
struct | __DMD_MemoryError |
struct | DMD_DisplayGeometry |
Dimensions of the display. | |
struct | DMD_MemoryError |
Information about a memory error. | |
Functions | |
EMSTATUS | DMD_init (DMD_InitConfig *initConfig) |
Initializes the DMD support for memory lcd display. | |
EMSTATUS | DMD_getDisplayGeometry (DMD_DisplayGeometry **geometry) |
Get the dimensions of the display and of the current clipping area. | |
EMSTATUS | DMD_setClippingArea (uint16_t xStart, uint16_t yStart, uint16_t width, uint16_t height) |
Sets the current clipping area. | |
EMSTATUS | DMD_writeData (uint16_t x, uint16_t y, const uint8_t data[], uint32_t numPixels) |
Draws pixels to the display. | |
EMSTATUS | DMD_writeColor (uint16_t x, uint16_t y, uint8_t red, uint8_t green, uint8_t blue, uint32_t numPixels) |
Draws a number of pixels of the same color to the display. | |
EMSTATUS | DMD_sleep (void) |
Turns off the display and puts it into sleep mode Does not turn off backlight. | |
EMSTATUS | DMD_wakeUp (void) |
Wakes up the display from sleep mode. | |
EMSTATUS | DMD_flipDisplay (int horizontal, int vertical) |
Set horizontal and vertical flip mode of display controller. | |
EMSTATUS | DMD_selectFramebuffer (void *framebuffer) |
Select the active framebuffer DMD functions will draw in. | |
EMSTATUS | DMD_getFrameBuffer (void **framebuffer) |
Get current framebuffer used by DMD for drawing (backbuffer). | |
EMSTATUS | DMD_updateDisplay (void) |
Update the display device with contents of active framebuffer. | |
Macros | |
#define | ECODE_DMD_BASE 0x00000000 |
Base of DMD error codes. | |
#define | DMD_OK 0x00000000 |
Successful call. | |
#define | DMD_ERROR_DRIVER_NOT_INITIALIZED (ECODE_DMD_BASE | 0x0001) |
Driver not initialized correctly. | |
#define | DMD_ERROR_DRIVER_ALREADY_INITIALIZED (ECODE_DMD_BASE | 0x0002) |
Driver is already initialized. | |
#define | DMD_ERROR_TOO_MUCH_DATA (ECODE_DMD_BASE | 0x0003) |
Length of data is larger than size of clip. | |
#define | DMD_ERROR_PIXEL_OUT_OF_BOUNDS (ECODE_DMD_BASE | 0x0004) |
Pixel is outside current clipping area. | |
#define | DMD_ERROR_EMPTY_CLIPPING_AREA (ECODE_DMD_BASE | 0x0005) |
Clipping area is empty. | |
#define | DMD_ERROR_WRONG_DEVICE_CODE (ECODE_DMD_BASE | 0x0006) |
Wrong device code. | |
#define | DMD_ERROR_MEMORY_ERROR (ECODE_DMD_BASE | 0x0007) |
Memory error. | |
#define | DMD_ERROR_NO_ERROR_CODE (ECODE_DMD_BASE | 0x0008) |
Error code expected, but didn't happen. | |
#define | DMD_ERROR_TEST_FAILED (ECODE_DMD_BASE | 0x0009) |
Test run failed. | |
#define | DMD_ERROR_NOT_SUPPORTED (ECODE_DMD_BASE | 0x000a) |
Function or option not supported - yet. | |
#define | DMD_ERROR_NOT_ENOUGH_MEMORY (ECODE_DMD_BASE | 0x000b) |
Not enough memory. | |
#define | DMD_TEST_DEVICE_CODE 0x00000001 |
Device code test. | |
#define | DMD_TEST_MEMORY 0x00000002 |
Memory test. | |
#define | DMD_TEST_PARAMETER_CHECKS 0x00000004 |
Parameter checks test. | |
#define | DMD_TEST_COLORS 0x00000008 |
Color test. | |
#define | DMD_TEST_CLIPPING 0x00000010 |
Clipping test. | |
Typedefs | |
typedef void | DMD_InitConfig |
Configuration parameter for DMD_init. | |
Function Documentation
◆ DMD_init()
EMSTATUS DMD_init | ( | DMD_InitConfig * | initConfig | ) |
Initializes the DMD support for memory lcd display.
- Parameters
-
initConfig
Not used in this DMD module.
- Returns
- DMD_OK on success, otherwise error code
◆ DMD_getDisplayGeometry()
EMSTATUS DMD_getDisplayGeometry | ( | DMD_DisplayGeometry ** | geometry | ) |
Get the dimensions of the display and of the current clipping area.
- Parameters
-
[out] geometry
Geometry structure
- Returns
- DMD_OK on success, otherwise error code
◆ DMD_setClippingArea()
EMSTATUS DMD_setClippingArea | ( | uint16_t | xStart, |
uint16_t | yStart, |
||
uint16_t | width, |
||
uint16_t | height |
||
) |
Sets the current clipping area.
- Note
- All coordinates given to writeData/writeColor/readData are relative to this clipping area.
- Parameters
-
xStart
X coordinate of the upper left corner of the clipping area yStart
Y coordinate of the upper left corner of the clipping area width
Width of the clipping area height
Height of the clipping area
- Returns
- DMD_OK on success, otherwise error code
◆ DMD_writeData()
EMSTATUS DMD_writeData | ( | uint16_t | x, |
uint16_t | y, |
||
const uint8_t | data[], |
||
uint32_t | numPixels |
||
) |
Draws pixels to the display.
- Parameters
-
x
X coordinate of the first pixel to be written, relative to the clipping area y
Y coordinate of the first pixel to be written, relative to the clipping area data
Array containing the pixel data. For monochrome displays, each 8-bit element contains 8 pixels values. For RGB displays, each bit in the array are one color component of the pixel, so that 3 bits represent one pixel. The pixels are ordered by increasing x coordinate, after the last pixel of a row, the next pixel will be the first pixel on the next row. numPixels
Number of pixels to be written
- Returns
- DMD_OK on success, otherwise error code
◆ DMD_writeColor()
EMSTATUS DMD_writeColor | ( | uint16_t | x, |
uint16_t | y, |
||
uint8_t | red, |
||
uint8_t | green, |
||
uint8_t | blue, |
||
uint32_t | numPixels |
||
) |
Draws a number of pixels of the same color to the display.
- Parameters
-
x
X coordinate of the first pixel to be written, relative to the clipping area y
Y coordinate of the first pixel to be written, relative to the clipping area red
Red component of the color green
Green component of the color blue
Blue component of the color numPixels
Number of pixels to be written
- Returns
- DMD_OK on success, otherwise error code
◆ DMD_sleep()
EMSTATUS DMD_sleep | ( | void |
| ) |
Turns off the display and puts it into sleep mode Does not turn off backlight.
- Returns
- DMD_OK on success, otherwise error code
◆ DMD_wakeUp()
EMSTATUS DMD_wakeUp | ( | void |
| ) |
Wakes up the display from sleep mode.
- Returns
- DMD_OK on success, otherwise error code
◆ DMD_flipDisplay()
EMSTATUS DMD_flipDisplay | ( | int | horizontal, |
int | vertical |
||
) |
Set horizontal and vertical flip mode of display controller.
- Parameters
-
horizontal
Set to flip display horizontally vertical
Set to flip display vertically
- Returns
- Returns DMD_OK if successful, error otherwise.
◆ DMD_selectFramebuffer()
EMSTATUS DMD_selectFramebuffer | ( | void * | framebuffer | ) |
Select the active framebuffer DMD functions will draw in.
- Parameters
-
framebuffer
Pointer to the framebuffer to be selected as active framebuffer.
- Returns
- Returns DMD_OK if successful, error otherwise.
◆ DMD_getFrameBuffer()
EMSTATUS DMD_getFrameBuffer | ( | void ** | framebuffer | ) |
Get current framebuffer used by DMD for drawing (backbuffer).
- Parameters
-
framebuffer
Pointer to a framebuffer array. Gets set to DMD's current buffer.
- Returns
- DMD_OK on success
◆ DMD_updateDisplay()
EMSTATUS DMD_updateDisplay | ( | void |
| ) |
Update the display device with contents of active framebuffer.
Only the dirty rows/lines are updated on the display device. Dirty rows/lines are those that have been written to since the last display update. When a new active framebuffer is selected, all lines/rows will be marked as dirty.
- Returns
- Returns DMD_OK if successful, error otherwise.
Macro Definition Documentation
◆ ECODE_DMD_BASE
#define ECODE_DMD_BASE 0x00000000 |
Base of DMD error codes.
◆ DMD_OK
#define DMD_OK 0x00000000 |
Successful call.
◆ DMD_ERROR_DRIVER_NOT_INITIALIZED
#define DMD_ERROR_DRIVER_NOT_INITIALIZED (ECODE_DMD_BASE | 0x0001) |
Driver not initialized correctly.
◆ DMD_ERROR_DRIVER_ALREADY_INITIALIZED
#define DMD_ERROR_DRIVER_ALREADY_INITIALIZED (ECODE_DMD_BASE | 0x0002) |
Driver is already initialized.
◆ DMD_ERROR_TOO_MUCH_DATA
#define DMD_ERROR_TOO_MUCH_DATA (ECODE_DMD_BASE | 0x0003) |
Length of data is larger than size of clip.
◆ DMD_ERROR_PIXEL_OUT_OF_BOUNDS
#define DMD_ERROR_PIXEL_OUT_OF_BOUNDS (ECODE_DMD_BASE | 0x0004) |
Pixel is outside current clipping area.
◆ DMD_ERROR_EMPTY_CLIPPING_AREA
#define DMD_ERROR_EMPTY_CLIPPING_AREA (ECODE_DMD_BASE | 0x0005) |
Clipping area is empty.
◆ DMD_ERROR_WRONG_DEVICE_CODE
#define DMD_ERROR_WRONG_DEVICE_CODE (ECODE_DMD_BASE | 0x0006) |
Wrong device code.
◆ DMD_ERROR_MEMORY_ERROR
#define DMD_ERROR_MEMORY_ERROR (ECODE_DMD_BASE | 0x0007) |
Memory error.
◆ DMD_ERROR_NO_ERROR_CODE
#define DMD_ERROR_NO_ERROR_CODE (ECODE_DMD_BASE | 0x0008) |
Error code expected, but didn't happen.
◆ DMD_ERROR_TEST_FAILED
#define DMD_ERROR_TEST_FAILED (ECODE_DMD_BASE | 0x0009) |
Test run failed.
◆ DMD_ERROR_NOT_SUPPORTED
#define DMD_ERROR_NOT_SUPPORTED (ECODE_DMD_BASE | 0x000a) |
Function or option not supported - yet.
◆ DMD_ERROR_NOT_ENOUGH_MEMORY
#define DMD_ERROR_NOT_ENOUGH_MEMORY (ECODE_DMD_BASE | 0x000b) |
Not enough memory.
◆ DMD_TEST_DEVICE_CODE
#define DMD_TEST_DEVICE_CODE 0x00000001 |
Device code test.
◆ DMD_TEST_MEMORY
#define DMD_TEST_MEMORY 0x00000002 |
Memory test.
◆ DMD_TEST_PARAMETER_CHECKS
#define DMD_TEST_PARAMETER_CHECKS 0x00000004 |
Parameter checks test.
◆ DMD_TEST_COLORS
#define DMD_TEST_COLORS 0x00000008 |
Color test.
◆ DMD_TEST_CLIPPING
#define DMD_TEST_CLIPPING 0x00000010 |
Clipping test.
Typedef Documentation
◆ DMD_InitConfig
typedef void DMD_InitConfig |
Configuration parameter for DMD_init.
This typedef is defined 'void' and may be defined differently in the future.