Status Flags
Description
*brief Status Flags
These constant values are returned by USBX_blockRead() and USBX_blockWrite().
Macros | |
#define | USBX_STATUS_OK USB_STATUS_OK |
Success. | |
#define | USBX_STATUS_EP_BUSY USB_STATUS_EP_BUSY |
Failed because the endpoint is busy. | |
#define | USBX_STATUS_ILLEGAL USB_STATUS_ILLEGAL |
Failed due to an illegal parameter. | |
#define | USBX_STATUS_EP_STALLED USB_STATUS_EP_STALLED |
Failed because the endpoint is stalled. | |
#define | USBX_STATUS_DEVICE_UNCONFIGURED USB_STATUS_DEVICE_UNCONFIGURED |
Failed because the device is not configured. | |
Macro Definition Documentation
◆ USBX_STATUS_OK
#define USBX_STATUS_OK USB_STATUS_OK |
Success.
◆ USBX_STATUS_EP_BUSY
#define USBX_STATUS_EP_BUSY USB_STATUS_EP_BUSY |
Failed because the endpoint is busy.
◆ USBX_STATUS_ILLEGAL
#define USBX_STATUS_ILLEGAL USB_STATUS_ILLEGAL |
Failed due to an illegal parameter.
◆ USBX_STATUS_EP_STALLED
#define USBX_STATUS_EP_STALLED USB_STATUS_EP_STALLED |
Failed because the endpoint is stalled.
◆ USBX_STATUS_DEVICE_UNCONFIGURED
#define USBX_STATUS_DEVICE_UNCONFIGURED USB_STATUS_DEVICE_UNCONFIGURED |
Failed because the device is not configured.