Status Flags

Description

*brief Status Flags

These constant values are returned by USBX_blockRead() and USBX_blockWrite() .

Macros

#define USBX_STATUS_OK USB_STATUS_OK
Success.
#define USBX_STATUS_EP_BUSY USB_STATUS_EP_BUSY
Failed because the endpoint is busy.
#define USBX_STATUS_ILLEGAL USB_STATUS_ILLEGAL
Failed due to an illegal parameter.
#define USBX_STATUS_EP_STALLED USB_STATUS_EP_STALLED
Failed because the endpoint is stalled.
#define USBX_STATUS_DEVICE_UNCONFIGURED USB_STATUS_DEVICE_UNCONFIGURED
Failed because the device is not configured.

Macro Definition Documentation

◆ USBX_STATUS_OK

#define USBX_STATUS_OK USB_STATUS_OK

Success.

◆ USBX_STATUS_EP_BUSY

#define USBX_STATUS_EP_BUSY USB_STATUS_EP_BUSY

Failed because the endpoint is busy.

◆ USBX_STATUS_ILLEGAL

#define USBX_STATUS_ILLEGAL USB_STATUS_ILLEGAL

Failed due to an illegal parameter.

◆ USBX_STATUS_EP_STALLED

#define USBX_STATUS_EP_STALLED USB_STATUS_EP_STALLED

Failed because the endpoint is stalled.

◆ USBX_STATUS_DEVICE_UNCONFIGURED

#define USBX_STATUS_DEVICE_UNCONFIGURED USB_STATUS_DEVICE_UNCONFIGURED

Failed because the device is not configured.