__GLIB_Font_t Struct Reference
Font definition structure.
#include <glib.h>
Data Fields |
|
| void * | pFontPixMap |
|
Pointer to the pixel map for the font.
|
|
| uint16_t | cntOfMapElements |
|
Number of elements in the font pixel map.
|
|
| uint8_t | sizeOfMapElement |
|
Size of each element in the font pixel map.
|
|
| uint8_t | fontRowOffset |
|
Font row offset.
|
|
| uint8_t | fontWidth |
|
Width in pixels of each character.
|
|
| uint8_t | fontHeight |
|
Height in pixels of each character.
|
|
| uint8_t | lineSpacing |
|
Number of pixels between each line in this font.
|
|
| uint8_t | charSpacing |
|
Number of pixels between each character in this font.
|
|
| GLIB_Font_Class | class |
|
The font class is used to tell glib if the font contains numbers only or characters and numbers.
|
|
Font definition structure.
Field Documentation
◆ pFontPixMap
| void* __GLIB_Font_t::pFontPixMap |
Pointer to the pixel map for the font.
◆ cntOfMapElements
| uint16_t __GLIB_Font_t::cntOfMapElements |
Number of elements in the font pixel map.
◆ sizeOfMapElement
| uint8_t __GLIB_Font_t::sizeOfMapElement |
Size of each element in the font pixel map.
◆ fontRowOffset
| uint8_t __GLIB_Font_t::fontRowOffset |
Font row offset.
◆ fontWidth
| uint8_t __GLIB_Font_t::fontWidth |
Width in pixels of each character.
◆ fontHeight
| uint8_t __GLIB_Font_t::fontHeight |
Height in pixels of each character.
◆ lineSpacing
| uint8_t __GLIB_Font_t::lineSpacing |
Number of pixels between each line in this font.
◆ charSpacing
| uint8_t __GLIB_Font_t::charSpacing |
Number of pixels between each character in this font.
◆ class
| GLIB_Font_Class __GLIB_Font_t::class |
The font class is used to tell glib if the font contains numbers only or characters and numbers.