UARTDRV_Buffer_FifoQueue_t Struct Reference

Transfer operation FIFO queue typedef.

#include <uartdrv.h>

Data Fields

volatile uint16_t head
An index of the next byte to send.
volatile uint16_t tail
An index of the location to enqueue the next message.
volatile uint16_t used
A number of bytes queued.
const uint16_t size
FIFO size.
UARTDRV_Buffer_t fifo [1]
FIFO of queued data. Actual size varies.

Transfer operation FIFO queue typedef.

Field Documentation

head

volatile uint16_t UARTDRV_Buffer_FifoQueue_t::head

An index of the next byte to send.

tail

volatile uint16_t UARTDRV_Buffer_FifoQueue_t::tail

An index of the location to enqueue the next message.

used

volatile uint16_t UARTDRV_Buffer_FifoQueue_t::used

A number of bytes queued.

size

const uint16_t UARTDRV_Buffer_FifoQueue_t::size

FIFO size.

fifo

UARTDRV_Buffer_t UARTDRV_Buffer_FifoQueue_t::fifo[1]

FIFO of queued data. Actual size varies.