Built-in keys

Description

Macros

#define MBEDTLS_PSA_KEY_ID_BUILTIN_MIN (( psa_key_id_t )0x7fff0000)
The minimum value for a key identifier that is built into the implementation.
#define MBEDTLS_PSA_KEY_ID_BUILTIN_MAX (( psa_key_id_t )0x7fffefff)
The maximum value for a key identifier that is built into the implementation.

Typedefs

typedef uint64_t psa_drv_slot_number_t
A slot number identifying a key in a driver.

Macro Definition Documentation

◆ MBEDTLS_PSA_KEY_ID_BUILTIN_MIN

#define MBEDTLS_PSA_KEY_ID_BUILTIN_MIN   (( psa_key_id_t )0x7fff0000)

The minimum value for a key identifier that is built into the implementation.

The range of key identifiers from MBEDTLS_PSA_KEY_ID_BUILTIN_MIN to MBEDTLS_PSA_KEY_ID_BUILTIN_MAX within the range from PSA_KEY_ID_VENDOR_MIN and PSA_KEY_ID_VENDOR_MAX and must not intersect with any other set of implementation-chosen key identifiers.

This value is part of the library's ABI since changing it would invalidate the values of built-in key identifiers in applications.

◆ MBEDTLS_PSA_KEY_ID_BUILTIN_MAX

#define MBEDTLS_PSA_KEY_ID_BUILTIN_MAX   (( psa_key_id_t )0x7fffefff)

The maximum value for a key identifier that is built into the implementation.

See MBEDTLS_PSA_KEY_ID_BUILTIN_MIN for more information.

Typedef Documentation

◆ psa_drv_slot_number_t

typedef uint64_t psa_drv_slot_number_t

A slot number identifying a key in a driver.

Values of this type are used to identify built-in keys.