Secure Element Authenticated Encryption with Additional Data

Description

Authenticated Encryption with Additional Data (AEAD) operations with secure elements must be done in one function call. While this creates a burden for implementers as there must be sufficient space in memory for the entire message, it prevents decrypted data from being made available before the authentication operation is complete and the data is known to be authentic.

Data Structures

struct psa_drv_se_aead_t
A struct containing all of the function pointers needed to implement secure element Authenticated Encryption with Additional Data operations.

Typedefs

typedef psa_status_t (* psa_drv_se_aead_encrypt_t ) ( psa_drv_se_context_t *drv_context, psa_key_slot_number_t key_slot, psa_algorithm_t algorithm, const uint8_t *p_nonce, size_t nonce_length, const uint8_t *p_additional_data, size_t additional_data_length, const uint8_t *p_plaintext, size_t plaintext_length, uint8_t *p_ciphertext, size_t ciphertext_size, size_t *p_ciphertext_length)
A function that performs a secure element authenticated encryption operation.
typedef psa_status_t (* psa_drv_se_aead_decrypt_t ) ( psa_drv_se_context_t *drv_context, psa_key_slot_number_t key_slot, psa_algorithm_t algorithm, const uint8_t *p_nonce, size_t nonce_length, const uint8_t *p_additional_data, size_t additional_data_length, const uint8_t *p_ciphertext, size_t ciphertext_length, uint8_t *p_plaintext, size_t plaintext_size, size_t *p_plaintext_length)
A function that peforms a secure element authenticated decryption operation.

Typedef Documentation

◆ psa_drv_se_aead_encrypt_t

typedef psa_status_t (* psa_drv_se_aead_encrypt_t) ( psa_drv_se_context_t *drv_context, psa_key_slot_number_t key_slot, psa_algorithm_t algorithm, const uint8_t *p_nonce, size_t nonce_length, const uint8_t *p_additional_data, size_t additional_data_length, const uint8_t *p_plaintext, size_t plaintext_length, uint8_t *p_ciphertext, size_t ciphertext_size, size_t *p_ciphertext_length)

A function that performs a secure element authenticated encryption operation.

Parameters
[in,out] drv_context The driver context structure.
[in] key_slot Slot containing the key to use.
[in] algorithm The AEAD algorithm to compute ( PSA_ALG_XXX value such that PSA_ALG_IS_AEAD ( alg ) is true)
[in] p_nonce Nonce or IV to use
[in] nonce_length Size of the p_nonce buffer in bytes
[in] p_additional_data Additional data that will be authenticated but not encrypted
[in] additional_data_length Size of p_additional_data in bytes
[in] p_plaintext Data that will be authenticated and encrypted
[in] plaintext_length Size of p_plaintext in bytes
[out] p_ciphertext Output buffer for the authenticated and encrypted data. The additional data is not part of this output. For algorithms where the encrypted data and the authentication tag are defined as separate outputs, the authentication tag is appended to the encrypted data.
[in] ciphertext_size Size of the p_ciphertext buffer in bytes
[out] p_ciphertext_length On success, the size of the output in the p_ciphertext buffer
Return values
PSA_SUCCESS Success.

◆ psa_drv_se_aead_decrypt_t

typedef psa_status_t (* psa_drv_se_aead_decrypt_t) ( psa_drv_se_context_t *drv_context, psa_key_slot_number_t key_slot, psa_algorithm_t algorithm, const uint8_t *p_nonce, size_t nonce_length, const uint8_t *p_additional_data, size_t additional_data_length, const uint8_t *p_ciphertext, size_t ciphertext_length, uint8_t *p_plaintext, size_t plaintext_size, size_t *p_plaintext_length)

A function that peforms a secure element authenticated decryption operation.

Parameters
[in,out] drv_context The driver context structure.
[in] key_slot Slot containing the key to use
[in] algorithm The AEAD algorithm to compute ( PSA_ALG_XXX value such that PSA_ALG_IS_AEAD ( alg ) is true)
[in] p_nonce Nonce or IV to use
[in] nonce_length Size of the p_nonce buffer in bytes
[in] p_additional_data Additional data that has been authenticated but not encrypted
[in] additional_data_length Size of p_additional_data in bytes
[in] p_ciphertext Data that has been authenticated and encrypted. For algorithms where the encrypted data and the authentication tag are defined as separate inputs, the buffer must contain the encrypted data followed by the authentication tag.
[in] ciphertext_length Size of p_ciphertext in bytes
[out] p_plaintext Output buffer for the decrypted data
[in] plaintext_size Size of the p_plaintext buffer in bytes
[out] p_plaintext_length On success, the size of the output in the p_plaintext buffer
Return values
PSA_SUCCESS Success.