sl_power_manager_em_transition_event_info_t Struct Reference

Struct representing energy mode transition event information.

#include <sl_power_manager.h>

Data Fields

const sl_power_manager_em_transition_event_t event_mask
Mask of the transitions on which the callback should be called.
const sl_power_manager_em_transition_on_event_t on_event
Function that must be called when the event occurs.

Struct representing energy mode transition event information.

Field Documentation

◆ event_mask

const sl_power_manager_em_transition_event_t sl_power_manager_em_transition_event_info_t::event_mask

Mask of the transitions on which the callback should be called.

◆ on_event

const sl_power_manager_em_transition_on_event_t sl_power_manager_em_transition_event_info_t::on_event

Function that must be called when the event occurs.