DPLL Initialization
Description
Initialize the Digital PLL.
Configures and locks the Digital PLL using the configuration in the configuration header
sl_device_init_dpll_config.h
, where settings including reference frequency, target frequency and lock mode are available.
If using Simplicity Studio, this configuration header is also configurable through the Project Configurator, by selecting the "Device Init: DPLL" configuration component.
Functions |
|
| sl_status_t | sl_device_init_dpll (void) |
|
Initialize DPLL.
|
|
Function Documentation
◆ sl_device_init_dpll()
| sl_status_t sl_device_init_dpll | ( | void |
|
) |
Initialize DPLL.
Configures and locks the Digital PLL using the configuration in the configuration header
sl_device_init_dpll_config.h
, where settings including reference frequency, target frequency and lock mode are available.
- Returns
- Status code
- Return values
-
SL_STATUS_OKDPLL successfully initialized and locked SL_STATUS_FAILDPLL lock was unsuccessful