psa_drv_se_cipher_t Struct Reference

A struct containing all of the function pointers needed to implement cipher operations using secure elements.

#include <crypto_se_driver.h>

Public Member Functions

size_t MBEDTLS_PRIVATE (context_size)
The size in bytes of the hardware-specific secure element cipher context structure.
psa_drv_se_cipher_setup_t MBEDTLS_PRIVATE (p_setup)
Function that performs a cipher setup operation.
psa_drv_se_cipher_set_iv_t MBEDTLS_PRIVATE (p_set_iv)
Function that sets a cipher IV (if necessary)
psa_drv_se_cipher_update_t MBEDTLS_PRIVATE (p_update)
Function that performs a cipher update operation.
psa_drv_se_cipher_finish_t MBEDTLS_PRIVATE (p_finish)
Function that completes a cipher operation.
psa_drv_se_cipher_abort_t MBEDTLS_PRIVATE (p_abort)
Function that aborts a cipher operation.
psa_drv_se_cipher_ecb_t MBEDTLS_PRIVATE (p_ecb)
Function that performs ECB mode for a cipher operation (Danger: ECB mode should not be used directly by clients of the PSA Crypto Client API)

A struct containing all of the function pointers needed to implement cipher operations using secure elements.

PSA Crypto API implementations should populate instances of the table as appropriate upon startup or at build time.

If one of the functions is not implemented (such as psa_drv_se_cipher_ecb_t ), it should be set to NULL.

Member Function Documentation

◆ MBEDTLS_PRIVATE() [1/7]

size_t psa_drv_se_cipher_t::MBEDTLS_PRIVATE ( context_size )

The size in bytes of the hardware-specific secure element cipher context structure.

◆ MBEDTLS_PRIVATE() [2/7]

psa_drv_se_cipher_setup_t psa_drv_se_cipher_t::MBEDTLS_PRIVATE ( p_setup )

Function that performs a cipher setup operation.

◆ MBEDTLS_PRIVATE() [3/7]

psa_drv_se_cipher_set_iv_t psa_drv_se_cipher_t::MBEDTLS_PRIVATE ( p_set_iv )

Function that sets a cipher IV (if necessary)

◆ MBEDTLS_PRIVATE() [4/7]

psa_drv_se_cipher_update_t psa_drv_se_cipher_t::MBEDTLS_PRIVATE ( p_update )

Function that performs a cipher update operation.

◆ MBEDTLS_PRIVATE() [5/7]

psa_drv_se_cipher_finish_t psa_drv_se_cipher_t::MBEDTLS_PRIVATE ( p_finish )

Function that completes a cipher operation.

◆ MBEDTLS_PRIVATE() [6/7]

psa_drv_se_cipher_abort_t psa_drv_se_cipher_t::MBEDTLS_PRIVATE ( p_abort )

Function that aborts a cipher operation.

◆ MBEDTLS_PRIVATE() [7/7]

psa_drv_se_cipher_ecb_t psa_drv_se_cipher_t::MBEDTLS_PRIVATE ( p_ecb )

Function that performs ECB mode for a cipher operation (Danger: ECB mode should not be used directly by clients of the PSA Crypto Client API)