RMU - Reset Management Unit
Description
Reset Management Unit (RMU) Peripheral API.
This module contains functions to control the RMU peripheral of Silicon Labs 32-bit MCUs and SoCs. RMU ensures correct reset operation and is responsible for connecting the different reset sources to the reset lines of the MCU or SoC.
| Functions | |
| void | RMU_ResetControl ( RMU_Reset_TypeDef reset, RMU_ResetMode_TypeDef mode) | 
| Disable/enable reset for various peripherals and signal sources. | |
| void | RMU_ResetCauseClear (void) | 
| Clear the reset cause register. | |
| uint32_t | RMU_ResetCauseGet (void) | 
| Get the cause of the last reset. | |
| Macros | |
| #define | RMU_LockupResetDisable (A) RMU_ResetControl ( rmuResetLockUp , A) | 
| RMU_LockupResetDisable kept for backwards compatibility. | |
| Enumerations | |
| enum | RMU_ResetMode_TypeDef
         
         { rmuResetModeClear = 0, rmuResetModeSet = 1 } | 
| RMU reset modes. | |
| enum | RMU_Reset_TypeDef
         
         { rmuResetBU = _RMU_CTRL_BURSTEN_MASK, rmuResetLockUp = _RMU_CTRL_LOCKUPRDIS_MASK } | 
| RMU controlled peripheral reset control and reset source control. | |
Function Documentation
◆ RMU_ResetControl()
| void RMU_ResetControl | ( | RMU_Reset_TypeDef | 
            reset,
            | 
| RMU_ResetMode_TypeDef | 
            mode
            | ||
| ) | 
Disable/enable reset for various peripherals and signal sources.
- Parameters
- 
         [in] resetReset types to enable/disable.s [in] modeReset mode. 
◆ RMU_ResetCauseClear()
| void RMU_ResetCauseClear | ( | void | 
            | ) | 
Clear the reset cause register.
This function clears all the reset cause bits of the RSTCAUSE register. The reset cause bits must be cleared by software before a new reset occurs. Otherwise, reset causes may accumulate. See RMU_ResetCauseGet() .
◆ RMU_ResetCauseGet()
| uint32_t RMU_ResetCauseGet | ( | void | 
            | ) | 
Get the cause of the last reset.
To be useful, the reset cause must be cleared by software before a new reset occurs. Otherwise, reset causes may accumulate. See RMU_ResetCauseClear() . This function call will return the main cause for reset, which can be a bit mask (several causes) and clear away "noise".
- Returns
- A reset cause mask. See the reference manual for a description of the reset cause mask.
Macro Definition Documentation
◆ RMU_LockupResetDisable
| #define RMU_LockupResetDisable | ( | 
            A
            | ) | RMU_ResetControl ( rmuResetLockUp , A) | 
RMU_LockupResetDisable kept for backwards compatibility.
Enumeration Type Documentation
◆ RMU_ResetMode_TypeDef
◆ RMU_Reset_TypeDef
| enum RMU_Reset_TypeDef |