RTCC - Real Timer Counter/Calendar
Description
Real Time Counter and Calendar (RTCC) Peripheral API.
This module contains functions to control the RTCC peripheral of Silicon Labs 32-bit MCUs and SoCs. The RTCC ensures timekeeping in low energy modes. The RTCC also includes a BCD calendar mode for easy time and date keeping.
Data Structures |
|
| struct | RTCC_Init_TypeDef |
|
RTCC initialization structure.
|
|
| struct | RTCC_CCChConf_TypeDef |
|
RTCC capture/compare channel configuration structure.
|
|
Functions |
|
| uint32_t | RTCC_ChannelCompareValueGet (int ch) |
|
Get the RTCC compare register value for a selected channel.
|
|
| void | RTCC_ChannelCompareValueSet (int ch, uint32_t value) |
|
Set the RTCC compare register value for a selected channel.
|
|
| uint32_t | RTCC_ChannelCaptureValueGet (int ch) |
|
Get the RTCC input capture register value for a selected channel.
|
|
| uint32_t | RTCC_ChannelCCVGet (int ch) |
|
Get the RTCC capture/compare register value for a selected channel.
|
|
| void | RTCC_ChannelCCVSet (int ch, uint32_t value) |
|
Set RTCC capture/compare register value for a selected channel.
|
|
| uint32_t | RTCC_CombinedCounterGet (void) |
|
Get the combined CNT/PRECNT register content.
|
|
| uint32_t | RTCC_CounterGet (void) |
|
Get the RTCC counter value.
|
|
| void | RTCC_CounterSet (uint32_t value) |
|
Set the RTCC CNT counter.
|
|
| void | RTCC_Enable (bool enable) |
|
Enable/disable RTCC counting.
|
|
| void | RTCC_Init (const RTCC_Init_TypeDef *init) |
|
Initialize RTCC.
|
|
| void | RTCC_ChannelInit (int ch, RTCC_CCChConf_TypeDef const *confPtr) |
|
Configure the selected capture/compare channel of the RTCC.
|
|
| void | RTCC_IntClear (uint32_t flags) |
|
Clear one or more pending RTCC interrupts.
|
|
| void | RTCC_IntDisable (uint32_t flags) |
|
Disable one or more RTCC interrupts.
|
|
| void | RTCC_IntEnable (uint32_t flags) |
|
Enable one or more RTCC interrupts.
|
|
| uint32_t | RTCC_IntGet (void) |
|
Get pending RTCC interrupt flags.
|
|
| uint32_t | RTCC_IntGetEnabled (void) |
|
Get enabled and pending RTCC interrupt flags.
|
|
| void | RTCC_IntSet (uint32_t flags) |
|
Set one or more pending RTCC interrupts from SW.
|
|
| void | RTCC_Lock (void) |
|
Lock RTCC registers.
|
|
| uint32_t | RTCC_PreCounterGet (void) |
|
Get the RTCC pre-counter value.
|
|
| void | RTCC_PreCounterSet (uint32_t preCntVal) |
|
Set the RTCC pre-counter value.
|
|
| void | RTCC_Reset (void) |
|
Restore RTCC to its reset state.
|
|
| void | RTCC_StatusClear (void) |
|
Clear the STATUS register.
|
|
| uint32_t | RTCC_StatusGet (void) |
|
Get the STATUS register value.
|
|
| void | RTCC_SyncWait (void) |
|
Wait for the RTCC to complete all synchronization of register changes and commands.
|
|
| void | RTCC_Start (void) |
|
Start the RTCC counter.
|
|
| void | RTCC_Stop (void) |
|
Stop the RTCC counter.
|
|
| void | RTCC_Unlock (void) |
|
Unlock RTCC registers.
|
|
Macros |
|
| #define | RTCC_INIT_DEFAULT |
|
Default RTCC initialization structure.
|
|
| #define | RTCC_CH_INIT_COMPARE_DEFAULT |
|
Default RTCC channel output compare initialization structure.
|
|
| #define | RTCC_CH_INIT_CAPTURE_DEFAULT |
|
Default RTCC channel input capture initialization structure.
|
|
| #define | RTCC_CH_VALID (ch) ((unsigned)(ch) < RTCC_CC_NUM) |
|
Number of RTCC capture/compare channels.
|
|
Typedefs |
|
| typedef uint8_t | RTCC_PRSSel_TypeDef |
|
PRS channel number.
|
|
Enumerations |
|
| enum |
RTCC_CntPresc_TypeDef
{
rtccCntPresc_1 = _RTCC_CFG_CNTPRESC_DIV1, rtccCntPresc_2 = _RTCC_CFG_CNTPRESC_DIV2, rtccCntPresc_4 = _RTCC_CFG_CNTPRESC_DIV4, rtccCntPresc_8 = _RTCC_CFG_CNTPRESC_DIV8, rtccCntPresc_16 = _RTCC_CFG_CNTPRESC_DIV16, rtccCntPresc_32 = _RTCC_CFG_CNTPRESC_DIV32, rtccCntPresc_64 = _RTCC_CFG_CNTPRESC_DIV64, rtccCntPresc_128 = _RTCC_CFG_CNTPRESC_DIV128, rtccCntPresc_256 = _RTCC_CFG_CNTPRESC_DIV256, rtccCntPresc_512 = _RTCC_CFG_CNTPRESC_DIV512, rtccCntPresc_1024 = _RTCC_CFG_CNTPRESC_DIV1024, rtccCntPresc_2048 = _RTCC_CFG_CNTPRESC_DIV2048, rtccCntPresc_4096 = _RTCC_CFG_CNTPRESC_DIV4096, rtccCntPresc_8192 = _RTCC_CFG_CNTPRESC_DIV8192, rtccCntPresc_16384 = _RTCC_CFG_CNTPRESC_DIV16384, rtccCntPresc_32768 = _RTCC_CFG_CNTPRESC_DIV32768 } |
|
Counter prescaler selection.
|
|
| enum |
RTCC_PrescMode_TypeDef
{
rtccCntTickPresc = _RTCC_CFG_CNTTICK_PRESC, rtccCntTickCCV0Match = _RTCC_CFG_CNTTICK_CCV0MATCH } |
|
Prescaler mode of the RTCC counter.
|
|
| enum |
RTCC_CapComChMode_TypeDef
{
rtccCapComChModeOff = _RTCC_CC_CTRL_MODE_OFF, rtccCapComChModeCapture = _RTCC_CC_CTRL_MODE_INPUTCAPTURE, rtccCapComChModeCompare = _RTCC_CC_CTRL_MODE_OUTPUTCOMPARE } |
|
Capture/Compare channel mode.
|
|
| enum |
RTCC_CompMatchOutAction_TypeDef
{
rtccCompMatchOutActionPulse = _RTCC_CC_CTRL_CMOA_PULSE, rtccCompMatchOutActionToggle = _RTCC_CC_CTRL_CMOA_TOGGLE, rtccCompMatchOutActionClear = _RTCC_CC_CTRL_CMOA_CLEAR, rtccCompMatchOutActionSet = _RTCC_CC_CTRL_CMOA_SET } |
|
Compare match output action mode.
|
|
| enum |
RTCC_InEdgeSel_TypeDef
{
rtccInEdgeRising = _RTCC_CC_CTRL_ICEDGE_RISING, rtccInEdgeFalling = _RTCC_CC_CTRL_ICEDGE_FALLING, rtccInEdgeBoth = _RTCC_CC_CTRL_ICEDGE_BOTH, rtccInEdgeNone = _RTCC_CC_CTRL_ICEDGE_NONE } |
|
Input edge select.
|
|
| enum |
RTCC_CompBase_TypeDef
{
rtccCompBaseCnt = _RTCC_CC_CTRL_COMPBASE_CNT, rtccCompBasePreCnt = _RTCC_CC_CTRL_COMPBASE_PRECNT } |
|
Capture/Compare channel compare mode.
|
|
Function Documentation
◆ RTCC_ChannelCompareValueGet()
|
inline |
Get the RTCC compare register value for a selected channel.
- Parameters
-
[in] chChannel selector.
- Returns
- Compare register value.
◆ RTCC_ChannelCompareValueSet()
|
inline |
Set the RTCC compare register value for a selected channel.
- Parameters
-
[in] chChannel selector. [in] valueCompare register value
◆ RTCC_ChannelCaptureValueGet()
|
inline |
Get the RTCC input capture register value for a selected channel.
- Parameters
-
[in] chChannel selector.
- Returns
- Capture register value.
◆ RTCC_ChannelCCVGet()
|
inline |
Get the RTCC capture/compare register value for a selected channel.
For parts with separate capture compare value registers, this function returns the compare value.
- Parameters
-
[in] chChannel selector.
- Returns
- Capture/compare register value.
◆ RTCC_ChannelCCVSet()
|
inline |
Set RTCC capture/compare register value for a selected channel.
For parts with separate capture compare value registers, this function sets the compare value.
- Parameters
-
[in] chChannel selector. [in] valueCapture/compare register value
◆ RTCC_CombinedCounterGet()
|
inline |
Get the combined CNT/PRECNT register content.
- Returns
- CNT/PRECNT register value.
◆ RTCC_CounterGet()
|
inline |
Get the RTCC counter value.
- Returns
- Current RTCC counter value.
◆ RTCC_CounterSet()
|
inline |
Set the RTCC CNT counter.
- Parameters
-
[in] valueCNT value.
◆ RTCC_Enable()
| void RTCC_Enable | ( | bool |
enable
|
) |
Enable/disable RTCC counting.
- Parameters
-
[in] enableTrue to enable RTCC counting, false to disable counting.
◆ RTCC_Init()
| void RTCC_Init | ( | const RTCC_Init_TypeDef * |
init
|
) |
Initialize RTCC.
Note that the compare values must be set separately with RTCC_CompareSet(), which should probably be done prior to the use of this function if configuring the RTCC to start when initialization is completed.
- Parameters
-
[in] initA pointer to the RTCC initialization structure.
◆ RTCC_ChannelInit()
| void RTCC_ChannelInit | ( | int |
ch,
|
| RTCC_CCChConf_TypeDef const * |
confPtr
|
||
| ) |
Configure the selected capture/compare channel of the RTCC.
Use this function to configure an RTCC channel. Select capture/compare mode, match output action, overflow output action, and PRS input configuration. See the configuration structure RTCC_CCChConf_TypeDef for more details.
- Parameters
-
[in] chA channel selector. [in] confPtrA pointer to the configuration structure.
Configure the selected capture/compare channel.
◆ RTCC_IntClear()
|
inline |
Clear one or more pending RTCC interrupts.
- Parameters
-
[in] flagsRTCC interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources.
◆ RTCC_IntDisable()
|
inline |
Disable one or more RTCC interrupts.
- Parameters
-
[in] flagsRTCC interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt.
◆ RTCC_IntEnable()
|
inline |
Enable one or more RTCC interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using RTCC_IntClear() prior to enabling the interrupt.
- Parameters
-
[in] flagsRTCC interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt.
◆ RTCC_IntGet()
|
inline |
Get pending RTCC interrupt flags.
- Note
- Event bits are not cleared by using this function.
- Returns
- Pending RTCC interrupt sources. Returns a set of interrupt flags OR-ed together for the interrupt sources set.
◆ RTCC_IntGetEnabled()
|
inline |
Get enabled and pending RTCC interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Returns
- Pending and enabled RTCC interrupt sources. Returns a set of interrupt flags OR-ed together for the interrupt sources set.
◆ RTCC_IntSet()
|
inline |
Set one or more pending RTCC interrupts from SW.
- Parameters
-
[in] flagsRTCC interrupt sources to set to pending. Use a set of interrupt flags (RTCC_IFS_nnn).
◆ RTCC_Lock()
|
inline |
Lock RTCC registers.
- Note
- When RTCC registers are locked, RTCC_CTRL, RTCC_PRECNT, RTCC_CNT, RTCC_TIME, RTCC_DATE, RTCC_IEN, RTCC_POWERDOWN and RTCC_CCx_XXX registers cannot be written to.
◆ RTCC_PreCounterGet()
|
inline |
Get the RTCC pre-counter value.
- Returns
- Current RTCC pre-counter value.
◆ RTCC_PreCounterSet()
|
inline |
Set the RTCC pre-counter value.
- Parameters
-
[in] preCntValRTCC pre-counter value to be set.
◆ RTCC_Reset()
| void RTCC_Reset | ( | void |
|
) |
Restore RTCC to its reset state.
◆ RTCC_StatusClear()
| void RTCC_StatusClear | ( | void |
|
) |
Clear the STATUS register.
◆ RTCC_StatusGet()
|
inline |
Get the STATUS register value.
- Returns
- Current STATUS register value.
◆ RTCC_SyncWait()
|
inline |
Wait for the RTCC to complete all synchronization of register changes and commands.
◆ RTCC_Start()
|
inline |
Start the RTCC counter.
This function will send a start command to the RTCC peripheral. The RTCC peripheral will use some LF clock ticks before the command is executed. The RTCC_SyncWait() function can be used to wait for the start command to be executed.
- Note
- This function requires the RTCC to be enabled.
◆ RTCC_Stop()
|
inline |
Stop the RTCC counter.
This function will send a stop command to the RTCC peripheral. The RTCC peripheral will use some LF clock ticks before the command is executed. The RTCC_SyncWait() function can be used to wait for the stop command to be executed.
- Note
- This function requires the RTCC to be enabled.
◆ RTCC_Unlock()
|
inline |
Unlock RTCC registers.
- Note
- When RTCC registers are locked, RTCC_CTRL, RTCC_PRECNT, RTCC_CNT, RTCC_TIME, RTCC_DATE, RTCC_IEN, RTCC_POWERDOWN and RTCC_CCx_XXX registers cannot be written to.
Macro Definition Documentation
◆ RTCC_INIT_DEFAULT
| #define RTCC_INIT_DEFAULT |
Default RTCC initialization structure.
◆ RTCC_CH_INIT_COMPARE_DEFAULT
| #define RTCC_CH_INIT_COMPARE_DEFAULT |
Default RTCC channel output compare initialization structure.
◆ RTCC_CH_INIT_CAPTURE_DEFAULT
| #define RTCC_CH_INIT_CAPTURE_DEFAULT |
Default RTCC channel input capture initialization structure.
◆ RTCC_CH_VALID
| #define RTCC_CH_VALID | ( |
ch
|
) | ((unsigned)(ch) < RTCC_CC_NUM) |
Number of RTCC capture/compare channels.
Validation of valid RTCC channel for assert statements.
Typedef Documentation
◆ RTCC_PRSSel_TypeDef
| typedef uint8_t RTCC_PRSSel_TypeDef |
PRS channel number.
This type is used when configuring input capture mode on a RTCC channel.
Enumeration Type Documentation
◆ RTCC_CntPresc_TypeDef
Counter prescaler selection.