IADC_SingleInput_t Struct Reference
IADC single input selection structure.
      
       #include <em_iadc.h>
      
     
| Data Fields | |
| IADC_NegInput_t | negInput | 
| Port/pin input for the negative side of the ADC. | |
| IADC_PosInput_t | posInput | 
| Port/pin input for the positive side of the ADC. | |
| uint8_t | configId | 
| Configuration id. | |
| bool | compare | 
| Perform digital window comparison on the result from this entry. | |
IADC single input selection structure.
Field Documentation
◆ negInput
| IADC_NegInput_t IADC_SingleInput_t::negInput | 
Port/pin input for the negative side of the ADC.
        
       
◆ posInput
| IADC_PosInput_t IADC_SingleInput_t::posInput | 
Port/pin input for the positive side of the ADC.
        
       
◆ configId
| uint8_t IADC_SingleInput_t::configId | 
Configuration id.
◆ compare
| bool IADC_SingleInput_t::compare | 
Perform digital window comparison on the result from this entry.