ADC - Analog to Digital Converter#

Analog to Digital Converter (ADC) Peripheral API.

This module contains functions to control the ADC peripheral of Silicon Labs 32-bit MCUs and SoCs. The ADC is used to convert analog signals into a digital representation.

Modules#

ADC_Init_TypeDef

ADC_InitScanInput_TypeDef

ADC_InitScan_TypeDef

ADC_InitSingle_TypeDef

Enumerations#

enum
adcAcqTime1 = _ADC_SINGLECTRL_AT_1CYCLE
adcAcqTime2 = _ADC_SINGLECTRL_AT_2CYCLES
adcAcqTime4 = _ADC_SINGLECTRL_AT_4CYCLES
adcAcqTime8 = _ADC_SINGLECTRL_AT_8CYCLES
adcAcqTime16 = _ADC_SINGLECTRL_AT_16CYCLES
adcAcqTime32 = _ADC_SINGLECTRL_AT_32CYCLES
adcAcqTime64 = _ADC_SINGLECTRL_AT_64CYCLES
adcAcqTime128 = _ADC_SINGLECTRL_AT_128CYCLES
adcAcqTime256 = _ADC_SINGLECTRL_AT_256CYCLES
}

Acquisition time (in ADC clock cycles).

enum
adcLPFilterBypass = _ADC_CTRL_LPFMODE_BYPASS
adcLPFilterRC = _ADC_CTRL_LPFMODE_RCFILT
adcLPFilterDeCap = _ADC_CTRL_LPFMODE_DECAP
}

Lowpass filter mode.

enum
adcOvsRateSel2 = _ADC_CTRL_OVSRSEL_X2
adcOvsRateSel4 = _ADC_CTRL_OVSRSEL_X4
adcOvsRateSel8 = _ADC_CTRL_OVSRSEL_X8
adcOvsRateSel16 = _ADC_CTRL_OVSRSEL_X16
adcOvsRateSel32 = _ADC_CTRL_OVSRSEL_X32
adcOvsRateSel64 = _ADC_CTRL_OVSRSEL_X64
adcOvsRateSel128 = _ADC_CTRL_OVSRSEL_X128
adcOvsRateSel256 = _ADC_CTRL_OVSRSEL_X256
adcOvsRateSel512 = _ADC_CTRL_OVSRSEL_X512
adcOvsRateSel1024 = _ADC_CTRL_OVSRSEL_X1024
adcOvsRateSel2048 = _ADC_CTRL_OVSRSEL_X2048
adcOvsRateSel4096 = _ADC_CTRL_OVSRSEL_X4096
}

Oversample rate select.

enum
adcPRSSELCh0 = _ADC_SINGLECTRL_PRSSEL_PRSCH0
adcPRSSELCh1 = _ADC_SINGLECTRL_PRSSEL_PRSCH1
adcPRSSELCh2 = _ADC_SINGLECTRL_PRSSEL_PRSCH2
adcPRSSELCh3 = _ADC_SINGLECTRL_PRSSEL_PRSCH3
adcPRSSELCh4 = _ADC_SINGLECTRL_PRSSEL_PRSCH4
adcPRSSELCh5 = _ADC_SINGLECTRL_PRSSEL_PRSCH5
adcPRSSELCh6 = _ADC_SINGLECTRL_PRSSEL_PRSCH6
adcPRSSELCh7 = _ADC_SINGLECTRL_PRSSEL_PRSCH7
adcPRSSELCh8 = _ADC_SINGLECTRL_PRSSEL_PRSCH8
adcPRSSELCh9 = _ADC_SINGLECTRL_PRSSEL_PRSCH9
adcPRSSELCh10 = _ADC_SINGLECTRL_PRSSEL_PRSCH10
adcPRSSELCh11 = _ADC_SINGLECTRL_PRSSEL_PRSCH11
}

Peripheral Reflex System signal used to trigger a single sample.

enum
adcRef1V25 = _ADC_SINGLECTRL_REF_1V25
adcRef2V5 = _ADC_SINGLECTRL_REF_2V5
adcRefVDD = _ADC_SINGLECTRL_REF_VDD
adcRef5VDIFF = _ADC_SINGLECTRL_REF_5VDIFF
adcRefExtSingle = _ADC_SINGLECTRL_REF_EXTSINGLE
adcRef2xExtDiff = _ADC_SINGLECTRL_REF_2XEXTDIFF
adcRef2xVDD = _ADC_SINGLECTRL_REF_2XVDD
}

Single and scan mode voltage references.

enum
adcRes12Bit = _ADC_SINGLECTRL_RES_12BIT
adcRes8Bit = _ADC_SINGLECTRL_RES_8BIT
adcRes6Bit = _ADC_SINGLECTRL_RES_6BIT
adcResOVS = _ADC_SINGLECTRL_RES_OVS
}

Sample resolution.

enum
adcSingleInputCh0 = _ADC_SINGLECTRL_INPUTSEL_CH0
adcSingleInputCh1 = _ADC_SINGLECTRL_INPUTSEL_CH1
adcSingleInputCh2 = _ADC_SINGLECTRL_INPUTSEL_CH2
adcSingleInputCh3 = _ADC_SINGLECTRL_INPUTSEL_CH3
adcSingleInputCh4 = _ADC_SINGLECTRL_INPUTSEL_CH4
adcSingleInputCh5 = _ADC_SINGLECTRL_INPUTSEL_CH5
adcSingleInputCh6 = _ADC_SINGLECTRL_INPUTSEL_CH6
adcSingleInputCh7 = _ADC_SINGLECTRL_INPUTSEL_CH7
adcSingleInputTemp = _ADC_SINGLECTRL_INPUTSEL_TEMP
adcSingleInputVDDDiv3 = _ADC_SINGLECTRL_INPUTSEL_VDDDIV3
adcSingleInputVDD = _ADC_SINGLECTRL_INPUTSEL_VDD
adcSingleInputVSS = _ADC_SINGLECTRL_INPUTSEL_VSS
adcSingleInputVrefDiv2 = _ADC_SINGLECTRL_INPUTSEL_VREFDIV2
adcSingleInputDACOut0 = _ADC_SINGLECTRL_INPUTSEL_DAC0OUT0
adcSingleInputDACOut1 = _ADC_SINGLECTRL_INPUTSEL_DAC0OUT1
adcSingleInputATEST = 15
adcSingleInputCh0Ch1 = _ADC_SINGLECTRL_INPUTSEL_CH0CH1
adcSingleInputCh2Ch3 = _ADC_SINGLECTRL_INPUTSEL_CH2CH3
adcSingleInputCh4Ch5 = _ADC_SINGLECTRL_INPUTSEL_CH4CH5
adcSingleInputCh6Ch7 = _ADC_SINGLECTRL_INPUTSEL_CH6CH7
adcSingleInputDiff0 = 4
}

Single sample input selection.

enum
adcStartSingle = ADC_CMD_SINGLESTART
adcStartScan = ADC_CMD_SCANSTART
adcStartScanAndSingle = ADC_CMD_SCANSTART | ADC_CMD_SINGLESTART
}

ADC start command.

enum
adcWarmupNormal = _ADC_CTRL_WARMUPMODE_NORMAL
adcWarmupFastBG = _ADC_CTRL_WARMUPMODE_FASTBG
adcWarmupKeepScanRefWarm = _ADC_CTRL_WARMUPMODE_KEEPSCANREFWARM
adcWarmupKeepADCWarm = _ADC_CTRL_WARMUPMODE_KEEPADCWARM
}

Warm-up mode.

Functions#

uint32_t
ADC_DataSingleGet(ADC_TypeDef *adc)

Get a single conversion result.

uint32_t
ADC_DataSinglePeek(ADC_TypeDef *adc)

Peek single conversion result.

uint32_t
ADC_DataScanGet(ADC_TypeDef *adc)

Get a scan result.

uint32_t
ADC_DataScanPeek(ADC_TypeDef *adc)

Peek scan result.

void
ADC_Init(ADC_TypeDef *adc, const ADC_Init_TypeDef *init)

Initialize ADC.

void
ADC_Reset(ADC_TypeDef *adc)

Reset ADC to a state that it was in after a hardware reset.

void
ADC_InitScan(ADC_TypeDef *adc, const ADC_InitScan_TypeDef *init)

Initialize the ADC scan sequence.

void
ADC_InitSingle(ADC_TypeDef *adc, const ADC_InitSingle_TypeDef *init)

Initialize the single ADC sample conversion.

uint8_t
ADC_TimebaseCalc(uint32_t hfperFreq)

Calculate a timebase value to get a timebase providing at least 1 us.

uint8_t
ADC_PrescaleCalc(uint32_t adcFreq, uint32_t hfperFreq)

Calculate the prescaler value used to determine the ADC clock.

void
ADC_IntClear(ADC_TypeDef *adc, uint32_t flags)

Clear one or more pending ADC interrupts.

void
ADC_IntDisable(ADC_TypeDef *adc, uint32_t flags)

Disable one or more ADC interrupts.

void
ADC_IntEnable(ADC_TypeDef *adc, uint32_t flags)

Enable one or more ADC interrupts.

uint32_t
ADC_IntGet(ADC_TypeDef *adc)

Get pending ADC interrupt flags.

uint32_t
ADC_IntGetEnabled(ADC_TypeDef *adc)

Get enabled and pending ADC interrupt flags.

void
ADC_IntSet(ADC_TypeDef *adc, uint32_t flags)

Set one or more pending ADC interrupts from software.

void
ADC_Start(ADC_TypeDef *adc, ADC_Start_TypeDef cmd)

Start scan sequence and/or single conversion.

Macros#

#define

Default configuration for ADC initialization structure.

#define

Default configuration for ADC scan initialization structure.

#define

Default configuration for ADC single conversion initialization structure.

Enumeration Documentation#

ADC_AcqTime_TypeDef#

ADC_AcqTime_TypeDef

Acquisition time (in ADC clock cycles).

Enumerator
adcAcqTime1

1 clock cycle.

adcAcqTime2

2 clock cycles.

adcAcqTime4

4 clock cycles.

adcAcqTime8

8 clock cycles.

adcAcqTime16

16 clock cycles.

adcAcqTime32

32 clock cycles.

adcAcqTime64

64 clock cycles.

adcAcqTime128

128 clock cycles.

adcAcqTime256

256 clock cycles.


ADC_LPFilter_TypeDef#

ADC_LPFilter_TypeDef

Lowpass filter mode.

Enumerator
adcLPFilterBypass

No filter or decoupling capacitor.

adcLPFilterRC

On-chip RC filter.

adcLPFilterDeCap

On-chip decoupling capacitor.


ADC_OvsRateSel_TypeDef#

ADC_OvsRateSel_TypeDef

Oversample rate select.

Enumerator
adcOvsRateSel2

2 samples per conversion result.

adcOvsRateSel4

4 samples per conversion result.

adcOvsRateSel8

8 samples per conversion result.

adcOvsRateSel16

16 samples per conversion result.

adcOvsRateSel32

32 samples per conversion result.

adcOvsRateSel64

64 samples per conversion result.

adcOvsRateSel128

128 samples per conversion result.

adcOvsRateSel256

256 samples per conversion result.

adcOvsRateSel512

512 samples per conversion result.

adcOvsRateSel1024

1024 samples per conversion result.

adcOvsRateSel2048

2048 samples per conversion result.

adcOvsRateSel4096

4096 samples per conversion result.


ADC_PRSSEL_TypeDef#

ADC_PRSSEL_TypeDef

Peripheral Reflex System signal used to trigger a single sample.

Enumerator
adcPRSSELCh0

PRS channel 0.

adcPRSSELCh1

PRS channel 1.

adcPRSSELCh2

PRS channel 2.

adcPRSSELCh3

PRS channel 3.

adcPRSSELCh4

PRS channel 4.

adcPRSSELCh5

PRS channel 5.

adcPRSSELCh6

PRS channel 6.

adcPRSSELCh7

PRS channel 7.

adcPRSSELCh8

PRS channel 8.

adcPRSSELCh9

PRS channel 9.

adcPRSSELCh10

PRS channel 10.

adcPRSSELCh11

PRS channel 11.


ADC_Ref_TypeDef#

ADC_Ref_TypeDef

Single and scan mode voltage references.

Using unshifted enumerations and or in ADC_CTRLX_VREFSEL_REG to select the extension register CTRLX_VREFSEL. ADC Reference

Enumerator
adcRef1V25

Internal 1.25 V reference.

adcRef2V5

Internal 2.5 V reference.

adcRefVDD

Buffered VDD.

adcRef5VDIFF

Internal differential 5 V reference.

adcRefExtSingle

Single-ended external reference from pin 6.

adcRef2xExtDiff

Differential external reference from pin 6 and 7.

adcRef2xVDD

Unbuffered 2xVDD.


ADC_Res_TypeDef#

ADC_Res_TypeDef

Sample resolution.

Enumerator
adcRes12Bit

12 bit sampling.

adcRes8Bit

8 bit sampling.

adcRes6Bit

6 bit sampling.

adcResOVS

Oversampling.


ADC_SingleInput_TypeDef#

ADC_SingleInput_TypeDef

Single sample input selection.

Enumerator
adcSingleInputCh0

Channel 0.

adcSingleInputCh1

Channel 1.

adcSingleInputCh2

Channel 2.

adcSingleInputCh3

Channel 3.

adcSingleInputCh4

Channel 4.

adcSingleInputCh5

Channel 5.

adcSingleInputCh6

Channel 6.

adcSingleInputCh7

Channel 7.

adcSingleInputTemp

Temperature reference.

adcSingleInputVDDDiv3

VDD divided by 3.

adcSingleInputVDD

VDD.

adcSingleInputVSS

VSS.

adcSingleInputVrefDiv2

Vref divided by 2.

adcSingleInputDACOut0

DAC output 0.

adcSingleInputDACOut1

DAC output 1.

adcSingleInputATEST

ATEST.

adcSingleInputCh0Ch1

Positive Ch0, negative Ch1.

adcSingleInputCh2Ch3

Positive Ch2, negative Ch3.

adcSingleInputCh4Ch5

Positive Ch4, negative Ch5.

adcSingleInputCh6Ch7

Positive Ch6, negative Ch7.

adcSingleInputDiff0

Differential 0.


ADC_Start_TypeDef#

ADC_Start_TypeDef

ADC start command.

Enumerator
adcStartSingle

Start a single conversion.

adcStartScan

Start a scan sequence.

adcStartScanAndSingle

Start a scan sequence and single conversion, typically used when tailgating a single conversion after a scan sequence.


ADC_Warmup_TypeDef#

ADC_Warmup_TypeDef

Warm-up mode.

Enumerator
adcWarmupNormal

ADC shutdown after each conversion.

adcWarmupFastBG

Do not warm up bandgap references.

adcWarmupKeepScanRefWarm

Reference selected for scan mode kept warm.

adcWarmupKeepADCWarm

ADC and reference selected for scan mode kept at warmup allowing continuous conversion.


Function Documentation#

ADC_DataSingleGet#

uint32_t ADC_DataSingleGet (ADC_TypeDef * adc)

Get a single conversion result.

Parameters
TypeDirectionArgument NameDescription
ADC_TypeDef *[in]adc

A pointer to the ADC peripheral register block.

Note

  • Check data valid flag before calling this function.

Returns

  • Single conversion data.


ADC_DataSinglePeek#

uint32_t ADC_DataSinglePeek (ADC_TypeDef * adc)

Peek single conversion result.

Parameters
TypeDirectionArgument NameDescription
ADC_TypeDef *[in]adc

A pointer to the ADC peripheral register block.

Note

  • Check data valid flag before calling this function.

Returns

  • Single conversion data.


ADC_DataScanGet#

uint32_t ADC_DataScanGet (ADC_TypeDef * adc)

Get a scan result.

Parameters
TypeDirectionArgument NameDescription
ADC_TypeDef *[in]adc

A pointer to the ADC peripheral register block.

Note

  • Check data valid flag before calling this function.

Returns

  • Scan conversion data.


ADC_DataScanPeek#

uint32_t ADC_DataScanPeek (ADC_TypeDef * adc)

Peek scan result.

Parameters
TypeDirectionArgument NameDescription
ADC_TypeDef *[in]adc

A pointer to the ADC peripheral register block.

Note

  • Check data valid flag before calling this function.

Returns

  • Scan conversion data.


ADC_Init#

void ADC_Init (ADC_TypeDef * adc, const ADC_Init_TypeDef * init)

Initialize ADC.

Parameters
TypeDirectionArgument NameDescription
ADC_TypeDef *[in]adc

A pointer to the ADC peripheral register block.

const ADC_Init_TypeDef *[in]init

A pointer to the ADC initialization structure.

Initializes common parts for both single conversion and scan sequence. In addition, single and/or scan control configuration must be done. See ADC_InitSingle() and ADC_InitScan() respectively. For ADC architectures with the ADCn->SCANINPUTSEL register, use ADC_ScanSingleEndedInputAdd() to configure single-ended scan inputs or ADC_ScanDifferentialInputAdd() to configure differential scan inputs. ADC_ScanInputClear() is also provided for applications that need to update the input configuration.

Note

  • This function will stop any ongoing conversion.


ADC_Reset#

void ADC_Reset (ADC_TypeDef * adc)

Reset ADC to a state that it was in after a hardware reset.

Parameters
TypeDirectionArgument NameDescription
ADC_TypeDef *[in]adc

A pointer to ADC peripheral register block.

Note

  • The ROUTE register is NOT reset by this function to allow a centralized setup of this feature.


ADC_InitScan#

void ADC_InitScan (ADC_TypeDef * adc, const ADC_InitScan_TypeDef * init)

Initialize the ADC scan sequence.

Parameters
TypeDirectionArgument NameDescription
ADC_TypeDef *[in]adc

A pointer to the ADC peripheral register block.

const ADC_InitScan_TypeDef *[in]init

A pointer to the ADC initialization structure.

See ADC_Start() for starting a scan sequence.

When selecting an external reference, the gain and offset calibration must be set explicitly (CAL register). For other references, the calibration is updated with values defined during manufacturing. For ADC architectures with the ADCn->SCANINPUTSEL register, use ADC_ScanSingleEndedInputAdd() to configure single-ended scan inputs or ADC_ScanDifferentialInputAdd() to configure differential scan inputs. ADC_ScanInputClear() is also provided for applications that need to update the input configuration.

Note

  • This function will stop any ongoing scan sequence.


ADC_InitSingle#

void ADC_InitSingle (ADC_TypeDef * adc, const ADC_InitSingle_TypeDef * init)

Initialize the single ADC sample conversion.

Parameters
TypeDirectionArgument NameDescription
ADC_TypeDef *[in]adc

A pointer to the ADC peripheral register block.

const ADC_InitSingle_TypeDef *[in]init

A pointer to the ADC initialization structure.

See ADC_Start() for starting a single conversion.

When selecting an external reference, the gain and offset calibration must be set explicitly (CAL register). For other references, the calibration is updated with values defined during manufacturing.

Note

  • This function will stop any ongoing single conversion.


ADC_TimebaseCalc#

uint8_t ADC_TimebaseCalc (uint32_t hfperFreq)

Calculate a timebase value to get a timebase providing at least 1 us.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]hfperFreq

Frequency in Hz of the reference HFPER/HFPERC clock. Set to 0 to use currently defined HFPER/HFPERC clock setting.

Returns

  • A timebase value to use for ADC to achieve at least 1 us.


ADC_PrescaleCalc#

uint8_t ADC_PrescaleCalc (uint32_t adcFreq, uint32_t hfperFreq)

Calculate the prescaler value used to determine the ADC clock.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]adcFreq

ADC frequency wanted. The frequency will automatically be adjusted to a valid range according to the reference manual.

uint32_t[in]hfperFreq

Frequency in Hz of reference HFPER/HFPERC clock. Set to 0 to use currently defined HFPER/HFPERC clock setting.

The ADC clock is given by: (HFPERCLK or HFPERCCLK) / (prescale + 1).

Note

  • The return value is clamped to the maximum prescaler value that the hardware supports.

Returns

  • A prescaler value to use for ADC in order to achieve a clock value <= adcFreq.


ADC_IntClear#

void ADC_IntClear (ADC_TypeDef * adc, uint32_t flags)

Clear one or more pending ADC interrupts.

Parameters
TypeDirectionArgument NameDescription
ADC_TypeDef *[in]adc

A pointer to the ADC peripheral register block.

uint32_t[in]flags

Pending ADC interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the ADC module (ADC_IF_nnn).


ADC_IntDisable#

void ADC_IntDisable (ADC_TypeDef * adc, uint32_t flags)

Disable one or more ADC interrupts.

Parameters
TypeDirectionArgument NameDescription
ADC_TypeDef *[in]adc

A pointer to the ADC peripheral register block.

uint32_t[in]flags

ADC interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the ADC module (ADC_IF_nnn).


ADC_IntEnable#

void ADC_IntEnable (ADC_TypeDef * adc, uint32_t flags)

Enable one or more ADC interrupts.

Parameters
TypeDirectionArgument NameDescription
ADC_TypeDef *[in]adc

A pointer to the ADC peripheral register block.

uint32_t[in]flags

ADC interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the ADC module (ADC_IF_nnn).

Note

  • Depending on use, a pending interrupt may already be set prior to enabling the interrupt. Consider using ADC_IntClear() prior to enabling if the pending interrupt should be ignored.


ADC_IntGet#

uint32_t ADC_IntGet (ADC_TypeDef * adc)

Get pending ADC interrupt flags.

Parameters
TypeDirectionArgument NameDescription
ADC_TypeDef *[in]adc

A pointer to the ADC peripheral register block.

Note

  • This function does not clear event bits.

Returns

  • ADC interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the ADC module (ADC_IF_nnn).


ADC_IntGetEnabled#

uint32_t ADC_IntGetEnabled (ADC_TypeDef * adc)

Get enabled and pending ADC interrupt flags.

Parameters
TypeDirectionArgument NameDescription
ADC_TypeDef *[in]adc

A pointer to the ADC peripheral register block.

Useful for handling more interrupt sources in the same interrupt handler.

Note

  • This function does not clear interrupt flags.

Returns

  • Pending and enabled ADC interrupt sources. The return value is the bitwise AND combination of

    • the OR combination of enabled interrupt sources in ADCx_IEN_nnn register (ADCx_IEN_nnn) and

    • the OR combination of valid interrupt flags of the ADC module (ADCx_IF_nnn).


ADC_IntSet#

void ADC_IntSet (ADC_TypeDef * adc, uint32_t flags)

Set one or more pending ADC interrupts from software.

Parameters
TypeDirectionArgument NameDescription
ADC_TypeDef *[in]adc

A pointer to the ADC peripheral register block.

uint32_t[in]flags

ADC interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the ADC module (ADC_IF_nnn).


ADC_Start#

void ADC_Start (ADC_TypeDef * adc, ADC_Start_TypeDef cmd)

Start scan sequence and/or single conversion.

Parameters
TypeDirectionArgument NameDescription
ADC_TypeDef *[in]adc

A pointer to the ADC peripheral register block.

ADC_Start_TypeDef[in]cmd

A command indicating which type of sampling to start.


Macro Definition Documentation#

ADC_INIT_DEFAULT#

#define ADC_INIT_DEFAULT
Value:
{ \
adcOvsRateSel2, /* 2x oversampling (if enabled). */ \
adcLPFilterBypass, /* No input filter selected. */ \
adcWarmupNormal, /* ADC shutdown after each conversion. */ \
_ADC_CTRL_TIMEBASE_DEFAULT, /* Use hardware default value. */ \
_ADC_CTRL_PRESC_DEFAULT, /* Use hardware default value. */ \
false /* Do not use tailgate. */ \
}

Default configuration for ADC initialization structure.


ADC_INITSCAN_DEFAULT#

#define ADC_INITSCAN_DEFAULT
Value:
{ \
adcPRSSELCh0, /* PRS ch0 (if enabled). */ \
adcAcqTime1, /* 1 ADC_CLK cycle acquisition time. */ \
adcRef1V25, /* 1.25 V internal reference. */ \
adcRes12Bit, /* 12 bit resolution. */ \
0, /* No input selected. */ \
false, /* Single-ended input. */ \
false, /* PRS disabled. */ \
false, /* Right adjust. */ \
false, /* Deactivate conversion after one scan sequence. */ \
}

Default configuration for ADC scan initialization structure.


ADC_INITSINGLE_DEFAULT#

#define ADC_INITSINGLE_DEFAULT
Value:
{ \
adcPRSSELCh0, /* PRS ch0 (if enabled). */ \
adcAcqTime1, /* 1 ADC_CLK cycle acquisition time. */ \
adcRef1V25, /* 1.25 V internal reference. */ \
adcRes12Bit, /* 12 bit resolution. */ \
adcSingleInpCh0, /* CH0 input selected. */ \
false, /* Single-ended input. */ \
false, /* PRS disabled. */ \
false, /* Right adjust. */ \
false /* Deactivate conversion after one scan sequence. */ \
}

Default configuration for ADC single conversion initialization structure.