API Documentation#

List of Modules

Description

BMP280 - Barometric Pressure Sensor

Driver for the Bosch Sensortec BMP280 barometric pressure sensor

BMP3xx - Barometric Pressure Sensor

Driver for the Bosch Sensortec BMP3xx barometric pressure sensor

CCS811 - Gas Sensor

Driver for the Cambridge CMOS Sensors CCS811 gas and indoor air quality sensor

Configuration Over SWO

Configuration Over SWO

EFP - Energy Friendly PMIC

EFP (Energy Friendly PMIC) driver

ICM20648 - Motion Sensor

Driver for the Invensense ICM20648 6-axis motion sensor

ICM20689 - Motion Sensor

Driver for the Invensense ICM20689 6-axis motion sensor

IMU - Inertial Measurement Unit

Inertial Measurement Unit driver

Joystick platform-hardware-driver

Joystick platform-hardware-driver

MEMLCD - Memory LCD

Memory LCD interface

MX25 SPI Flash Shutdown

Provide a function to put the MX25 SPI flash into deep power down mode to reduce power consumption

Microphone

Sound level driver for PDM and I2S microphones

Si1133 - Light and UV Sensor

Driver for the Silicon Labs Si1133 ambient light and UV sensor

Si70xx - RHT Sensor

Silicon Labs Si7006/13/20/21 Relative Humidity and Temperature Sensor I2C driver

Si7210 - Magnetic Hall Effect sensor

Driver for the Silicon Labs Si7210 Hall effect sensor

Si72xx - Magnetic Hall Effect Sensor

VEML6035 - Ambient Light Sensor

Driver for the Vishay VEML6025 ambient light sensor