DCDC initialization structure.

Public Attributes#

Device external power configuration.

DCDC regulator operating mode in EM0/1.

uint16_t

Target output voltage (mV).

uint16_t

Estimated average load current in EM0/1.

uint16_t

Estimated average load current in EM2 (uA).

uint16_t

Maximum average DCDC output current (mA).

Select analog peripheral power in DCDC-to-DVDD mode.

DCDC Low-noise mode compensator control.

Public Attribute Documentation#

powerConfig#

EMU_PowerConfig_TypeDef EMU_DCDCInit_TypeDef::powerConfig

Device external power configuration.

emuPowerConfig_DcdcToDvdd is currently the only supported mode.


Definition at line 952 of file platform/emlib/inc/em_emu.h

dcdcMode#

EMU_DcdcMode_TypeDef EMU_DCDCInit_TypeDef::dcdcMode

DCDC regulator operating mode in EM0/1.


Definition at line 954 of file platform/emlib/inc/em_emu.h

mVout#

uint16_t EMU_DCDCInit_TypeDef::mVout

Target output voltage (mV).


Definition at line 955 of file platform/emlib/inc/em_emu.h

em01LoadCurrent_mA#

uint16_t EMU_DCDCInit_TypeDef::em01LoadCurrent_mA

Estimated average load current in EM0/1.

(mA). This estimate is also used for EM1 optimization; if EM1 current is expected to be higher than EM0, then this parameter should hold the higher EM1 current.


Definition at line 956 of file platform/emlib/inc/em_emu.h

em234LoadCurrent_uA#

uint16_t EMU_DCDCInit_TypeDef::em234LoadCurrent_uA

Estimated average load current in EM2 (uA).

This estimate is also used for EM3 and 4 optimization; if EM3 or 4 current is expected to be higher than EM2, then this parameter should hold the higher EM3 or 4 current.


Definition at line 960 of file platform/emlib/inc/em_emu.h

maxCurrent_mA#

uint16_t EMU_DCDCInit_TypeDef::maxCurrent_mA

Maximum average DCDC output current (mA).

This can be set to the maximum for the power source, for example the maximum for a battery.


Definition at line 964 of file platform/emlib/inc/em_emu.h

anaPeripheralPower#

EMU_DcdcAnaPeripheralPower_TypeDef EMU_DCDCInit_TypeDef::anaPeripheralPower

Select analog peripheral power in DCDC-to-DVDD mode.


Definition at line 968 of file platform/emlib/inc/em_emu.h

reverseCurrentControl#

EMU_DcdcLnReverseCurrentControl_TypeDef EMU_DCDCInit_TypeDef::reverseCurrentControl

Low-noise reverse current control.

NOTE: this parameter uses special encoding: >= 0 is forced CCM mode where the parameter is used as the reverse current threshold in mA. -1 is encoded as emuDcdcLnHighEfficiencyMode (EFM32 only).


Definition at line 970 of file platform/emlib/inc/em_emu.h

dcdcLnCompCtrl#

EMU_DcdcLnCompCtrl_TypeDef EMU_DCDCInit_TypeDef::dcdcLnCompCtrl

DCDC Low-noise mode compensator control.


Definition at line 975 of file platform/emlib/inc/em_emu.h