QSPI Device Write Instruction Configuration Structure.
Public Attributes#
uint8_t
Write opcode.
uint8_t
Number of dummy read clock cycles.
Transfer type used for address.
Transfer type used for data.
bool
Enable/disable automatic issuing of WEL (Write Enable Latch) command before a write operation.
Public Attribute Documentation#
addrTransfer#
QSPI_TransferType_TypeDef QSPI_WriteConfig_TypeDef::addrTransfer
Transfer type used for address.
dataTransfer#
QSPI_TransferType_TypeDef QSPI_WriteConfig_TypeDef::dataTransfer
Transfer type used for data.
autoWEL#
bool QSPI_WriteConfig_TypeDef::autoWEL
Enable/disable automatic issuing of WEL (Write Enable Latch) command before a write operation.
When writing to a flash device, the WEL within the flash device must be high before a write sequence can be issued. The QSPI peripheral can automatically issue the WEL command before triggering a write sequence. The command used for enabling the WEL is WREN (0x06) and is common between devices.