You are viewing documentation for version:
CAN initialization structure.
Public Attributes#
bool
True to set the CAN Device in normal mode after initialization.
bool
True to reset messages during initialization.
uint8_t
Default Propagation Time Segment.
uint8_t
Default Phase Buffer Segment 1.
uint8_t
Default Phase Buffer Segment 2.
uint8_t
Default Synchronization Jump Width.
Public Attribute Documentation#
enable#
bool CAN_Init_TypeDef::enable
True to set the CAN Device in normal mode after initialization.
resetMessages#
bool CAN_Init_TypeDef::resetMessages
True to reset messages during initialization.
bitrate#
uint32_t CAN_Init_TypeDef::bitrate
Default bitrate.
propagationTimeSegment#
uint8_t CAN_Init_TypeDef::propagationTimeSegment
Default Propagation Time Segment.
phaseBufferSegment1#
uint8_t CAN_Init_TypeDef::phaseBufferSegment1
Default Phase Buffer Segment 1.
phaseBufferSegment2#
uint8_t CAN_Init_TypeDef::phaseBufferSegment2
Default Phase Buffer Segment 2.
synchronisationJumpWidth#
uint8_t CAN_Init_TypeDef::synchronisationJumpWidth
Default Synchronization Jump Width.