HFXO initialization structure.
Initialization values should be obtained from a configuration tool, application note or crystal data sheet.
Public Attributes#
uint16_t
Startup phase CTUNE (load capacitance) value.
uint16_t
Steady-state phase CTUNE (load capacitance) value.
uint16_t
Startup XO core bias current trim.
uint16_t
Steady-state XO core bias current trim.
uint8_t
Timeout - peak detection.
uint8_t
Timeout - steady-state.
uint8_t
Timeout - startup.
Oscillator mode.
Public Attribute Documentation#
ctuneStartup#
uint16_t CMU_HFXOInit_TypeDef::ctuneStartup
Startup phase CTUNE (load capacitance) value.
ctuneSteadyState#
uint16_t CMU_HFXOInit_TypeDef::ctuneSteadyState
Steady-state phase CTUNE (load capacitance) value.
xoCoreBiasTrimStartup#
uint16_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimStartup
Startup XO core bias current trim.
xoCoreBiasTrimSteadyState#
uint16_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimSteadyState
Steady-state XO core bias current trim.