Core control (LESENSE_CTRL/CFG) descriptor structure.
Public Attributes#
Select scan start mode to control how the scan start is being triggered.
Select PRS source for scan start if scanMode is set to lesensePrsPulse.
Select scan configuration register usage strategy.
Set to true to invert ACMP0 output.
Set to true to invert ACMP1 output.
Set to true to sample both ACMPs simultaneously.
Set to true in order to store SCANRES in the RAM (accessible via RESDATA) after each scan.
Set to true in order to always make LESENSE write to the result buffer, even if it is full.
Select trigger conditions for the interrupt and DMA.
Configure trigger condition for the DMA wakeup from EM2.
Select bias mode.
Set to true to keep LESENSE running in the debug mode.
Public Attribute Documentation#
scanStart#
LESENSE_ScanMode_TypeDef LESENSE_CoreCtrlDesc_TypeDef::scanStart
Select scan start mode to control how the scan start is being triggered.
prsSel#
LESENSE_PRSSel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::prsSel
Select PRS source for scan start if scanMode is set to lesensePrsPulse.
scanConfSel#
LESENSE_ScanConfSel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::scanConfSel
Select scan configuration register usage strategy.
dualSample#
bool LESENSE_CoreCtrlDesc_TypeDef::dualSample
Set to true to sample both ACMPs simultaneously.
storeScanRes#
bool LESENSE_CoreCtrlDesc_TypeDef::storeScanRes
Set to true in order to store SCANRES in the RAM (accessible via RESDATA) after each scan.
bufOverWr#
bool LESENSE_CoreCtrlDesc_TypeDef::bufOverWr
Set to true in order to always make LESENSE write to the result buffer, even if it is full.
bufTrigLevel#
LESENSE_BufTrigLevel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::bufTrigLevel
Select trigger conditions for the interrupt and DMA.
wakeupOnDMA#
LESENSE_DMAWakeUp_TypeDef LESENSE_CoreCtrlDesc_TypeDef::wakeupOnDMA
Configure trigger condition for the DMA wakeup from EM2.
debugRun#
bool LESENSE_CoreCtrlDesc_TypeDef::debugRun
Set to true to keep LESENSE running in the debug mode.