You are viewing documentation for version:
LFXO initialization structure. 
Initialization values should be obtained from a configuration tool, application note or crystal data sheet. 
Public Attributes#
uint8_t
Internal capacitance tuning. 
bool
EM4 wakeup on failure enable. 
bool
Oscillator failure detection enable. 
bool
Disable on-demand requests. 
Public Attribute Documentation#
gain#
uint8_t CMU_LFXOInit_TypeDef::gain
Startup gain. 
capTune#
uint8_t CMU_LFXOInit_TypeDef::capTune
Internal capacitance tuning. 
timeout#
CMU_LfxoStartupDelay_TypeDef CMU_LFXOInit_TypeDef::timeout
Startup delay. 
mode#
CMU_LfxoOscMode_TypeDef CMU_LFXOInit_TypeDef::mode
Oscillator mode. 
highAmplitudeEn#
bool CMU_LFXOInit_TypeDef::highAmplitudeEn
High amplitude enable. 
agcEn#
bool CMU_LFXOInit_TypeDef::agcEn
AGC enable. 
failDetEM4WUEn#
bool CMU_LFXOInit_TypeDef::failDetEM4WUEn
EM4 wakeup on failure enable. 
failDetEn#
bool CMU_LFXOInit_TypeDef::failDetEn
Oscillator failure detection enable. 
disOnDemand#
bool CMU_LFXOInit_TypeDef::disOnDemand
Disable on-demand requests. 
forceEn#
bool CMU_LFXOInit_TypeDef::forceEn
Force oscillator enable. 
regLock#
bool CMU_LFXOInit_TypeDef::regLock
Lock register access.