Scan sequence initialization structure.
Public Attributes#
Peripheral reflex system trigger selection.
Acquisition time (in ADC clock cycles).
Sample reference selection.
Sample resolution.
Scan input selection.
Select if single-ended or differential input.
Peripheral reflex system trigger enable.
Select if left adjustment should be done.
Select if continuous conversion until explicit stop.
Public Attribute Documentation#
prsSel#
ADC_PRSSEL_TypeDef ADC_InitScan_TypeDef::prsSel
Peripheral reflex system trigger selection.
Only applicable if prsEnable is enabled.
reference#
ADC_Ref_TypeDef ADC_InitScan_TypeDef::reference
Sample reference selection.
Note that, for external references, the ADC calibration register must be set explicitly.
input#
uint32_t ADC_InitScan_TypeDef::input
Scan input selection.
If single ended (diff is false), use logical combination of ADC_SCANCTRL_INPUTMASK_CHx defines. If differential input (diff is true), use logical combination of ADC_SCANCTRL_INPUTMASK_CHxCHy defines. (Notice underscore prefix for defines used.)