Interruptible operations#
Macros#
#define
PSA_INTERRUPTIBLE_MAX_OPS_UNLIMITED UINT32_MAX
Maximum value for use with psa_interruptible_set_max_ops() to determine the maximum number of ops allowed to be executed by an interruptible function in a single call.
#define
PSA_INTERRUPTIBLE_MAX_OPS_UNLIMITED UINT32_MAX
Maximum value for use with psa_interruptible_set_max_ops() to determine the maximum number of ops allowed to be executed by an interruptible function in a single call.