External random generator#
Functions#
External random generator function, implemented by the platform.
Function Documentation#
mbedtls_psa_external_get_random#
psa_status_t mbedtls_psa_external_get_random (mbedtls_psa_external_random_context_t * context, uint8_t * output, size_t output_size, size_t * output_length)
External random generator function, implemented by the platform.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| mbedtls_psa_external_random_context_t * | [inout] | context | Pointer to the random generator context. This is all-bits-zero on the first call and preserved between successive calls. |
| uint8_t * | [out] | output | Output buffer. On success, this buffer contains random data with a uniform distribution. |
| size_t | N/A | output_size | The size of the |
| size_t * | [out] | output_length | On success, set this value to |
When the compile-time option #MBEDTLS_PSA_CRYPTO_EXTERNAL_RNG is enabled, this function replaces Mbed TLS's entropy and DRBG modules for all random generation triggered via PSA crypto interfaces.
Note
This random generator must deliver random numbers with cryptographic quality and high performance. It must supply unpredictable numbers with a uniform distribution. The implementation of this function is responsible for ensuring that the random generator is seeded with sufficient entropy. If you have a hardware TRNG which is slow or delivers non-uniform output, declare it as an entropy source with mbedtls_entropy_add_source() instead of enabling this option.