Interruptible sign/verify hash#
Functions#
Set the maximum number of ops allowed to be executed by an interruptible function in a single call.
Get the maximum number of ops allowed to be executed by an interruptible function in a single call.
Get the number of ops that a hash signing operation has taken so far.
Get the number of ops that a hash verification operation has taken so far.
Start signing a hash or short message with a private key, in an interruptible manner.
Continue and eventually complete the action of signing a hash or short message with a private key, in an interruptible manner.
Abort a sign hash operation.
Start reading and verifying a hash or short message, in an interruptible manner.
Continue and eventually complete the action of reading and verifying a hash or short message signed with a private key, in an interruptible manner.
Abort a verify hash operation.
Function Documentation#
psa_interruptible_set_max_ops#
void psa_interruptible_set_max_ops (uint32_t max_ops)
Set the maximum number of ops allowed to be executed by an interruptible function in a single call.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | max_ops | The maximum number of ops to be executed in a single call. This can be a number from 0 to PSA_INTERRUPTIBLE_MAX_OPS_UNLIMITED, where 0 is the least amount of work done per call. |
Warnings
This is a beta API, and thus subject to change at any point. It is not bound by the usual interface stability promises.
Note
The time taken to execute a single op is implementation specific and depends on software, hardware, the algorithm, key type and curve chosen. Even within a single operation, successive ops can take differing amounts of time. The only guarantee is that lower values for
max_opsmeans functions will block for a lesser maximum amount of time. The functionspsa_sign_interruptible_get_num_ops()andpsa_verify_interruptible_get_num_ops()are provided to help with tuning this value.This value defaults to PSA_INTERRUPTIBLE_MAX_OPS_UNLIMITED, which means the whole operation will be done in one go, regardless of the number of ops required.
If more ops are needed to complete a computation, PSA_OPERATION_INCOMPLETE will be returned by the function performing the computation. It is then the caller's responsibility to either call again with the same operation context until it returns 0 or an error code; or to call the relevant abort function if the answer is no longer required.
The interpretation of
max_opsis also implementation defined. On a hard real time system, this can indicate a hard deadline, as a real-time system needs a guarantee of not spending more than X time, however care must be taken in such an implementation to avoid the situation whereby calls just return, not being able to do any actual work within the allotted time. On a non-real-time system, the implementation can be more relaxed, but again whether this number should be interpreted as as hard or soft limit or even whether a less than or equals as regards to ops executed in a single call is implementation defined.For keys in local storage when no accelerator driver applies, please see also the documentation for
mbedtls_ecp_set_max_ops(), which is the internal implementation in these cases.
Warnings
With implementations that interpret this number as a hard limit, setting this number too small may result in an infinite loop, whereby each call results in immediate return with no ops done (as there is not enough time to execute any), and thus no result will ever be achieved.
Note
This only applies to functions whose documentation mentions they may return PSA_OPERATION_INCOMPLETE.
psa_interruptible_get_max_ops#
uint32_t psa_interruptible_get_max_ops (void )
Get the maximum number of ops allowed to be executed by an interruptible function in a single call.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This will return the last value set by psa_interruptible_set_max_ops() or PSA_INTERRUPTIBLE_MAX_OPS_UNLIMITED if that function has never been called.
Warnings
This is a beta API, and thus subject to change at any point. It is not bound by the usual interface stability promises.
Returns
Maximum number of ops allowed to be executed by an interruptible function in a single call.
psa_sign_hash_get_num_ops#
uint32_t psa_sign_hash_get_num_ops (const psa_sign_hash_interruptible_operation_t * operation)
Get the number of ops that a hash signing operation has taken so far.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const psa_sign_hash_interruptible_operation_t * | N/A | operation | The |
If the operation has completed, then this will represent the number of ops required for the entire operation. After initialization or calling psa_sign_hash_interruptible_abort() on the operation, a value of 0 will be returned.
Note
This interface is guaranteed re-entrant and thus may be called from driver code.
Warnings
This is a beta API, and thus subject to change at any point. It is not bound by the usual interface stability promises.
This is a helper provided to help you tune the value passed to psa_interruptible_set_max_ops().
Returns
Number of ops that the operation has taken so far.
psa_verify_hash_get_num_ops#
uint32_t psa_verify_hash_get_num_ops (const psa_verify_hash_interruptible_operation_t * operation)
Get the number of ops that a hash verification operation has taken so far.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const psa_verify_hash_interruptible_operation_t * | N/A | operation | The |
If the operation has completed, then this will represent the number of ops required for the entire operation. After initialization or calling psa_verify_hash_interruptible_abort() on the operation, a value of 0 will be returned.
Warnings
This is a beta API, and thus subject to change at any point. It is not bound by the usual interface stability promises.
This is a helper provided to help you tune the value passed to psa_interruptible_set_max_ops().
Returns
Number of ops that the operation has taken so far.
psa_sign_hash_start#
psa_status_t psa_sign_hash_start (psa_sign_hash_interruptible_operation_t * operation, mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t * hash, size_t hash_length)
Start signing a hash or short message with a private key, in an interruptible manner.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| psa_sign_hash_interruptible_operation_t * | [inout] | operation | The |
| mbedtls_svc_key_id_t | N/A | key | Identifier of the key to use for the operation. It must be an asymmetric key pair. The key must allow the usage PSA_KEY_USAGE_SIGN_HASH. |
| psa_algorithm_t | N/A | alg | A signature algorithm ( |
| const uint8_t * | [in] | hash | The hash or message to sign. |
| size_t | N/A | hash_length | Size of the |
See Also
psa_sign_hash_complete()
Warnings
This is a beta API, and thus subject to change at any point. It is not bound by the usual interface stability promises.
Note
This function combined with
psa_sign_hash_complete()is equivalent topsa_sign_hash()butpsa_sign_hash_complete()can return early and resume according to the limit set withpsa_interruptible_set_max_ops()to reduce the maximum time spent in a function call.Users should call
psa_sign_hash_complete()repeatedly on the same context after a successful call to this function untilpsa_sign_hash_complete()either returns 0 or an error.psa_sign_hash_complete()will return PSA_OPERATION_INCOMPLETE if there is more work to do. Alternatively users can callpsa_sign_hash_abort()at any point if they no longer want the result.If this function returns an error status, the operation enters an error state and must be aborted by calling
psa_sign_hash_abort().
psa_sign_hash_complete#
psa_status_t psa_sign_hash_complete (psa_sign_hash_interruptible_operation_t * operation, uint8_t * signature, size_t signature_size, size_t * signature_length)
Continue and eventually complete the action of signing a hash or short message with a private key, in an interruptible manner.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| psa_sign_hash_interruptible_operation_t * | [inout] | operation | The |
| uint8_t * | [out] | signature | Buffer where the signature is to be written. |
| size_t | N/A | signature_size | Size of the
|
| size_t * | [out] | signature_length | On success, the number of bytes that make up the returned signature value. |
See Also
psa_sign_hash_start()
Warnings
This is a beta API, and thus subject to change at any point. It is not bound by the usual interface stability promises.
Note
This function combined with
psa_sign_hash_start()is equivalent topsa_sign_hash()but this function can return early and resume according to the limit set withpsa_interruptible_set_max_ops()to reduce the maximum time spent in a function call.Users should call this function on the same operation object repeatedly until it either returns 0 or an error. This function will return PSA_OPERATION_INCOMPLETE if there is more work to do. Alternatively users can call
psa_sign_hash_abort()at any point if they no longer want the result.When this function returns successfully, the operation becomes inactive. If this function returns an error status, the operation enters an error state and must be aborted by calling
psa_sign_hash_abort().
See Also
psa_sign_hash_start()
Warnings
This is a beta API, and thus subject to change at any point. It is not bound by the usual interface stability promises.
Note
This function combined with
psa_sign_hash_start()is equivalent topsa_sign_hash()but this function can return early and resume according to the limit set withpsa_interruptible_set_max_ops()to reduce the maximum time spent in a function call.Users should call this function on the same operation object repeatedly until it either returns 0 or an error. This function will return PSA_OPERATION_INCOMPLETE if there is more work to do. Alternatively users can call
psa_sign_hash_abort()at any point if they no longer want the result.When this function returns successfully, the operation becomes inactive. If this function returns an error status, the operation enters an error state and must be aborted by calling
psa_sign_hash_abort().
psa_sign_hash_abort#
psa_status_t psa_sign_hash_abort (psa_sign_hash_interruptible_operation_t * operation)
Abort a sign hash operation.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| psa_sign_hash_interruptible_operation_t * | [inout] | operation | Initialized sign hash operation. |
Warnings
This is a beta API, and thus subject to change at any point. It is not bound by the usual interface stability promises.
Note
This function is the only function that clears the number of ops completed as part of the operation. Please ensure you copy this value via
psa_sign_hash_get_num_ops()if required before calling.Aborting an operation frees all associated resources except for the
operationstructure itself. Once aborted, the operation object can be reused for another operation by callingpsa_sign_hash_start()again.You may call this function any time after the operation object has been initialized. In particular, calling
psa_sign_hash_abort()after the operation has already been terminated by a call topsa_sign_hash_abort()or psa_sign_hash_complete() is safe.
psa_verify_hash_start#
psa_status_t psa_verify_hash_start (psa_verify_hash_interruptible_operation_t * operation, mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t * hash, size_t hash_length, const uint8_t * signature, size_t signature_length)
Start reading and verifying a hash or short message, in an interruptible manner.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| psa_verify_hash_interruptible_operation_t * | [inout] | operation | The |
| mbedtls_svc_key_id_t | N/A | key | Identifier of the key to use for the operation. The key must allow the usage PSA_KEY_USAGE_VERIFY_HASH. |
| psa_algorithm_t | N/A | alg | A signature algorithm ( |
| const uint8_t * | [in] | hash | The hash whose signature is to be verified. |
| size_t | N/A | hash_length | Size of the |
| const uint8_t * | [in] | signature | Buffer containing the signature to verify. |
| size_t | N/A | signature_length | Size of the |
See Also
psa_verify_hash_complete()
Warnings
This is a beta API, and thus subject to change at any point. It is not bound by the usual interface stability promises.
Note
This function combined with
psa_verify_hash_complete()is equivalent topsa_verify_hash()butpsa_verify_hash_complete()can return early and resume according to the limit set withpsa_interruptible_set_max_ops()to reduce the maximum time spent in a function.Users should call
psa_verify_hash_complete()repeatedly on the same operation object after a successful call to this function untilpsa_verify_hash_complete()either returns 0 or an error.psa_verify_hash_complete()will return PSA_OPERATION_INCOMPLETE if there is more work to do. Alternatively users can callpsa_verify_hash_abort()at any point if they no longer want the result.If this function returns an error status, the operation enters an error state and must be aborted by calling
psa_verify_hash_abort().
psa_verify_hash_complete#
psa_status_t psa_verify_hash_complete (psa_verify_hash_interruptible_operation_t * operation)
Continue and eventually complete the action of reading and verifying a hash or short message signed with a private key, in an interruptible manner.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| psa_verify_hash_interruptible_operation_t * | [inout] | operation | The |
See Also
psa_verify_hash_start()
Warnings
This is a beta API, and thus subject to change at any point. It is not bound by the usual interface stability promises.
Note
This function combined with
psa_verify_hash_start()is equivalent topsa_verify_hash()but this function can return early and resume according to the limit set withpsa_interruptible_set_max_ops()to reduce the maximum time spent in a function call.Users should call this function on the same operation object repeatedly until it either returns 0 or an error. This function will return PSA_OPERATION_INCOMPLETE if there is more work to do. Alternatively users can call
psa_verify_hash_abort()at any point if they no longer want the result.When this function returns successfully, the operation becomes inactive. If this function returns an error status, the operation enters an error state and must be aborted by calling
psa_verify_hash_abort().
psa_verify_hash_abort#
psa_status_t psa_verify_hash_abort (psa_verify_hash_interruptible_operation_t * operation)
Abort a verify hash operation.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| psa_verify_hash_interruptible_operation_t * | [inout] | operation | Initialized verify hash operation. |
Warnings
This is a beta API, and thus subject to change at any point. It is not bound by the usual interface stability promises.
Note
This function is the only function that clears the number of ops completed as part of the operation. Please ensure you copy this value via
psa_verify_hash_get_num_ops()if required before calling.Aborting an operation frees all associated resources except for the operation structure itself. Once aborted, the operation object can be reused for another operation by calling
psa_verify_hash_start()again.You may call this function any time after the operation object has been initialized. In particular, calling
psa_verify_hash_abort()after the operation has already been terminated by a call topsa_verify_hash_abort()or psa_verify_hash_complete() is safe.