DCDC Initialization#
Initialize the DC-DC converter.
Configures the DC-DC converter. If the DC-DC converter is not to be used, the configuration option SL_DEVICE_INIT_DCDC_ENABLE
can be disabled, and the converter will be powered off. On Series 1 devices, this option should only be used when DVDD is externally powered.
To enable the bypass switch and short the DC-DC converter input to the DC-DC output, set the configuration option SL_DEVICE_INIT_DCDC_BYPASS
.
See AN0948 Power Configurations and DC-DC for further details about DC-DC converter configuration and operation.
Functions#
sl_status_t
sl_device_init_dcdc(void)
Initialize DCDC.
Function Documentation#
sl_device_init_dcdc#
sl_status_t sl_device_init_dcdc (void )
Initialize DCDC.
Parameters
N/A |
Configure and start the DCDC
Returns
Status code
Definition at line
77
of file platform/service/device_init/inc/sl_device_init_dcdc.h
Macro Definition Documentation#
SL_DEVICE_INIT_DCDC_TYPE_BUCK#
#define SL_DEVICE_INIT_DCDC_TYPE_BUCKValue:
0
DC/DC Converter Type.
Buck Type
Definition at line
65
of file platform/service/device_init/inc/sl_device_init_dcdc.h
SL_DEVICE_INIT_DCDC_TYPE_BOOST#
#define SL_DEVICE_INIT_DCDC_TYPE_BOOSTValue:
1
Boost Type.
Definition at line
66
of file platform/service/device_init/inc/sl_device_init_dcdc.h