You are viewing documentation for version:
Information about a memory error.
Public Attributes#
uint16_t
X coordinate of the address where the error happened.
uint16_t
Y coordinate of the address where the error happened.
uint8_t
The color that was written to the memory address.
uint8_t
The color that was read from the memory address.
Public Attribute Documentation#
uint16_t DMD_MemoryError::x
X coordinate of the address where the error happened.
uint16_t DMD_MemoryError::y
Y coordinate of the address where the error happened.
writtenColor#
uint8_t DMD_MemoryError::writtenColor[3]
The color that was written to the memory address.
readColor#
uint8_t DMD_MemoryError::readColor[3]
The color that was read from the memory address.