GPIO - General Purpose Input Output#

General Purpose Input Output peripheral.



Introduction#

This module contains functions to control the GPIO peripheral of Silicon Labs 32-bit MCUs and SoCs. The GPIO peripheral is used for interrupt configuration, pin configuration and direct pin manipulation as well as routing for peripheral pin connections.

Example#

The following example demonstrates the basic GPIO operations available in the Silicon Labs GPIO API. This example shows how to:

  • Define and configure a GPIO pin as an output

  • Control pin state (high, low, toggle)

  • Read the pin's input state

  • Configure and enable external interrupts

    This code can be used as a starting point for controlling LEDs, reading button inputs, or configuring interrupt-driven GPIO events in your application.

{
  // Enable bus clock for GPIO
  sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_GPIO);

  // Define GPIO pin
  sl_gpio_t led_pin = {
    .port = 0,  // Port A
    .pin = 0    // Pin 0
  };

  // Configure pin as push-pull output
  sl_hal_gpio_set_pin_mode(&led_pin, SL_GPIO_MODE_PUSH_PULL, false);

  // Set pin high
  sl_hal_gpio_set_pin(&led_pin);

  // Wait a moment
  for(volatile int i = 0; i < 100000; i++);

  // Clear pin (set low)
  sl_hal_gpio_clear_pin(&led_pin);

  // Toggle pin
  sl_hal_gpio_toggle_pin(&led_pin);

  // Read pin input
  bool pin_state = sl_hal_gpio_get_pin_input(&led_pin);

  // Configure external interrupt
  int32_t int_no = sl_hal_gpio_configure_external_interrupt(&led_pin,
                                                           SL_HAL_GPIO_INTERRUPT_UNAVAILABLE,
                                                           SL_GPIO_INTERRUPT_RISING_EDGE);

  // Enable interrupt
  sl_hal_gpio_enable_interrupts(1 << int_no);
}

Functions#

void
sl_hal_gpio_set_pin_mode(const sl_gpio_t *gpio, sl_gpio_mode_t mode, bool output_value)

Set the mode for a GPIO pin.

sl_gpio_mode_t
sl_hal_gpio_get_pin_mode(const sl_gpio_t *gpio)

Get the mode for a GPIO pin.

int32_t
sl_hal_gpio_configure_external_interrupt(const sl_gpio_t *gpio, int32_t int_no, sl_gpio_interrupt_flag_t flags)

Configure the GPIO external pin interrupt by connecting external interrupt id with gpio pin.

void
sl_hal_gpio_enable_pin_em4_wakeup(uint32_t pinmask, uint32_t polaritymask)

Enable GPIO pin wake-up from EM4.

int32_t
sl_hal_gpio_configure_wakeup_em4_external_interrupt(const sl_gpio_t *gpio, int32_t int_no, bool polarity)

Configure EM4WU pins as external level-sensitive interrupts.

void

Lock the GPIO configuration.

void

Unlock the GPIO configuration.

uint32_t

Gets the GPIO configuration state.

bool
sl_hal_gpio_is_gpio_port(sl_gpio_port_t port)
void
sl_hal_gpio_set_pin(const sl_gpio_t *gpio)

Set a single pin in GPIO data out register to 1.

void
sl_hal_gpio_set_port(sl_gpio_port_t port, uint32_t pins)

Set bits GPIO data out register to 1.

void
sl_hal_gpio_set_port_value(sl_gpio_port_t port, uint32_t val, uint32_t mask)

Set GPIO port data out register.

void
sl_hal_gpio_clear_pin(const sl_gpio_t *gpio)

Set a single pin in GPIO data out port register to 0.

void
sl_hal_gpio_clear_port(sl_gpio_port_t port, uint32_t pins)

Set bits in DOUT register for a port to 0.

bool
sl_hal_gpio_get_pin_input(const sl_gpio_t *gpio)

Read the pad value for a single pin in a GPIO port.

bool
sl_hal_gpio_get_pin_output(const sl_gpio_t *gpio)

Get current setting for a pin in a GPIO port data out register.

uint32_t
sl_hal_gpio_get_port_input(sl_gpio_port_t port)

Read the pad values for GPIO port.

uint32_t
sl_hal_gpio_get_port_output(sl_gpio_port_t port)

Get current setting for a GPIO port data out register.

void
sl_hal_gpio_toggle_pin(const sl_gpio_t *gpio)

Toggle a single pin in GPIO port data out register.

void
sl_hal_gpio_toggle_port(sl_gpio_port_t port, uint32_t pins)

Toggle pins in GPIO port data out register.

sl_status_t
sl_hal_gpio_set_slew_rate(const sl_gpio_t *gpio, uint8_t slewrate)

Set slewrate for pins on a GPIO port which are configured into normal modes.

sl_status_t
sl_hal_gpio_get_slew_rate(const sl_gpio_t *gpio, uint8_t *slewrate)

Get slewrate for pins on a GPIO port.

void
sl_hal_gpio_set_slew_rate_alternate(sl_gpio_port_t port, uint8_t slewrate_alt)

Set slewrate for pins on a GPIO port which are configured into alternate modes.

uint8_t

Get slewrate for pins on a GPIO port which are configured into alternate modes.

void

Enable one or more GPIO interrupts.

void

Disable one or more GPIO interrupts.

void

Clear one or more pending GPIO interrupts.

void

Set one or more pending GPIO interrupts from SW.

uint32_t

Get pending GPIO interrupts.

uint32_t

Get enabled GPIO interrupts.

uint32_t

Get enabled and pending GPIO interrupt flags.

int32_t
sl_hal_gpio_get_external_interrupt_number(uint8_t pin, uint32_t enabled_interrupts_mask)

The available external interrupt number getter.

int32_t

The available em4 wakeup interrupt number getter.

void

Disable GPIO pin wake-up from EM4.

void

Enable GPIO pin retention of output enable, output value, pull enable, and pull direction in EM4.

uint32_t

Check which GPIO pin(s) that caused a wake-up from EM4.

void

Enable/Disable serial wire output pin.

void

Enable/disable serial wire clock pin.

void

Enable/disable serial wire data I/O pin.

Macros#

#define

Define for port specific pin mask.

#define
#define
#define
#define

Define for port specific pin count.

#define
#define
#define
#define
#define
#define

Validation of port.

#define

Validation of port and pin.

#define

Number of external/EM4 interrupt lines for array sizing (0-15 = 16 elements)

#define

Maximum valid interrupt index for validation (highest valid index is 15)

#define
SL_HAL_GPIO_EM4WUEN_SHIFT _GPIO_EM4WUEN_EM4WUEN_SHIFT

Shift value for EM4WUEN.

#define
SL_HAL_GPIO_INT_IF_EVEN_MASK ((_GPIO_IF_MASK) & 0x55555555UL)

Masks for even and odd interrupt bits.

#define
SL_HAL_GPIO_INT_IF_ODD_MASK ((_GPIO_IF_MASK) & 0xAAAAAAAAUL)
#define

Validation of mode.

#define

Validation of interrupt number and pin.

Function Documentation#

sl_hal_gpio_set_pin_mode#

void sl_hal_gpio_set_pin_mode (const sl_gpio_t * gpio, sl_gpio_mode_t mode, bool output_value)

Set the mode for a GPIO pin.

Parameters
TypeDirectionArgument NameDescription
const sl_gpio_t *[in]gpio

Pointer to GPIO structure with port and pin

sl_gpio_mode_t[in]mode

The desired pin mode.

bool[in]output_value

A value to set for the pin in the DOUT register. The DOUT setting is important for some input mode configurations to determine the pull-up/down direction.


sl_hal_gpio_get_pin_mode#

sl_gpio_mode_t sl_hal_gpio_get_pin_mode (const sl_gpio_t * gpio)

Get the mode for a GPIO pin.

Parameters
TypeDirectionArgument NameDescription
const sl_gpio_t *[in]gpio

Pointer to GPIO structure with port and pin

Returns

  • Return the pin mode.


sl_hal_gpio_configure_external_interrupt#

int32_t sl_hal_gpio_configure_external_interrupt (const sl_gpio_t * gpio, int32_t int_no, sl_gpio_interrupt_flag_t flags)

Configure the GPIO external pin interrupt by connecting external interrupt id with gpio pin.

Parameters
TypeDirectionArgument NameDescription
const sl_gpio_t *[in]gpio

Pointer to GPIO structure with port and pin

int32_t[in]int_no

The interrupt number to trigger.

sl_gpio_interrupt_flag_t[in]flags

Interrupt configuration flags. sl_hal_gpio_interrupt_flag_t for more information.

Note

  • This function configure the pin interrupt with pin ,port and external interrupt id as input. If external interrupt id is provided as input it will be considered as the input or else available interrupt number will be generated by looping through the interrupt group and will be used. User can provide SL_HAL_GPIO_INTERRUPT_UNAVAILABLE if user don't want to provide interrupt id.

  • the pin number can be selected freely within a group. Interrupt numbers are divided into 4 groups (int_no / 4) and valid pin number within the interrupt groups are: 0: pins 0-3 (interrupt number 0-3) 1: pins 4-7 (interrupt number 4-7) 2: pins 8-11 (interrupt number 8-11) 3: pins 12-15 (interrupt number 12-15)

  • It is recommended to disable interrupts before configuring the GPIO pin interrupt. See sl_hal_gpio_disable_interrupts() for more information. The GPIO interrupt handler must be in place before enabling the interrupt. Notice that any pending interrupt for the selected interrupt is cleared by this function. Notice that only interrupt will be configured by this function. It is not enabled. It is recommended to enable interrupts after configuring the GPIO pin interrupt if needed. See sl_hal_gpio_enable_interrupts() for more information.

Returns

  • Return the available interrupt number


sl_hal_gpio_enable_pin_em4_wakeup#

void sl_hal_gpio_enable_pin_em4_wakeup (uint32_t pinmask, uint32_t polaritymask)

Enable GPIO pin wake-up from EM4.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]pinmask

A bitmask containing the bitwise logic OR of which GPIO pin(s) to enable.

uint32_t[in]polaritymask

A bitmask containing the bitwise logic OR of GPIO pin(s) wake-up polarity.

When the function exits, EM4 mode can be safely entered.

Note

  • It is assumed that the GPIO pin modes are set correctly. Valid modes are SL_GPIO_MODE_INPUT and SL_GPIO_MODE_INPUT_PULL.


sl_hal_gpio_configure_wakeup_em4_external_interrupt#

int32_t sl_hal_gpio_configure_wakeup_em4_external_interrupt (const sl_gpio_t * gpio, int32_t int_no, bool polarity)

Configure EM4WU pins as external level-sensitive interrupts.

Parameters
TypeDirectionArgument NameDescription
const sl_gpio_t *[in]gpio

Pointer to GPIO structure with port and pin

int32_t[in]int_no

The EM4WU interrupt number to trigger.

bool[in]polarity

true = Active high level-sensitive interrupt. false = Active low level-sensitive interrupt.

Note

  • It is recommended to disable interrupts before configuring the GPIO pin interrupt. See sl_hal_gpio_disable_interrupts() for more information. The provided port, pin and int_no inputs should be valid EM4 related parameters because there are dedicated port, pin and EM4 Wakeup interrupt combination for configuring the port, pin for EM4 functionality. User can provide SL_HAL_GPIO_INTERRUPT_UNAVAILABLE if user don't want to provide interrupt id. The GPIO interrupt handler must be in place before enabling the interrupt. Notice that any pending interrupt for the selected interrupt is cleared by this function. Notice that any only EM4WU interrupt is configured by this function. It is not enabled. It is recommended to enable interrupts after configuring the GPIO pin interrupt if needed. See sl_hal_gpio_enable_interrupts() for more information.

Returns

  • Return the available EM4WU interrupt number


sl_hal_gpio_lock#

void sl_hal_gpio_lock (void )

Lock the GPIO configuration.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • Configuration lock affects the GPIO_Px_MODEL, GPIO_Px_MODEH, GPIO_Px_CTRL, GPIO_Px_PINLOCKN, GPIO_EXTIPSELL, GPIO_EXTIPSELH, GPIO_EXTIPINSELL, GPIO_EXTIPINSELH, GPIO_INSENSE, GPIO_ROUTE, GPIO_ROUTEPEN, and GPIO_ROUTELOC0 registers when they are present on a specific device.

  • Unwanted or accidental changes to GPIO configuration can be avoided by using the configuration lock register. Any value other than 0xA534 written to GPIO_LOCK enables the configuration lock. Pins are unlocked by a reset or by writing 0xA534 to the GPIO_LOCK register.


sl_hal_gpio_unlock#

void sl_hal_gpio_unlock (void )

Unlock the GPIO configuration.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • Configuration lock affects the GPIO_Px_MODEL, GPIO_Px_MODEH, GPIO_Px_CTRL, GPIO_Px_PINLOCKN, GPIO_EXTIPSELL, GPIO_EXTIPSELH, GPIO_EXTIPINSELL, GPIO_EXTIPINSELH, GPIO_INSENSE, GPIO_ROUTE, GPIO_ROUTEPEN, and GPIO_ROUTELOC0 registers when they are present on a specific device.

  • Unwanted or accidental changes to GPIO configuration can be avoided by using the configuration lock register. Any value other than 0xA534 written to GPIO_LOCK enables the configuration lock. Pins are unlocked by a reset or by writing 0xA534 to the GPIO_LOCK register.


sl_hal_gpio_get_lock_status#

uint32_t sl_hal_gpio_get_lock_status (void )

Gets the GPIO configuration state.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Return the GPIO lock state.


sl_hal_gpio_is_gpio_port#

bool sl_hal_gpio_is_gpio_port (sl_gpio_port_t port)
Parameters
TypeDirectionArgument NameDescription
sl_gpio_port_tN/Aport

sl_hal_gpio_set_pin#

void sl_hal_gpio_set_pin (const sl_gpio_t * gpio)

Set a single pin in GPIO data out register to 1.

Parameters
TypeDirectionArgument NameDescription
const sl_gpio_t *[in]gpio

Pointer to GPIO structure with port and pin


sl_hal_gpio_set_port#

void sl_hal_gpio_set_port (sl_gpio_port_t port, uint32_t pins)

Set bits GPIO data out register to 1.

Parameters
TypeDirectionArgument NameDescription
sl_gpio_port_t[in]port

The GPIO port to access.

uint32_t[in]pins

Bit mask for bits to set to 1 in DOUT register.


sl_hal_gpio_set_port_value#

void sl_hal_gpio_set_port_value (sl_gpio_port_t port, uint32_t val, uint32_t mask)

Set GPIO port data out register.

Parameters
TypeDirectionArgument NameDescription
sl_gpio_port_t[in]port

The GPIO port to access.

uint32_t[in]val

Value to write to port data out register.

uint32_t[in]mask

Mask indicating which bits to modify.


sl_hal_gpio_clear_pin#

void sl_hal_gpio_clear_pin (const sl_gpio_t * gpio)

Set a single pin in GPIO data out port register to 0.

Parameters
TypeDirectionArgument NameDescription
const sl_gpio_t *[in]gpio

Pointer to GPIO structure with port and pin


sl_hal_gpio_clear_port#

void sl_hal_gpio_clear_port (sl_gpio_port_t port, uint32_t pins)

Set bits in DOUT register for a port to 0.

Parameters
TypeDirectionArgument NameDescription
sl_gpio_port_t[in]port

The GPIO port to access.

uint32_t[in]pins

Bit mask for bits to clear in DOUT register.


sl_hal_gpio_get_pin_input#

bool sl_hal_gpio_get_pin_input (const sl_gpio_t * gpio)

Read the pad value for a single pin in a GPIO port.

Parameters
TypeDirectionArgument NameDescription
const sl_gpio_t *[in]gpio

Pointer to GPIO structure with port and pin.

Returns

  • The pin value, 0 or 1.


sl_hal_gpio_get_pin_output#

bool sl_hal_gpio_get_pin_output (const sl_gpio_t * gpio)

Get current setting for a pin in a GPIO port data out register.

Parameters
TypeDirectionArgument NameDescription
const sl_gpio_t *[in]gpio

Pointer to GPIO structure with port and pin.

Returns

  • The DOUT setting for the requested pin, 0 or 1.


sl_hal_gpio_get_port_input#

uint32_t sl_hal_gpio_get_port_input (sl_gpio_port_t port)

Read the pad values for GPIO port.

Parameters
TypeDirectionArgument NameDescription
sl_gpio_port_t[in]port

The GPIO port to access.

Returns

  • The pad values for the GPIO port.


sl_hal_gpio_get_port_output#

uint32_t sl_hal_gpio_get_port_output (sl_gpio_port_t port)

Get current setting for a GPIO port data out register.

Parameters
TypeDirectionArgument NameDescription
sl_gpio_port_t[in]port

The GPIO port to access.

Returns

  • The data out setting for the requested port.


sl_hal_gpio_toggle_pin#

void sl_hal_gpio_toggle_pin (const sl_gpio_t * gpio)

Toggle a single pin in GPIO port data out register.

Parameters
TypeDirectionArgument NameDescription
const sl_gpio_t *[in]gpio

Pointer to GPIO structure with port and pin.


sl_hal_gpio_toggle_port#

void sl_hal_gpio_toggle_port (sl_gpio_port_t port, uint32_t pins)

Toggle pins in GPIO port data out register.

Parameters
TypeDirectionArgument NameDescription
sl_gpio_port_t[in]port

The GPIO port to access.

uint32_t[in]pins

Bit mask with pins to toggle.


sl_hal_gpio_set_slew_rate#

sl_status_t sl_hal_gpio_set_slew_rate (const sl_gpio_t * gpio, uint8_t slewrate)

Set slewrate for pins on a GPIO port which are configured into normal modes.

Parameters
TypeDirectionArgument NameDescription
const sl_gpio_t *[in]gpio

Pointer to GPIO structure with port and pin

uint8_t[in]slewrate

The slewrate to configure for pins on this GPIO port.

Note

    • This API supports both port-specific slew rate (one setting for the whole port) and per-pin slew rate (each pin in a port configured separately); which applies depends on the part.

Returns

  • SL_STATUS_OK if there's no error. SL_STATUS_INVALID_PARAMETER if port is invalid. SL_STATUS_NOT_SUPPORTED if the feature is not supported on this device or for the selected port.


sl_hal_gpio_get_slew_rate#

sl_status_t sl_hal_gpio_get_slew_rate (const sl_gpio_t * gpio, uint8_t * slewrate)

Get slewrate for pins on a GPIO port.

Parameters
TypeDirectionArgument NameDescription
const sl_gpio_t *[in]gpio

Pointer to GPIO structure with port and pin

uint8_t *[out]slewrate

Pointer to store the slewrate of selected GPIO port.

Note

    • This API supports both port-specific slew rate (one setting for the whole port) and per-pin slew rate (each pin in a port configured separately); which applies depends on the part.

Returns

  • SL_STATUS_OK if there's no error. SL_STATUS_INVALID_PARAMETER if port is invalid. SL_STATUS_NOT_SUPPORTED if the feature is not supported on this device or for the selected port.


sl_hal_gpio_set_slew_rate_alternate#

void sl_hal_gpio_set_slew_rate_alternate (sl_gpio_port_t port, uint8_t slewrate_alt)

Set slewrate for pins on a GPIO port which are configured into alternate modes.

Parameters
TypeDirectionArgument NameDescription
sl_gpio_port_t[in]port

The GPIO port to configure.

uint8_t[in]slewrate_alt

The slewrate to configure for pins using alternate modes on this GPIO port.


sl_hal_gpio_get_slew_rate_alternate#

uint8_t sl_hal_gpio_get_slew_rate_alternate (sl_gpio_port_t port)

Get slewrate for pins on a GPIO port which are configured into alternate modes.

Parameters
TypeDirectionArgument NameDescription
sl_gpio_port_t[in]port

The GPIO port to access to get slew rate.

Returns

  • Return the alternate slewrate setting for selected GPIO port.


sl_hal_gpio_enable_interrupts#

void sl_hal_gpio_enable_interrupts (uint32_t flags)

Enable one or more GPIO interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

GPIO interrupt sources to enable.


sl_hal_gpio_disable_interrupts#

void sl_hal_gpio_disable_interrupts (uint32_t flags)

Disable one or more GPIO interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

GPIO interrupt sources to disable.


sl_hal_gpio_clear_interrupts#

void sl_hal_gpio_clear_interrupts (uint32_t flags)

Clear one or more pending GPIO interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

Bitwise logic OR of GPIO interrupt sources to clear.


sl_hal_gpio_set_interrupts#

void sl_hal_gpio_set_interrupts (uint32_t flags)

Set one or more pending GPIO interrupts from SW.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

GPIO interrupt sources to set to pending.


sl_hal_gpio_get_pending_interrupts#

uint32_t sl_hal_gpio_get_pending_interrupts (void )

Get pending GPIO interrupts.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • GPIO interrupt sources pending.


sl_hal_gpio_get_enabled_interrupts#

uint32_t sl_hal_gpio_get_enabled_interrupts (void )

Get enabled GPIO interrupts.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Enabled GPIO interrupt sources.


sl_hal_gpio_get_enabled_pending_interrupts#

uint32_t sl_hal_gpio_get_enabled_pending_interrupts (void )

Get enabled and pending GPIO interrupt flags.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Enabled and pending interrupt sources.

Note

  • Useful for handling more interrupt sources in the same interrupt handler.


sl_hal_gpio_get_external_interrupt_number#

int32_t sl_hal_gpio_get_external_interrupt_number (uint8_t pin, uint32_t enabled_interrupts_mask)

The available external interrupt number getter.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]pin

The GPIO pin to access.

uint32_t[in]enabled_interrupts_mask

Contains enabled GPIO interrupts mask.

Returns

  • The available interrupt number based on interrupt and pin grouping.


sl_hal_gpio_get_em4_interrupt_number#

int32_t sl_hal_gpio_get_em4_interrupt_number (const sl_gpio_t * gpio)

The available em4 wakeup interrupt number getter.

Parameters
TypeDirectionArgument NameDescription
const sl_gpio_t *[in]gpio

Pointer to GPIO structure with port and pin.

Returns

  • The available em4 wakeup interrupt number based on associated port and pin.


sl_hal_gpio_disable_pin_em4_wakeup#

void sl_hal_gpio_disable_pin_em4_wakeup (uint32_t pinmask)

Disable GPIO pin wake-up from EM4.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]pinmask

Bit mask containing the bitwise logic OR of which GPIO pin(s) to disable.


sl_hal_gpio_set_pin_em4_retention#

void sl_hal_gpio_set_pin_em4_retention (bool enable)

Enable GPIO pin retention of output enable, output value, pull enable, and pull direction in EM4.

Parameters
TypeDirectionArgument NameDescription
bool[in]enable

true - enable EM4 pin retention. false - disable EM4 pin retention.

Note

  • The behavior of this function depends on the configured GPIO retention mode. If the GPIO retention mode is configured to be "SWUNLATCH" then this function will not change anything. If the retention mode is anything else then this function will set the GPIO retention mode to "EM4EXIT" when the enable argument is true, and "Disabled" when false.


sl_hal_gpio_get_pin_em4_wakeup_cause#

uint32_t sl_hal_gpio_get_pin_em4_wakeup_cause (void )

Check which GPIO pin(s) that caused a wake-up from EM4.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Bit mask containing the bitwise logic OR of which GPIO pin(s) caused the wake-up.


sl_hal_gpio_enable_debug_swo#

void sl_hal_gpio_enable_debug_swo (bool enable)

Enable/Disable serial wire output pin.

Parameters
TypeDirectionArgument NameDescription
bool[in]enable

false - disable serial wire viewer pin (default after reset). true - enable serial wire viewer pin.

Note

  • Enabling this pin is not sufficient to fully enable serial wire output, which is also dependent on issues outside the GPIO module.

  • If debug port is locked, SWO pin is not disabled automatically. To avoid information leakage through SWO, disable SWO pin after locking debug port.


sl_hal_gpio_enable_debug_swd_clk#

void sl_hal_gpio_enable_debug_swd_clk (bool enable)

Enable/disable serial wire clock pin.

Parameters
TypeDirectionArgument NameDescription
bool[in]enable

false - disable serial wire clock. true - enable serial wire clock (default after reset).

Note

  • Disabling SWDClk will disable the debug interface, which may result in a lockout if done early in startup (before debugger is able to halt core).


sl_hal_gpio_enable_debug_swd_io#

void sl_hal_gpio_enable_debug_swd_io (bool enable)

Enable/disable serial wire data I/O pin.

Parameters
TypeDirectionArgument NameDescription
bool[in]enable

false - disable serial wire data pin. true - enable serial wire data pin (default after reset).

Note

  • Disabling SWDClk will disable the debug interface, which may result in a lockout if done early in startup (before debugger is able to halt core).


Macro Definition Documentation#

SL_HAL_GPIO_PORT_A_PIN_MASK#

#define SL_HAL_GPIO_PORT_A_PIN_MASK
Value:
(GPIO_PA_MASK)

Define for port specific pin mask.


SL_HAL_GPIO_PORT_B_PIN_MASK#

#define SL_HAL_GPIO_PORT_B_PIN_MASK
Value:
(GPIO_PB_MASK)

SL_HAL_GPIO_PORT_C_PIN_MASK#

#define SL_HAL_GPIO_PORT_C_PIN_MASK
Value:
(GPIO_PC_MASK)

SL_HAL_GPIO_PORT_D_PIN_MASK#

#define SL_HAL_GPIO_PORT_D_PIN_MASK
Value:
(GPIO_PD_MASK)

SL_HAL_GPIO_PORT_E_PIN_MASK#

#define SL_HAL_GPIO_PORT_E_PIN_MASK
Value:
0

SL_HAL_GPIO_PORT_F_PIN_MASK#

#define SL_HAL_GPIO_PORT_F_PIN_MASK
Value:
0

SL_HAL_GPIO_PORT_G_PIN_MASK#

#define SL_HAL_GPIO_PORT_G_PIN_MASK
Value:
0

SL_HAL_GPIO_PORT_H_PIN_MASK#

#define SL_HAL_GPIO_PORT_H_PIN_MASK
Value:
0

SL_HAL_GPIO_PORT_I_PIN_MASK#

#define SL_HAL_GPIO_PORT_I_PIN_MASK
Value:
0

SL_HAL_GPIO_PORT_J_PIN_MASK#

#define SL_HAL_GPIO_PORT_J_PIN_MASK
Value:
0

SL_HAL_GPIO_PORT_K_PIN_MASK#

#define SL_HAL_GPIO_PORT_K_PIN_MASK
Value:
0

SL_HAL_GPIO_PORT_A_PIN_COUNT#

#define SL_HAL_GPIO_PORT_A_PIN_COUNT
Value:
(GPIO_PA_COUNT)

Define for port specific pin count.


SL_HAL_GPIO_PORT_B_PIN_COUNT#

#define SL_HAL_GPIO_PORT_B_PIN_COUNT
Value:
(GPIO_PB_COUNT)

SL_HAL_GPIO_PORT_C_PIN_COUNT#

#define SL_HAL_GPIO_PORT_C_PIN_COUNT
Value:
(GPIO_PC_COUNT)

SL_HAL_GPIO_PORT_D_PIN_COUNT#

#define SL_HAL_GPIO_PORT_D_PIN_COUNT
Value:
(GPIO_PD_COUNT)

SL_HAL_GPIO_PORT_E_PIN_COUNT#

#define SL_HAL_GPIO_PORT_E_PIN_COUNT
Value:
0

SL_HAL_GPIO_PORT_F_PIN_COUNT#

#define SL_HAL_GPIO_PORT_F_PIN_COUNT
Value:
0

SL_HAL_GPIO_PORT_G_PIN_COUNT#

#define SL_HAL_GPIO_PORT_G_PIN_COUNT
Value:
0

SL_HAL_GPIO_PORT_H_PIN_COUNT#

#define SL_HAL_GPIO_PORT_H_PIN_COUNT
Value:
0

SL_HAL_GPIO_PORT_I_PIN_COUNT#

#define SL_HAL_GPIO_PORT_I_PIN_COUNT
Value:
0

SL_HAL_GPIO_PORT_J_PIN_COUNT#

#define SL_HAL_GPIO_PORT_J_PIN_COUNT
Value:
0

SL_HAL_GPIO_PORT_K_PIN_COUNT#

#define SL_HAL_GPIO_PORT_K_PIN_COUNT
Value:
0

SL_HAL_GPIO_PORT_SIZE#

#define SL_HAL_GPIO_PORT_SIZE
Value:
( \
(port) == SL_GPIO_PORT_A ? SL_HAL_GPIO_PORT_A_PIN_COUNT \
: (port) == SL_GPIO_PORT_B ? SL_HAL_GPIO_PORT_B_PIN_COUNT \
: (port) == SL_GPIO_PORT_C ? SL_HAL_GPIO_PORT_C_PIN_COUNT \
: (port) == SL_GPIO_PORT_D ? SL_HAL_GPIO_PORT_D_PIN_COUNT \
: (port) == SL_GPIO_PORT_E ? SL_HAL_GPIO_PORT_E_PIN_COUNT \
: (port) == SL_GPIO_PORT_F ? SL_HAL_GPIO_PORT_F_PIN_COUNT \
: (port) == SL_GPIO_PORT_G ? SL_HAL_GPIO_PORT_G_PIN_COUNT \
: (port) == SL_GPIO_PORT_H ? SL_HAL_GPIO_PORT_H_PIN_COUNT \
: (port) == SL_GPIO_PORT_I ? SL_HAL_GPIO_PORT_I_PIN_COUNT \
: (port) == SL_GPIO_PORT_J ? SL_HAL_GPIO_PORT_J_PIN_COUNT \
: (port) == SL_GPIO_PORT_K ? SL_HAL_GPIO_PORT_K_PIN_COUNT \
: 0)

SL_HAL_GPIO_PORT_MASK#

#define SL_HAL_GPIO_PORT_MASK
Value:
( \
((int)port) == SL_GPIO_PORT_A ? SL_HAL_GPIO_PORT_A_PIN_MASK \
: ((int)port) == SL_GPIO_PORT_B ? SL_HAL_GPIO_PORT_B_PIN_MASK \
: ((int)port) == SL_GPIO_PORT_C ? SL_HAL_GPIO_PORT_C_PIN_MASK \
: ((int)port) == SL_GPIO_PORT_D ? SL_HAL_GPIO_PORT_D_PIN_MASK \
: ((int)port) == SL_GPIO_PORT_E ? SL_HAL_GPIO_PORT_E_PIN_MASK \
: ((int)port) == SL_GPIO_PORT_F ? SL_HAL_GPIO_PORT_F_PIN_MASK \
: ((int)port) == SL_GPIO_PORT_G ? SL_HAL_GPIO_PORT_G_PIN_MASK \
: ((int)port) == SL_GPIO_PORT_H ? SL_HAL_GPIO_PORT_H_PIN_MASK \
: ((int)port) == SL_GPIO_PORT_I ? SL_HAL_GPIO_PORT_I_PIN_MASK \
: ((int)port) == SL_GPIO_PORT_J ? SL_HAL_GPIO_PORT_J_PIN_MASK \
: ((int)port) == SL_GPIO_PORT_K ? SL_HAL_GPIO_PORT_K_PIN_MASK \
: 0UL)

SL_HAL_GPIO_PORT_IS_VALID#

#define SL_HAL_GPIO_PORT_IS_VALID
Value:
(port)

Validation of port.


SL_HAL_GPIO_PORT_PIN_IS_VALID#

#define SL_HAL_GPIO_PORT_PIN_IS_VALID
Value:
(port, pin)

Validation of port and pin.


SL_HAL_GPIO_NO_OF_EXT_INTERRUPTS#

#define SL_HAL_GPIO_NO_OF_EXT_INTERRUPTS
Value:
16

Number of external/EM4 interrupt lines for array sizing (0-15 = 16 elements)


SL_HAL_GPIO_INTERRUPT_MAX#

#define SL_HAL_GPIO_INTERRUPT_MAX
Value:
15

Maximum valid interrupt index for validation (highest valid index is 15)


SL_HAL_GPIO_EM4WUEN_SHIFT#

#define SL_HAL_GPIO_EM4WUEN_SHIFT
Value:
_GPIO_EM4WUEN_EM4WUEN_SHIFT

Shift value for EM4WUEN.


SL_HAL_GPIO_INT_IF_EVEN_MASK#

#define SL_HAL_GPIO_INT_IF_EVEN_MASK
Value:
((_GPIO_IF_MASK) & 0x55555555UL)

Masks for even and odd interrupt bits.


SL_HAL_GPIO_INT_IF_ODD_MASK#

#define SL_HAL_GPIO_INT_IF_ODD_MASK
Value:
((_GPIO_IF_MASK) & 0xAAAAAAAAUL)

SL_HAL_GPIO_MODE_IS_VALID#

#define SL_HAL_GPIO_MODE_IS_VALID
Value:
(mode)

Validation of mode.


SL_HAL_GPIO_INTNO_PIN_VALID#

#define SL_HAL_GPIO_INTNO_PIN_VALID
Value:
(int_no, pin)

Validation of interrupt number and pin.