WDOG - Watchdog Timer#

Watchdog timer peripheral API.


The Watchdog API functions provide full support for the WDOG peripheral. The WDOG resets the system in case of a fault condition.

Example#

The following example demonstrates how to configure and use the Watchdog Timer. This example shows how to initialize the watchdog with a custom configuration, enable interrupts, feed the watchdog, and properly clean up when done.

// WDOG warning interrupt handler
void WDOG0_IRQHandler(void)
{
  // Get pending interrupts
  uint32_t flags = sl_hal_wdog_get_pending_interrupts(WDOG0);

  // Check for warning interrupt
  if (flags & WDOG_IF_WARN) {
    // Clear the warning interrupt flag
    sl_hal_wdog_clear_interrupts(WDOG0, WDOG_IF_WARN);

    // Feed the watchdog before timeout occurs
    sl_hal_wdog_feed(WDOG0);

    // Application can perform other actions here
    // ...
  }
}

void wdog_example(void)
{
  // Enable bus clock for WDOG0
  sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_WDOG0);

  // Initialize WDOG with default configuration
  sl_hal_wdog_init_t init = SL_HAL_WDOG_INIT_DEFAULT;

  // Customize configuration
  init.period_select = SL_WDOG_PERIOD_64k;        // Set timeout period
  init.warning_time_select = SL_WDOG_WARNING_TIME75; // Get warning at 75% of timeout

  // Initialize WDOG with our configuration
  sl_hal_wdog_init(WDOG0, &init);

  // Enable warning interrupt
  sl_hal_wdog_clear_interrupts(WDOG0, WDOG_IF_WARN);
  sl_hal_wdog_enable_interrupts(WDOG0, WDOG_IF_WARN);

  // Enable NVIC interrupt for WDOG
  sl_interrupt_manager_clear_irq_pending(WDOG0_IRQn);
  sl_interrupt_manager_enable_irq(WDOG0_IRQn);

  // Enable WDOG - this starts the watchdog timer
  sl_hal_wdog_enable(WDOG0);

  // Verify WDOG is enabled (optional)
  if (sl_hal_wdog_is_enabled(WDOG0)) {
    // WDOG is now running

    // Feed the watchdog initially
    sl_hal_wdog_feed(WDOG0);

    // Wait for feed operation to complete
    sl_hal_wdog_wait_sync(WDOG0);

    // Main application loop would continue here
    // The watchdog will now trigger a warning interrupt at 75% of timeout
    // which will feed the watchdog in the interrupt handler
    // ...
  }

  // When no longer needed, disable the watchdog (if not locked)
  if (!sl_hal_wdog_is_locked(WDOG0)) {
    sl_hal_wdog_disable(WDOG0);
    sl_hal_wdog_wait_ready(WDOG0);

    // Disable NVIC interrupt for WDOG
    sl_interrupt_manager_disable_irq(WDOG0_IRQn);
  }
}

Modules#

sl_hal_wdog_init_t

Enumerations#

enum
SL_WDOG_PERIOD_9 = _WDOG_CFG_PERSEL_SEL0
SL_WDOG_PERIOD_17 = _WDOG_CFG_PERSEL_SEL1
SL_WDOG_PERIOD_33 = _WDOG_CFG_PERSEL_SEL2
SL_WDOG_PERIOD_65 = _WDOG_CFG_PERSEL_SEL3
SL_WDOG_PERIOD_129 = _WDOG_CFG_PERSEL_SEL4
SL_WDOG_PERIOD_257 = _WDOG_CFG_PERSEL_SEL5
SL_WDOG_PERIOD_513 = _WDOG_CFG_PERSEL_SEL6
SL_WDOG_PERIOD_1k = _WDOG_CFG_PERSEL_SEL7
SL_WDOG_PERIOD_2k = _WDOG_CFG_PERSEL_SEL8
SL_WDOG_PERIOD_4k = _WDOG_CFG_PERSEL_SEL9
SL_WDOG_PERIOD_8k = _WDOG_CFG_PERSEL_SEL10
SL_WDOG_PERIOD_16k = _WDOG_CFG_PERSEL_SEL11
SL_WDOG_PERIOD_32k = _WDOG_CFG_PERSEL_SEL12
SL_WDOG_PERIOD_64k = _WDOG_CFG_PERSEL_SEL13
SL_WDOG_PERIOD_128k = _WDOG_CFG_PERSEL_SEL14
SL_WDOG_PERIOD_256k = _WDOG_CFG_PERSEL_SEL15
}

Watchdog timeout period selection.

enum
SL_WDOG_WARNING_DISABLE = _WDOG_CFG_WARNSEL_DIS
SL_WDOG_WARNING_TIME25 = _WDOG_CFG_WARNSEL_SEL1
SL_WDOG_WARNING_TIME50 = _WDOG_CFG_WARNSEL_SEL2
SL_WDOG_WARNING_TIME75 = _WDOG_CFG_WARNSEL_SEL3
}

Select Watchdog warning timeout period as percentage of timeout.

enum
SL_WDOG_ILLEGAL_WINDOW_DISABLE = _WDOG_CFG_WINSEL_DIS
SL_WDOG_ILLEGAL_WINDOW_TIME12_5 = _WDOG_CFG_WINSEL_SEL1
SL_WDOG_ILLEGAL_WINDOW_TIME25_0 = _WDOG_CFG_WINSEL_SEL2
SL_WDOG_ILLEGAL_WINDOW_TIME37_5 = _WDOG_CFG_WINSEL_SEL3
SL_WDOG_ILLEGAL_WINDOW_TIME50_0 = _WDOG_CFG_WINSEL_SEL4
SL_WDOG_ILLEGAL_WINDOW_TIME62_5 = _WDOG_CFG_WINSEL_SEL5
SL_WDOG_ILLEGAL_WINDOW_TIME75_0 = _WDOG_CFG_WINSEL_SEL6
SL_WDOG_ILLEGAL_WINDOW_TIME87_5 = _WDOG_CFG_WINSEL_SEL7
}

Select Watchdog illegal window limit.

Functions#

void
sl_hal_wdog_enable(WDOG_TypeDef *wdog)

Enable the watchdog peripheral.

void
sl_hal_wdog_disable(WDOG_TypeDef *wdog)

Disable the watchdog peripheral.

void
sl_hal_wdog_feed(WDOG_TypeDef *wdog)

Feed the watchdog peripheral.

void
sl_hal_wdog_init(WDOG_TypeDef *wdog, const sl_hal_wdog_init_t *init)

Initialize watchdog (assuming the watchdog configuration has not been locked).

void
sl_hal_wdog_lock(WDOG_TypeDef *wdog)

Lock the watchdog configuration.

void
sl_hal_wdog_wait_sync(WDOG_TypeDef *wdog)

Wait for the watchdog to complete all synchronization of register changes and commands.

void
sl_hal_wdog_wait_ready(WDOG_TypeDef *wdog)

Wait for the watchdog to be completely disabled after calling sl_hal_wdog_disable().

void
sl_hal_wdog_unlock(WDOG_TypeDef *wdog)

Unlock the watchdog configuration.

void
sl_hal_wdog_clear_interrupts(WDOG_TypeDef *wdog, uint32_t flags)

Clear one or more pending watchdog interrupts.

void
sl_hal_wdog_disable_interrupts(WDOG_TypeDef *wdog, uint32_t flags)

Disable one or more watchdog interrupts.

void
sl_hal_wdog_enable_interrupts(WDOG_TypeDef *wdog, uint32_t flags)

Enable one or more watchdog interrupts.

uint32_t

Get pending watchdog interrupt flags.

uint32_t

Get enabled and pending watchdog interrupt flags.

void
sl_hal_wdog_set_interrupts(WDOG_TypeDef *wdog, uint32_t flags)

Set one or more pending watchdog interrupts from SW.

bool
sl_hal_wdog_is_enabled(WDOG_TypeDef *wdog)

Get enabled status of the watchdog.

bool
sl_hal_wdog_is_locked(WDOG_TypeDef *wdog)

Get locked status of the watchdog.

Macros#

#define

Check if WDOG instance is valid.

#define

Suggested default configuration for WDOG initialization structure.

Enumeration Documentation#

sl_hal_wdog_period_select_t#

sl_hal_wdog_period_select_t

Watchdog timeout period selection.

Enumerator
SL_WDOG_PERIOD_9

9 clock periods.

SL_WDOG_PERIOD_17

17 clock periods.

SL_WDOG_PERIOD_33

33 clock periods.

SL_WDOG_PERIOD_65

65 clock periods.

SL_WDOG_PERIOD_129

129 clock periods.

SL_WDOG_PERIOD_257

257 clock periods.

SL_WDOG_PERIOD_513

513 clock periods.

SL_WDOG_PERIOD_1k

1025 clock periods.

SL_WDOG_PERIOD_2k

2049 clock periods.

SL_WDOG_PERIOD_4k

4097 clock periods.

SL_WDOG_PERIOD_8k

8193 clock periods.

SL_WDOG_PERIOD_16k

16385 clock periods.

SL_WDOG_PERIOD_32k

32769 clock periods.

SL_WDOG_PERIOD_64k

65537 clock periods.

SL_WDOG_PERIOD_128k

131073 clock periods.

SL_WDOG_PERIOD_256k

262145 clock periods.


sl_hal_wdog_warning_timeout_select_t#

sl_hal_wdog_warning_timeout_select_t

Select Watchdog warning timeout period as percentage of timeout.

Enumerator
SL_WDOG_WARNING_DISABLE

Watchdog warning period is disabled.

SL_WDOG_WARNING_TIME25

Watchdog warning period is 25% of the timeout.

SL_WDOG_WARNING_TIME50

Watchdog warning period is 50% of the timeout.

SL_WDOG_WARNING_TIME75

Watchdog warning period is 75% of the timeout.


sl_hal_wdog_illegal_window_select_t#

sl_hal_wdog_illegal_window_select_t

Select Watchdog illegal window limit.

Enumerator
SL_WDOG_ILLEGAL_WINDOW_DISABLE

Watchdog illegal window disabled.

SL_WDOG_ILLEGAL_WINDOW_TIME12_5

Window timeout is 12.5% of the timeout.

SL_WDOG_ILLEGAL_WINDOW_TIME25_0

Window timeout is 25% of the timeout.

SL_WDOG_ILLEGAL_WINDOW_TIME37_5

Window timeout is 37.5% of the timeout.

SL_WDOG_ILLEGAL_WINDOW_TIME50_0

Window timeout is 50% of the timeout.

SL_WDOG_ILLEGAL_WINDOW_TIME62_5

Window timeout is 62.5% of the timeout.

SL_WDOG_ILLEGAL_WINDOW_TIME75_0

Window timeout is 75% of the timeout.

SL_WDOG_ILLEGAL_WINDOW_TIME87_5

Window timeout is 87.5% of the timeout.


Function Documentation#

sl_hal_wdog_enable#

void sl_hal_wdog_enable (WDOG_TypeDef * wdog)

Enable the watchdog peripheral.

Parameters
TypeDirectionArgument NameDescription
WDOG_TypeDef *[in]wdog

Pointer to the WDOG peripheral register block.

Note

  • This function modifies the WDOG CTRL register which requires synchronization into the low-frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed.


sl_hal_wdog_disable#

void sl_hal_wdog_disable (WDOG_TypeDef * wdog)

Disable the watchdog peripheral.

Parameters
TypeDirectionArgument NameDescription
WDOG_TypeDef *[in]wdog

Pointer to the WDOG peripheral register block.

Note

  • This function modifies the WDOG CTRL register which requires synchronization into the low-frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed.


sl_hal_wdog_feed#

void sl_hal_wdog_feed (WDOG_TypeDef * wdog)

Feed the watchdog peripheral.

Parameters
TypeDirectionArgument NameDescription
WDOG_TypeDef *[in]wdog

Pointer to the WDOG peripheral register block.

When WDOG is activated, it must be fed (i.e., clearing the counter) before it reaches the defined timeout period. Otherwise, WDOG will generate a reset.

Note

  • Note that WDOG is an asynchronous peripheral and when calling the sl_hal_wdog_feed() function the hardware starts the process of clearing the counter. This process takes some time before it completes depending on the selected oscillator (up to 4 peripheral clock cycles). When using the ULFRCO for instance as the oscillator the watchdog runs on a 1 kHz clock and a watchdog clear operation might take up to 4 ms.

If the device supports EM2 or EM3 and it enters EM2 or EM3 while a command is in progress then that command will be aborted. An application can use sl_hal_wdog_sync_wait() to wait for a command to complete.


sl_hal_wdog_init#

void sl_hal_wdog_init (WDOG_TypeDef * wdog, const sl_hal_wdog_init_t * init)

Initialize watchdog (assuming the watchdog configuration has not been locked).

Parameters
TypeDirectionArgument NameDescription
WDOG_TypeDef *[in]wdog

Pointer to the WDOG peripheral register block.

const sl_hal_wdog_init_t *[in]init

The structure holding the WDOG configuration. A default setting #WDOG_INIT_DEFAULT is available for initialization.

Note

  • This function modifies the WDOG CTRL register which requires synchronization into the low-frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed.


sl_hal_wdog_lock#

void sl_hal_wdog_lock (WDOG_TypeDef * wdog)

Lock the watchdog configuration.

Parameters
TypeDirectionArgument NameDescription
WDOG_TypeDef *[in]wdog

Pointer to WDOG peripheral register block.

This prevents errors from overwriting the WDOG configuration, possibly disabling it. Only a reset can unlock the WDOG configuration once locked.

If the LFRCO or LFXO clocks are used to clock WDOG, consider using the option of inhibiting those clocks to be disabled. See the #WDOG_INIT_DEFAULT initialization structure.

Note

  • This function modifies the WDOG CTRL register which requires synchronization into the low-frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed.


sl_hal_wdog_wait_sync#

void sl_hal_wdog_wait_sync (WDOG_TypeDef * wdog)

Wait for the watchdog to complete all synchronization of register changes and commands.

Parameters
TypeDirectionArgument NameDescription
WDOG_TypeDef *[in]wdog

Pointer to WDOG peripheral register block.


sl_hal_wdog_wait_ready#

void sl_hal_wdog_wait_ready (WDOG_TypeDef * wdog)

Wait for the watchdog to be completely disabled after calling sl_hal_wdog_disable().

Parameters
TypeDirectionArgument NameDescription
WDOG_TypeDef *[in]wdog

Pointer to WDOG peripheral register block.


sl_hal_wdog_unlock#

void sl_hal_wdog_unlock (WDOG_TypeDef * wdog)

Unlock the watchdog configuration.

Parameters
TypeDirectionArgument NameDescription
WDOG_TypeDef *[in]wdog

Pointer to WDOG peripheral register block.

Note that this function will have no effect on devices where a reset is the only way to unlock the watchdog.


sl_hal_wdog_clear_interrupts#

void sl_hal_wdog_clear_interrupts (WDOG_TypeDef * wdog, uint32_t flags)

Clear one or more pending watchdog interrupts.

Parameters
TypeDirectionArgument NameDescription
WDOG_TypeDef *[in]wdog

Pointer to the WDOG peripheral register block.

uint32_t[in]flags

WDOG interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources.


sl_hal_wdog_disable_interrupts#

void sl_hal_wdog_disable_interrupts (WDOG_TypeDef * wdog, uint32_t flags)

Disable one or more watchdog interrupts.

Parameters
TypeDirectionArgument NameDescription
WDOG_TypeDef *[in]wdog

Pointer to the WDOG peripheral register block.

uint32_t[in]flags

WDOG interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt.


sl_hal_wdog_enable_interrupts#

void sl_hal_wdog_enable_interrupts (WDOG_TypeDef * wdog, uint32_t flags)

Enable one or more watchdog interrupts.

Parameters
TypeDirectionArgument NameDescription
WDOG_TypeDef *[in]wdog

Pointer to the WDOG peripheral register block.

uint32_t[in]flags

WDOG interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt.

Note

  • Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using sl_hal_wdog_clear_interrupts() prior to enabling the interrupt.


sl_hal_wdog_get_pending_interrupts#

uint32_t sl_hal_wdog_get_pending_interrupts (WDOG_TypeDef * wdog)

Get pending watchdog interrupt flags.

Parameters
TypeDirectionArgument NameDescription
WDOG_TypeDef *[in]wdog

Pointer to the WDOG peripheral register block.

Returns

  • Pending WDOG interrupt sources. Returns a set of interrupt flags OR-ed together for the interrupt sources set.

Note

  • The event bits are not cleared by the use of this function.


sl_hal_wdog_get_enabled_pending_interrupts#

uint32_t sl_hal_wdog_get_enabled_pending_interrupts (WDOG_TypeDef * wdog)

Get enabled and pending watchdog interrupt flags.

Parameters
TypeDirectionArgument NameDescription
WDOG_TypeDef *[in]wdog

Pointer to the WDOG peripheral register block.

Returns

  • Pending and enabled WDOG interrupt sources. Returns a set of interrupt flags OR-ed together for the interrupt sources set.

Useful for handling more interrupt sources in the same interrupt handler.


sl_hal_wdog_set_interrupts#

void sl_hal_wdog_set_interrupts (WDOG_TypeDef * wdog, uint32_t flags)

Set one or more pending watchdog interrupts from SW.

Parameters
TypeDirectionArgument NameDescription
WDOG_TypeDef *[in]wdog

Pointer to the WDOG peripheral register block.

uint32_t[in]flags

WDOG interrupt sources to set to pending. Use a set of interrupt flags (WDOG_IFS_nnn).


sl_hal_wdog_is_enabled#

bool sl_hal_wdog_is_enabled (WDOG_TypeDef * wdog)

Get enabled status of the watchdog.

Parameters
TypeDirectionArgument NameDescription
WDOG_TypeDef *[in]wdog

Pointer to the WDOG peripheral register block.

Returns

  • True if Watchdog is enabled, false otherwise.


sl_hal_wdog_is_locked#

bool sl_hal_wdog_is_locked (WDOG_TypeDef * wdog)

Get locked status of the watchdog.

Parameters
TypeDirectionArgument NameDescription
WDOG_TypeDef *[in]wdog

Pointer to the WDOG peripheral register block.

Returns

  • True if Watchdog is locked, false otherwise.


Macro Definition Documentation#

SL_HAL_WDOG_REF_VALID#

#define SL_HAL_WDOG_REF_VALID
Value:
(ref)

Check if WDOG instance is valid.


SL_HAL_WDOG_INIT_DEFAULT#

#define SL_HAL_WDOG_INIT_DEFAULT
Value:
{ \
false, /* WDOG is not counting during debug halt. */ \
false, /* The clear bit will clear the WDOG counter. */ \
false, /* WDOG is not counting when in EM1. */ \
false, /* WDOG is not counting when in EM2. */ \
false, /* WDOG is not counting when in EM3. */ \
false, /* EM4 can be entered. */ \
false, /* PRS Source 0 missing event will not trigger a WDOG reset. */ \
false, /* PRS Source 1 missing event will not trigger a WDOG reset. */ \
false, /* Do not lock WDOG configuration. */ \
SL_WDOG_PERIOD_256k, /* Set longest possible timeout period. */ \
SL_WDOG_WARNING_DISABLE, /* Disable warning interrupt. */ \
SL_WDOG_ILLEGAL_WINDOW_DISABLE, /* Disable illegal window interrupt. */ \
false /* Do not disable reset. */ \
}

Suggested default configuration for WDOG initialization structure.