VDAC - Digital to Analog Voltage Converter.#

Digital to Analog Voltage Converter (VDAC) Peripheral API.

This module contains functions to control the VDAC peripheral of Silicon Labs' 32-bit MCUs and SoCs. VDAC converts digital values to analog signals at up to 500 ksps with 12-bit accuracy. VDAC is designed for low energy consumption, but can also provide very good performance.

The following steps are necessary for basic operation:

Clock enable:

sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_VDAC0);

Initialize the VDAC with default settings and modify selected fields:

sl_hal_vdac_init_t vdac_init                 = SL_HAL_VDAC_INIT_DEFAULT;
sl_hal_vdac_init_channel_t vdac_channel_init = SL_HAL_VDAC_CHANNEL_INIT_DEFAULT;

Set prescaler to get 1 MHz VDAC clock frequency. Calculate clock frequency used for VDAC.

sl_clock_branch_t clock_branch;
uint32_t src_clk_freq;
clock_branch = sl_device_peripheral_get_clock_branch(SL_PERIPHERAL_VDAC0);

sl_clock_manager_get_clock_branch_frequency(clock_branch, &src_clk_freq);
vdac_init.prescaler = sl_hal_vdac_calculate_prescaler(VDAC0, 1000000, src_clk_freq);

sl_hal_vdac_init(VDAC0, &vdac_init);
sl_hal_vdac_init_channel(VDAC0, &vdac_channel_init, 0);
sl_hal_vdac_enable_channel(VDAC0, 0);

Perform a conversion:

sl_hal_vdac_set_output_channel(VDAC0, 0, 250);

Modules#

sl_hal_vdac_init_t

sl_hal_vdac_init_channel_t

Enumerations#

enum
SL_HAL_VDAC_CHANNEL_0 = 0
SL_HAL_VDAC_CHANNEL_1 = 1
}

VDAC channel.

enum
SL_HAL_VDAC_REFRESH_CYCLES_2 = _VDAC_CFG_REFRESHPERIOD_CYCLES2
SL_HAL_VDAC_REFRESH_CYCLES_4 = _VDAC_CFG_REFRESHPERIOD_CYCLES4
SL_HAL_VDAC_REFRESH_CYCLES_8 = _VDAC_CFG_REFRESHPERIOD_CYCLES8
SL_HAL_VDAC_REFRESH_CYCLES_16 = _VDAC_CFG_REFRESHPERIOD_CYCLES16
SL_HAL_VDAC_REFRESH_CYCLES_32 = _VDAC_CFG_REFRESHPERIOD_CYCLES32
SL_HAL_VDAC_REFRESH_CYCLES_64 = _VDAC_CFG_REFRESHPERIOD_CYCLES64
SL_HAL_VDAC_REFRESH_CYCLES_128 = _VDAC_CFG_REFRESHPERIOD_CYCLES128
SL_HAL_VDAC_REFRESH_CYCLES_256 = _VDAC_CFG_REFRESHPERIOD_CYCLES256
}

Channel refresh period.

enum
SL_HAL_VDAC_OVERFLOW_CYCLE_2 = _VDAC_CFG_TIMEROVRFLOWPERIOD_CYCLES2
SL_HAL_VDAC_OVERFLOW_CYCLE_4 = _VDAC_CFG_TIMEROVRFLOWPERIOD_CYCLES4
SL_HAL_VDAC_OVERFLOW_CYCLE_8 = _VDAC_CFG_TIMEROVRFLOWPERIOD_CYCLES8
SL_HAL_VDAC_OVERFLOW_CYCLE_16 = _VDAC_CFG_TIMEROVRFLOWPERIOD_CYCLES16
SL_HAL_VDAC_OVERFLOW_CYCLE_32 = _VDAC_CFG_TIMEROVRFLOWPERIOD_CYCLES32
SL_HAL_VDAC_OVERFLOW_CYCLE_64 = _VDAC_CFG_TIMEROVRFLOWPERIOD_CYCLES64
}

Timer overflow period.

enum
SL_HAL_VDAC_VREF_1V25 = _VDAC_CFG_REFRSEL_V125
SL_HAL_VDAC_VREF_2V5 = _VDAC_CFG_REFRSEL_V25
SL_HAL_VDAC_VREF_AVDD = _VDAC_CFG_REFRSEL_VDD
SL_HAL_VDAC_VREF_EXTERNAL_PIN = _VDAC_CFG_REFRSEL_EXT
}

Reference voltage for VDAC.

enum
SL_HAL_VDAC_REFRESH_NONE = _VDAC_CH0CFG_REFRESHSOURCE_NONE
SL_HAL_VDAC_REFRESH_SOURCE_TIMER = _VDAC_CH0CFG_REFRESHSOURCE_REFRESHTIMER
SL_HAL_VDAC_REFRESH_SYNC_PRS = _VDAC_CH0CFG_REFRESHSOURCE_SYNCPRS
SL_HAL_VDAC_REFRESH_ASYNC_PRS = _VDAC_CH0CFG_REFRESHSOURCE_ASYNCPRS
}

Refresh source for VDAC.

enum
SL_HAL_VDAC_TRIGGER_MODE_NONE = _VDAC_CH0CFG_TRIGMODE_NONE
SL_HAL_VDAC_TRIGGER_MODE_SW = _VDAC_CH0CFG_TRIGMODE_SW
SL_HAL_VDAC_TRIGGER_MODE_SYNC_PRS = _VDAC_CH0CFG_TRIGMODE_SYNCPRS
SL_HAL_VDAC_TRIGGER_MODE_LESENSE = _VDAC_CH0CFG_TRIGMODE_LESENSE
SL_HAL_VDAC_TRIGGER_MODE_INTERNAL_TIMER = _VDAC_CH0CFG_TRIGMODE_INTERNALTIMER
SL_HAL_VDAC_TRIGGER_MODE_ASYNC_PRS = _VDAC_CH0CFG_TRIGMODE_ASYNCPRS
}

Channel conversion trigger mode.

enum
SL_HAL_VDAC_POWER_MODE_HIGH_POWER = _VDAC_CH0CFG_POWERMODE_HIGHPOWER
SL_HAL_VDAC_POWER_MODE_LOW_POWER = _VDAC_CH0CFG_POWERMODE_LOWPOWER
}

Channel power mode.

enum
SL_HAL_VDAC_PORT_NONE = _VDAC_OUTCTRL_ABUSPORTSELCH0_NONE
SL_HAL_VDAC_PORT_A = _VDAC_OUTCTRL_ABUSPORTSELCH0_PORTA
SL_HAL_VDAC_PORT_B = _VDAC_OUTCTRL_ABUSPORTSELCH0_PORTB
SL_HAL_VDAC_PORT_C = _VDAC_OUTCTRL_ABUSPORTSELCH0_PORTC
SL_HAL_VDAC_PORT_D = _VDAC_OUTCTRL_ABUSPORTSELCH0_PORTD
}

VDAC channel Abus port selection.

Functions#

void
sl_hal_vdac_init(VDAC_TypeDef *vdac, const sl_hal_vdac_init_t *init)

Initialize VDAC.

void
sl_hal_vdac_init_channel(VDAC_TypeDef *vdac, const sl_hal_vdac_init_channel_t *init, uint32_t channel)

Initialize a VDAC channel.

void
sl_hal_vdac_enable_channel(VDAC_TypeDef *vdac, uint32_t channel)

Enable the VDAC channel.

void
sl_hal_vdac_disable_channel(VDAC_TypeDef *vdac, uint32_t channel)

Disable the VDAC channel.

void
sl_hal_vdac_set_output_channel(VDAC_TypeDef *vdac, uint32_t channel, uint32_t value)

Set the output signal of a VDAC channel to a given value.

uint32_t
sl_hal_vdac_calculate_prescaler(VDAC_TypeDef *vdac, uint32_t vdac_frequency, uint32_t reference_frequency)

Calculate the prescaler value used to determine VDAC clock.

void
sl_hal_vdac_reset(VDAC_TypeDef *vdac)

Reset VDAC to its default state.

void
sl_hal_vdac_wait_sync(VDAC_TypeDef *vdac)

Wait for the vdac to complete all synchronization of register changes and commands.

void
sl_hal_vdac_wait_ready(VDAC_TypeDef *vdac)

Wait for the vdac to be completely disabled.

void
sl_hal_vdac_enable(VDAC_TypeDef *vdac)

Enables the VDAC module.

void
sl_hal_vdac_disable(VDAC_TypeDef *vdac)

Disables the VDAC module and ensures all operations are synchronized.

void
sl_hal_vdac_enable_interrupts(VDAC_TypeDef *vdac, uint32_t flags)

Enable one or more VDAC interrupts.

void
sl_hal_vdac_disable_interrupts(VDAC_TypeDef *vdac, uint32_t flags)

Disable one or more VDAC interrupts.

void
sl_hal_vdac_set_interrupts(VDAC_TypeDef *vdac, uint32_t flags)

Set one or more pending VDAC interrupts from SW.

void
sl_hal_vdac_clear_interrupts(VDAC_TypeDef *vdac, uint32_t flags)

Clear one or more pending VDAC interrupts.

uint32_t

Get pending VDAC interrupt flags.

uint32_t

Get enabled and pending VDAC interrupt flags.

void
sl_hal_vdac_sine_mode_start(VDAC_TypeDef *vdac)

Start Sine mode.

void
sl_hal_vdac_sine_mode_stop(VDAC_TypeDef *vdac)

Stop Sine mode.

uint32_t
sl_hal_vdac_get_status(VDAC_TypeDef *vdac)

Get the VDAC Status register.

Macros#

#define

VDAC instance validation.

#define

Default configuration for VDAC initialization structure.

#define

Sine mode configuration for VDAC initialization structure.

#define

Default configuration for VDAC channel initialization structure.

Enumeration Documentation#

sl_hal_vdac_channel_t#

sl_hal_vdac_channel_t

VDAC channel.

Enumerator
SL_HAL_VDAC_CHANNEL_0

Channel 0 of VDAC.

SL_HAL_VDAC_CHANNEL_1

Channel 1 of VDAC.


sl_hal_vdac_refresh_t#

sl_hal_vdac_refresh_t

Channel refresh period.

Enumerator
SL_HAL_VDAC_REFRESH_CYCLES_2

Refresh every 2 clock cycles.

SL_HAL_VDAC_REFRESH_CYCLES_4

Refresh every 4 clock cycles.

SL_HAL_VDAC_REFRESH_CYCLES_8

Refresh every 8 clock cycles.

SL_HAL_VDAC_REFRESH_CYCLES_16

Refresh every 16 clock cycles.

SL_HAL_VDAC_REFRESH_CYCLES_32

Refresh every 32 clock cycles.

SL_HAL_VDAC_REFRESH_CYCLES_64

Refresh every 64 clock cycles.

SL_HAL_VDAC_REFRESH_CYCLES_128

Refresh every 128 clock cycles.

SL_HAL_VDAC_REFRESH_CYCLES_256

Refresh every 256 clock cycles.


sl_hal_vdac_timer_overflow_period_t#

sl_hal_vdac_timer_overflow_period_t

Timer overflow period.

Enumerator
SL_HAL_VDAC_OVERFLOW_CYCLE_2

Overflows every 2 clock cycles.

SL_HAL_VDAC_OVERFLOW_CYCLE_4

Overflows every 4 clock cycles.

SL_HAL_VDAC_OVERFLOW_CYCLE_8

Overflows every 8 clock cycles.

SL_HAL_VDAC_OVERFLOW_CYCLE_16

Overflows every 16 clock cycles.

SL_HAL_VDAC_OVERFLOW_CYCLE_32

Overflows every 32 clock cycles.

SL_HAL_VDAC_OVERFLOW_CYCLE_64

Overflows every 64 clock cycles.


sl_hal_vdac_vref_t#

sl_hal_vdac_vref_t

Reference voltage for VDAC.

Enumerator
SL_HAL_VDAC_VREF_1V25

Internal 1.25 V band gap reference.

SL_HAL_VDAC_VREF_2V5

Internal 2.5 V band gap reference.

SL_HAL_VDAC_VREF_AVDD

AVDD reference.

SL_HAL_VDAC_VREF_EXTERNAL_PIN

External pin reference.


sl_hal_vdac_refresh_source_t#

sl_hal_vdac_refresh_source_t

Refresh source for VDAC.

Enumerator
SL_HAL_VDAC_REFRESH_NONE

No refresh source.

SL_HAL_VDAC_REFRESH_SOURCE_TIMER

Refresh triggered by refresh timer overflow.

SL_HAL_VDAC_REFRESH_SYNC_PRS

Refresh triggered by sync PRS.

SL_HAL_VDAC_REFRESH_ASYNC_PRS

Refresh triggered by async PRS.


sl_hal_vdac_trigger_mode_t#

sl_hal_vdac_trigger_mode_t

Channel conversion trigger mode.

Enumerator
SL_HAL_VDAC_TRIGGER_MODE_NONE

No conversion trigger source selected.

SL_HAL_VDAC_TRIGGER_MODE_SW

Channel is triggered by CHnDATA or COMBDATA write.

SL_HAL_VDAC_TRIGGER_MODE_SYNC_PRS

Channel is triggered by Sync PRS input.

SL_HAL_VDAC_TRIGGER_MODE_LESENSE

Channel is triggered by LESENSE.

SL_HAL_VDAC_TRIGGER_MODE_INTERNAL_TIMER

Channel is triggered by Internal Timer.

SL_HAL_VDAC_TRIGGER_MODE_ASYNC_PRS

Channel is triggered by Async PRS input.


sl_hal_vdac_power_mode_t#

sl_hal_vdac_power_mode_t

Channel power mode.

Enumerator
SL_HAL_VDAC_POWER_MODE_HIGH_POWER

High power buffer mode.

SL_HAL_VDAC_POWER_MODE_LOW_POWER

Low power buffer mode.


sl_hal_vdac_port_selection_t#

sl_hal_vdac_port_selection_t

VDAC channel Abus port selection.

Enumerator
SL_HAL_VDAC_PORT_NONE

No GPIO selected.

SL_HAL_VDAC_PORT_A

Port A selected.

SL_HAL_VDAC_PORT_B

Port B selected.

SL_HAL_VDAC_PORT_C

Port C selected.

SL_HAL_VDAC_PORT_D

Port D selected.


Function Documentation#

sl_hal_vdac_init#

void sl_hal_vdac_init (VDAC_TypeDef * vdac, const sl_hal_vdac_init_t * init)

Initialize VDAC.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.

const sl_hal_vdac_init_t *[in]init

A pointer to the VDAC initialization structure.

Initializes the common parts for both channels. This function will also load calibration values from the Device Information (DI) page into the VDAC calibration register. To complete a VDAC setup, channel control configuration must also be done. See sl_hal_vdac_init_channel().

Note

  • This function will disable both channels prior to configuration.


sl_hal_vdac_init_channel#

void sl_hal_vdac_init_channel (VDAC_TypeDef * vdac, const sl_hal_vdac_init_channel_t * init, uint32_t channel)

Initialize a VDAC channel.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.

const sl_hal_vdac_init_channel_t *[in]init

A pointer to the VDAC channel initialization structure.

uint32_t[in]channel

A channel number to initialize.

Configures a specific VDAC channel with the provided settings.


sl_hal_vdac_enable_channel#

void sl_hal_vdac_enable_channel (VDAC_TypeDef * vdac, uint32_t channel)

Enable the VDAC channel.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.

uint32_t[in]channel

A channel to enable.


sl_hal_vdac_disable_channel#

void sl_hal_vdac_disable_channel (VDAC_TypeDef * vdac, uint32_t channel)

Disable the VDAC channel.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.

uint32_t[in]channel

A channel to disable.


sl_hal_vdac_set_output_channel#

void sl_hal_vdac_set_output_channel (VDAC_TypeDef * vdac, uint32_t channel, uint32_t value)

Set the output signal of a VDAC channel to a given value.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.

uint32_t[in]channel

A channel number to set the output of.

uint32_t[in]value

A value to write to the channel output register CHnDATA.

This function sets the output signal of a VDAC channel by writing value to the corresponding CHnDATA register.


sl_hal_vdac_calculate_prescaler#

uint32_t sl_hal_vdac_calculate_prescaler (VDAC_TypeDef * vdac, uint32_t vdac_frequency, uint32_t reference_frequency)

Calculate the prescaler value used to determine VDAC clock.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.

uint32_t[in]vdac_frequency

VDAC frequency target. The frequency will automatically be adjusted to be below the maximum allowed VDAC clock.

uint32_t[in]reference_frequency

Frequency in Hz of the reference VDAC.

The VDAC clock is given by the input clock divided by the prescaler+1. VDAC_CLK = IN_CLK / (prescale + 1) The maximum VDAC clock is 1 MHz.

Note

  • If the requested VDAC frequency is low and the maximum prescaler value can't adjust the actual VDAC frequency lower than requested, the maximum prescaler value is returned resulting in a higher VDAC frequency than requested.

Returns

  • A prescaler value to use for VDAC to achieve a clock value less than or equal to vdac_frequency.


sl_hal_vdac_reset#

void sl_hal_vdac_reset (VDAC_TypeDef * vdac)

Reset VDAC to its default state.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.


sl_hal_vdac_wait_sync#

void sl_hal_vdac_wait_sync (VDAC_TypeDef * vdac)

Wait for the vdac to complete all synchronization of register changes and commands.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.


sl_hal_vdac_wait_ready#

void sl_hal_vdac_wait_ready (VDAC_TypeDef * vdac)

Wait for the vdac to be completely disabled.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.


sl_hal_vdac_enable#

void sl_hal_vdac_enable (VDAC_TypeDef * vdac)

Enables the VDAC module.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.


sl_hal_vdac_disable#

void sl_hal_vdac_disable (VDAC_TypeDef * vdac)

Disables the VDAC module and ensures all operations are synchronized.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.


sl_hal_vdac_enable_interrupts#

void sl_hal_vdac_enable_interrupts (VDAC_TypeDef * vdac, uint32_t flags)

Enable one or more VDAC interrupts.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.

uint32_t[in]flags

VDAC interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the VDAC module (VDAC_IF_nnn).

Note

  • Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using sl_hal_vdac_clear_interrupts() prior to enabling the interrupt.


sl_hal_vdac_disable_interrupts#

void sl_hal_vdac_disable_interrupts (VDAC_TypeDef * vdac, uint32_t flags)

Disable one or more VDAC interrupts.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.

uint32_t[in]flags

VDAC interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the VDAC module (VDAC_IF_nnn).


sl_hal_vdac_set_interrupts#

void sl_hal_vdac_set_interrupts (VDAC_TypeDef * vdac, uint32_t flags)

Set one or more pending VDAC interrupts from SW.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.

uint32_t[in]flags

VDAC interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the VDAC module (VDAC_IF_nnn).


sl_hal_vdac_clear_interrupts#

void sl_hal_vdac_clear_interrupts (VDAC_TypeDef * vdac, uint32_t flags)

Clear one or more pending VDAC interrupts.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.

uint32_t[in]flags

Pending VDAC interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the VDAC module (VDAC_IF_nnn).


sl_hal_vdac_get_pending_interrupts#

uint32_t sl_hal_vdac_get_pending_interrupts (VDAC_TypeDef * vdac)

Get pending VDAC interrupt flags.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.

Returns

  • VDAC interrupt sources pending. Use a bitwise logic OR combination of valid interrupt flags for the VDAC module (VDAC_IF_nnn).


sl_hal_vdac_get_enabled_pending_interrupts#

uint32_t sl_hal_vdac_get_enabled_pending_interrupts (VDAC_TypeDef * vdac)

Get enabled and pending VDAC interrupt flags.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.

Useful for handling more interrupt sources in the same interrupt handler.

Returns

  • Pending and enabled VDAC interrupt sources. The return value is the bitwise AND combination of

    • the OR combination of enabled interrupt sources in VDACx_IEN_nnn register (VDACx_IEN_nnn) and

    • the OR combination of valid interrupt flags of the VDAC module (VDACx_IF_nnn).

Note

  • Interrupt flags are not cleared by the use of this function.


sl_hal_vdac_sine_mode_start#

void sl_hal_vdac_sine_mode_start (VDAC_TypeDef * vdac)

Start Sine mode.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.

This function sends the sine mode start signal to the DAC.


sl_hal_vdac_sine_mode_stop#

void sl_hal_vdac_sine_mode_stop (VDAC_TypeDef * vdac)

Stop Sine mode.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.

This function sends the sine mode stop signal to the DAC.


sl_hal_vdac_get_status#

uint32_t sl_hal_vdac_get_status (VDAC_TypeDef * vdac)

Get the VDAC Status register.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.

Returns

  • Current STATUS register value.


Macro Definition Documentation#

SL_HAL_VDAC_REF_VALID#

#define SL_HAL_VDAC_REF_VALID
Value:
(ref)

VDAC instance validation.


SL_HAL_VDAC_INIT_DEFAULT#

#define SL_HAL_VDAC_INIT_DEFAULT
Value:
{ \
_VDAC_CFG_WARMUPTIME_DEFAULT, /* Number of prescaled DAC_CLK for VDAC to warmup. */ \
false, /* Continue while debugging. */ \
false, /* On demand clock. */ \
false, /* DMA wake up. */ \
false, /* Bias keep warm. */ \
SL_HAL_VDAC_REFRESH_CYCLES_2, /* Refresh every 2nd cycle. */ \
SL_HAL_VDAC_OVERFLOW_CYCLE_2, /* Internal overflow every 2nd cycle. */ \
0, /* No prescaling. */ \
SL_HAL_VDAC_VREF_1V25, /* 1.25 V internal low noise reference. */ \
false, /* Do not reset prescaler on CH 0 start. */ \
false, /* Sine wave is stopped at the sample it's currently outputting. */ \
false, /* Disable sine mode. */ \
false, /* Differential mode. */ \
}

Default configuration for VDAC initialization structure.


SL_HAL_VDAC_INIT_SINE_GENERATION_MODE#

#define SL_HAL_VDAC_INIT_SINE_GENERATION_MODE
Value:
{ \
_VDAC_CFG_WARMUPTIME_DEFAULT, /* Number of prescaled DAC_CLK for VDAC to warmup. */ \
false, /* Continue while debugging. */ \
true, /* On demand clock. */ \
false, /* DMA wake up. */ \
false, /* Bias keep warm. */ \
SL_HAL_VDAC_REFRESH_CYCLES_8, /* Refresh every 8th cycle. */ \
SL_HAL_VDAC_OVERFLOW_CYCLE_2, /* Internal overflow every 2nd cycle. */ \
0, /* No prescaling. */ \
SL_HAL_VDAC_VREF_1V25, /* 1.25 V internal low noise reference. */ \
false, /* Do not reset prescaler on CH 0 start. */ \
false, /* Sine wave is stopped at the sample it's currently outputting. */ \
true, /* Enable sine mode. */ \
false, /* Differential mode. */ \
}

Sine mode configuration for VDAC initialization structure.


SL_HAL_VDAC_CHANNEL_INIT_DEFAULT#

#define SL_HAL_VDAC_CHANNEL_INIT_DEFAULT
Value:
{ \
false, /* Turn off between sample off conversions. */ \
true, /* Enable High cap mode. */ \
0, /* FIFO data low watermark at 0. */ \
SL_HAL_VDAC_REFRESH_NONE, /* Channel refresh source. */ \
SL_HAL_VDAC_TRIGGER_MODE_SW, /* Conversion triggered by CH0DATA or COMBDATA write. */ \
SL_HAL_VDAC_POWER_MODE_HIGH_POWER, /* High power mode enabled. */ \
false, /* Continuous conversion mode. */ \
0, /* ABUS pin selected. */ \
SL_HAL_VDAC_PORT_NONE, /* No Analog bus port selected. */ \
false, /* Output not shorted. */ \
false, /* Alternative output disabled. */ \
true, /* Main output enabled. */ \
0, /* Hold out time. Previously called settle time. */ \
}

Default configuration for VDAC channel initialization structure.