Building Your Wi-Fi Matter End Device and the chip-tool#
Build Environment for Linux#
This section will go through the steps required to build the chip-tool for Linux.
Do not execute any commands on this page as ROOT (no su required), unless specified
Prepare Linux Packages#
Update the latest packages by typing following commands in terminal:
$ sudo apt update
$ sudo apt installPrerequisites for Matter (CHIP) project on Linux#
1. Installing packages on Ubuntu Laptop/PC#
Open the Linux terminal from Start menu
Install required packages on Ubuntu Laptop/PC using the following commands:
$ sudo apt install git gcc g++ pkg-config libssl-dev libdbus-1-dev libglib2.0-dev libavahi-client-dev ninja-build python3-venv python3-dev python3-pip unzip libgirepository1.0-dev libcairo2-dev libreadline-dev
2. Building the Environment#
To build environment follow the Software setup and Compiling chip-tool steps given in SW_SETUP,